<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic s32k312 HSE AB SWAP in S32K</title>
    <link>https://community.nxp.com/t5/S32K/s32k312-HSE-AB-SWAP/m-p/2389535#M59633</link>
    <description>&lt;P&gt;hi:&lt;/P&gt;&lt;P&gt;I am currently using the AB swap function with HSE on the S32K312.&lt;/P&gt;&lt;P&gt;For example, the program is currently running from Partition A. During the first update, we erase/program the flash in Partition B, and then call the HSE interface to enable Partition B. At this point, no reset is performed.&lt;/P&gt;&lt;P&gt;During the second update, we still erase/program the flash in Partition B. However, if power is lost during the programming process and the device is powered on again, the program fails to run.&lt;/P&gt;&lt;P&gt;I would like to ask: if we enable Secure Boot, can we use SMR and Secure Recovery Mode to implement software-based switching/jumping between Partition A and Partition B?&lt;/P&gt;</description>
    <pubDate>Thu, 02 Jul 2026 08:33:43 GMT</pubDate>
    <dc:creator>ruller</dc:creator>
    <dc:date>2026-07-02T08:33:43Z</dc:date>
    <item>
      <title>s32k312 HSE AB SWAP</title>
      <link>https://community.nxp.com/t5/S32K/s32k312-HSE-AB-SWAP/m-p/2389535#M59633</link>
      <description>&lt;P&gt;hi:&lt;/P&gt;&lt;P&gt;I am currently using the AB swap function with HSE on the S32K312.&lt;/P&gt;&lt;P&gt;For example, the program is currently running from Partition A. During the first update, we erase/program the flash in Partition B, and then call the HSE interface to enable Partition B. At this point, no reset is performed.&lt;/P&gt;&lt;P&gt;During the second update, we still erase/program the flash in Partition B. However, if power is lost during the programming process and the device is powered on again, the program fails to run.&lt;/P&gt;&lt;P&gt;I would like to ask: if we enable Secure Boot, can we use SMR and Secure Recovery Mode to implement software-based switching/jumping between Partition A and Partition B?&lt;/P&gt;</description>
      <pubDate>Thu, 02 Jul 2026 08:33:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k312-HSE-AB-SWAP/m-p/2389535#M59633</guid>
      <dc:creator>ruller</dc:creator>
      <dc:date>2026-07-02T08:33:43Z</dc:date>
    </item>
    <item>
      <title>Re: s32k312 HSE AB SWAP</title>
      <link>https://community.nxp.com/t5/S32K/s32k312-HSE-AB-SWAP/m-p/2389924#M59648</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/261717"&gt;@ruller&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Take a look at the thread &lt;A href="https://community.nxp.com/t5/S32K/How-to-enable-the-rollback-function-of-Hse-AB-SWAP-on-S32K3/td-p/2145179" target="_blank" rel="noopener"&gt;How to enable the rollback function of HSE AB_SWAP on S32K3?&lt;/A&gt; It has some suggestions around rollback and recovery that might help with your implementation.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
      <pubDate>Thu, 02 Jul 2026 21:04:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k312-HSE-AB-SWAP/m-p/2389924#M59648</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2026-07-02T21:04:14Z</dc:date>
    </item>
  </channel>
</rss>