<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32k388 Boot ROM in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32k388-Boot-ROM/m-p/2387918#M59566</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/263854"&gt;@Ars_&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Booting in managed by sBAF which is actually code in internal FLASH. These Boot ROM sections are for HSE use.&lt;/P&gt;
&lt;P&gt;From an internal discussion, I can see that there was a request to modify the description, I will bump the thread to see when this fix will be applied.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 29 Jun 2026 21:12:45 GMT</pubDate>
    <dc:creator>Julián_AragónM</dc:creator>
    <dc:date>2026-06-29T21:12:45Z</dc:date>
    <item>
      <title>S32k388 Boot ROM</title>
      <link>https://community.nxp.com/t5/S32K/S32k388-Boot-ROM/m-p/2387407#M59544</link>
      <description>&lt;P&gt;There is mention of Boot ROM in the reference manual, but no further information is available.&lt;/P&gt;&lt;P&gt;RM just says five instances of 32kb boot rom is available&amp;nbsp;&lt;/P&gt;&lt;P&gt;At what point boot rom becomes relevant. Is there a firmware that run from here by the HSE even before sbaf is ran&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 28 Jun 2026 12:36:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k388-Boot-ROM/m-p/2387407#M59544</guid>
      <dc:creator>Ars_</dc:creator>
      <dc:date>2026-06-28T12:36:17Z</dc:date>
    </item>
    <item>
      <title>Re: S32k388 Boot ROM</title>
      <link>https://community.nxp.com/t5/S32K/S32k388-Boot-ROM/m-p/2387918#M59566</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/263854"&gt;@Ars_&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Booting in managed by sBAF which is actually code in internal FLASH. These Boot ROM sections are for HSE use.&lt;/P&gt;
&lt;P&gt;From an internal discussion, I can see that there was a request to modify the description, I will bump the thread to see when this fix will be applied.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 29 Jun 2026 21:12:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k388-Boot-ROM/m-p/2387918#M59566</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2026-06-29T21:12:45Z</dc:date>
    </item>
  </channel>
</rss>