<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: FS26 - MICROCONTROLLER COMPATIBILITY</title>
    <link>https://community.nxp.com/t5/S32K/FS26-MICROCONTROLLER-COMPATIBILITY/m-p/2385083#M59453</link>
    <description>Thank you for your answer.&lt;BR /&gt;-What makes a preprogrammed FS26 compatible with the s32k396 non-compatible with the s32k344, since the s32k344 has less current consumption compared to the s32k396?&lt;BR /&gt;-Is there a document that defines the various programmed versions?&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Enrico</description>
    <pubDate>Tue, 23 Jun 2026 12:44:48 GMT</pubDate>
    <dc:creator>ESof</dc:creator>
    <dc:date>2026-06-23T12:44:48Z</dc:date>
    <item>
      <title>FS26 - MICROCONTROLLER COMPATIBILITY</title>
      <link>https://community.nxp.com/t5/S32K/FS26-MICROCONTROLLER-COMPATIBILITY/m-p/2384819#M59439</link>
      <description>&lt;P&gt;Good evening,&lt;BR /&gt;I have the following questions regarding the FS26 - S32KXX family compatibility.&amp;nbsp;&lt;BR /&gt;1-Is there a single orderable FS26 option compatible both with a s32k344 and s32k396?&lt;BR /&gt;2-what do the third and fourth last digits of the FS26 part number stand for? (i.e. MFS2633HMDE4AD referring to E4)&amp;nbsp; Is the compatibility with a specific microcontroller defined in those digits?&lt;BR /&gt;&lt;BR /&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Tue, 23 Jun 2026 08:24:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FS26-MICROCONTROLLER-COMPATIBILITY/m-p/2384819#M59439</guid>
      <dc:creator>ESof</dc:creator>
      <dc:date>2026-06-23T08:24:34Z</dc:date>
    </item>
    <item>
      <title>Re: FS26 - MICROCONTROLLER COMPATIBILITY</title>
      <link>https://community.nxp.com/t5/S32K/FS26-MICROCONTROLLER-COMPATIBILITY/m-p/2385078#M59451</link>
      <description>&lt;P&gt;Hello Enrico,&lt;/P&gt;
&lt;P&gt;No, there is no single pre-programmed, orderable FS26 part number that natively supports both MCUs.&lt;/P&gt;
&lt;P&gt;Regarding the part number suffix (for example E4 in MFS2633HMDE4AD), this suffix represents a specific OTP/programmed variant. It is not by itself a generic MCU compatibility field. The actual base device capability is mainly defined by the FS26xyB/FS26xyD portion of the part number, which defines the silicon feature set (for example VCORE capability, number of trackers, LDT/FS1B presence and ASIL B vs ASIL D), while the suffix identifies the exact programmed version.&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;</description>
      <pubDate>Tue, 23 Jun 2026 12:38:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FS26-MICROCONTROLLER-COMPATIBILITY/m-p/2385078#M59451</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2026-06-23T12:38:03Z</dc:date>
    </item>
    <item>
      <title>Re: FS26 - MICROCONTROLLER COMPATIBILITY</title>
      <link>https://community.nxp.com/t5/S32K/FS26-MICROCONTROLLER-COMPATIBILITY/m-p/2385083#M59453</link>
      <description>Thank you for your answer.&lt;BR /&gt;-What makes a preprogrammed FS26 compatible with the s32k396 non-compatible with the s32k344, since the s32k344 has less current consumption compared to the s32k396?&lt;BR /&gt;-Is there a document that defines the various programmed versions?&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Enrico</description>
      <pubDate>Tue, 23 Jun 2026 12:44:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FS26-MICROCONTROLLER-COMPATIBILITY/m-p/2385083#M59453</guid>
      <dc:creator>ESof</dc:creator>
      <dc:date>2026-06-23T12:44:48Z</dc:date>
    </item>
    <item>
      <title>Re: FS26 - MICROCONTROLLER COMPATIBILITY</title>
      <link>https://community.nxp.com/t5/S32K/FS26-MICROCONTROLLER-COMPATIBILITY/m-p/2385087#M59454</link>
      <description>&lt;P&gt;Hello Enrico,&lt;/P&gt;
&lt;P&gt;Even if S32K344 has lower current consumption, a version programmed for S32K396 may still differ in voltage settings, sequencing, monitoring thresholds and safety configuration, so it should not be assumed to be interchangeable. The detailed programmed-version definition is provided in the FS26 datasheet, especially in the orderable part number tables, the OTP description section and the complete OTP content table referenced by the datasheet.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BRs, Tomas&lt;/P&gt;</description>
      <pubDate>Tue, 23 Jun 2026 12:50:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FS26-MICROCONTROLLER-COMPATIBILITY/m-p/2385087#M59454</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2026-06-23T12:50:55Z</dc:date>
    </item>
  </channel>
</rss>