<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックUsing S32K3X8EVB-Q289 On-Board Debugger to Program a Custom S32K358 Target</title>
    <link>https://community.nxp.com/t5/S32K/Using-S32K3X8EVB-Q289-On-Board-Debugger-to-Program-a-Custom/m-p/2384026#M59406</link>
    <description>&lt;P class=""&gt;&lt;SPAN&gt;I am currently using the S32K3X8EVB-Q289 evaluation board and have developed a custom hardware design based on the S32K358 MCU.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;Could you please clarify:&lt;/SPAN&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;SPAN&gt;Is programming/debugging an external S32K358 target using the EVB's on-board debugger officially supported?&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;If supported, what jumper settings or hardware modifications are required on the EVB?&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;Which debug connector should be used for this purpose?&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;Are there any limitations compared to using an S32 Debug Probe ?&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;Is there any documentation or application note describing this configuration?&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN&gt;Thank you for your support.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Yash Gupta&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 22 Jun 2026 09:01:00 GMT</pubDate>
    <dc:creator>Yash2530</dc:creator>
    <dc:date>2026-06-22T09:01:00Z</dc:date>
    <item>
      <title>Using S32K3X8EVB-Q289 On-Board Debugger to Program a Custom S32K358 Target</title>
      <link>https://community.nxp.com/t5/S32K/Using-S32K3X8EVB-Q289-On-Board-Debugger-to-Program-a-Custom/m-p/2384026#M59406</link>
      <description>&lt;P class=""&gt;&lt;SPAN&gt;I am currently using the S32K3X8EVB-Q289 evaluation board and have developed a custom hardware design based on the S32K358 MCU.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;Could you please clarify:&lt;/SPAN&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;SPAN&gt;Is programming/debugging an external S32K358 target using the EVB's on-board debugger officially supported?&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;If supported, what jumper settings or hardware modifications are required on the EVB?&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;Which debug connector should be used for this purpose?&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;Are there any limitations compared to using an S32 Debug Probe ?&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;Is there any documentation or application note describing this configuration?&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN&gt;Thank you for your support.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Yash Gupta&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Jun 2026 09:01:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Using-S32K3X8EVB-Q289-On-Board-Debugger-to-Program-a-Custom/m-p/2384026#M59406</guid>
      <dc:creator>Yash2530</dc:creator>
      <dc:date>2026-06-22T09:01:00Z</dc:date>
    </item>
    <item>
      <title>Re: Using S32K3X8EVB-Q289 On-Board Debugger to Program a Custom S32K358 Target</title>
      <link>https://community.nxp.com/t5/S32K/Using-S32K3X8EVB-Q289-On-Board-Debugger-to-Program-a-Custom/m-p/2384177#M59416</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/263979"&gt;@Yash2530&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;1.&amp;nbsp;Yes, using the S32K3X8EVB-Q289 on-board debugger to program/debug an external S32K358 target is supported. Actually, the EVB’s on-board OpenSDA debugger uses a P&amp;amp;E Micro-developed bootloader/debug application&amp;nbsp;-&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio/Which-debugging-interface-is-better/m-p/1715877" target="_blank"&gt;https://community.nxp.com/t5/S32-Design-Studio/Which-debugging-interface-is-better/m-p/1715877&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;2.&amp;nbsp;No soldering rework or jumper setting is required on the EVB for this use case.&lt;/P&gt;
&lt;P&gt;3. J55&amp;nbsp;USB host connector.&lt;/P&gt;
&lt;P&gt;4.&amp;nbsp;In practice, for standard flashing and source-level debug of an external S32K358 target, the EVB’s on-board debugger should be sufficient. Since I don't know what feature is important to you, please compare features by yourself:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/software/automotive-software-and-tools/s32-design-studio-ide/s32-debugger-for-s32-platform:S32DBG-S32PLATFORM" target="_blank"&gt;https://www.nxp.com/design/design-center/software/automotive-software-and-tools/s32-design-studio-ide/s32-debugger-for-s32-platform:S32DBG-S32PLATFORM&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320180&amp;amp;productTab=5045" target="_blank"&gt;https://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320180&amp;amp;productTab=5045&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;5. Yes,&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/Download?colCode=S32K3X8EVB-Q289HWUM" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=S32K3X8EVB-Q289HWUM&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Mon, 22 Jun 2026 13:14:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Using-S32K3X8EVB-Q289-On-Board-Debugger-to-Program-a-Custom/m-p/2384177#M59416</guid>
      <dc:creator>PavelL</dc:creator>
      <dc:date>2026-06-22T13:14:20Z</dc:date>
    </item>
  </channel>
</rss>