<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Build Error in 1500V BMS Reference Application – SAF Library Errors in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Build-Error-in-1500V-BMS-Reference-Application-SAF-Library/m-p/2381321#M59270</link>
    <description>&lt;P&gt;Dear NXP Support Team,&lt;/P&gt;&lt;P&gt;We are facing a fatal build error in our 1500V BMS Reference Application project (S32K3-BESS-Firmware-Version-0.8.0-Demo) in S32 Design Studio.&lt;/P&gt;&lt;P&gt;Multiple sCheck_*.h headers referenced in sCheck_Cfg.c are not found anywhere in the SDK (see attached screenshot).&lt;/P&gt;&lt;P&gt;Installed SAF Package: s32k3x_saf_1_0_4&lt;/P&gt;&lt;P&gt;This is causing a cascade of 20 build failures across Middleware, OS, Startup_Code, and SAF modules.&lt;/P&gt;&lt;P&gt;Could you please advise whether s32k3x_saf_1_0_4 includes the sCheck library, and if not, which package version we should install?&lt;/P&gt;&lt;P&gt;Attached is the full build log, installed packages list, and a screenshot of the missing headers for your reference.&lt;/P&gt;</description>
    <pubDate>Mon, 15 Jun 2026 11:05:02 GMT</pubDate>
    <dc:creator>GauravXB</dc:creator>
    <dc:date>2026-06-15T11:05:02Z</dc:date>
    <item>
      <title>Build Error in 1500V BMS Reference Application – SAF Library Errors</title>
      <link>https://community.nxp.com/t5/S32K/Build-Error-in-1500V-BMS-Reference-Application-SAF-Library/m-p/2381321#M59270</link>
      <description>&lt;P&gt;Dear NXP Support Team,&lt;/P&gt;&lt;P&gt;We are facing a fatal build error in our 1500V BMS Reference Application project (S32K3-BESS-Firmware-Version-0.8.0-Demo) in S32 Design Studio.&lt;/P&gt;&lt;P&gt;Multiple sCheck_*.h headers referenced in sCheck_Cfg.c are not found anywhere in the SDK (see attached screenshot).&lt;/P&gt;&lt;P&gt;Installed SAF Package: s32k3x_saf_1_0_4&lt;/P&gt;&lt;P&gt;This is causing a cascade of 20 build failures across Middleware, OS, Startup_Code, and SAF modules.&lt;/P&gt;&lt;P&gt;Could you please advise whether s32k3x_saf_1_0_4 includes the sCheck library, and if not, which package version we should install?&lt;/P&gt;&lt;P&gt;Attached is the full build log, installed packages list, and a screenshot of the missing headers for your reference.&lt;/P&gt;</description>
      <pubDate>Mon, 15 Jun 2026 11:05:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Build-Error-in-1500V-BMS-Reference-Application-SAF-Library/m-p/2381321#M59270</guid>
      <dc:creator>GauravXB</dc:creator>
      <dc:date>2026-06-15T11:05:02Z</dc:date>
    </item>
    <item>
      <title>Re: Build Error in 1500V BMS Reference Application – SAF Library Errors</title>
      <link>https://community.nxp.com/t5/S32K/Build-Error-in-1500V-BMS-Reference-Application-SAF-Library/m-p/2381351#M59273</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/263776"&gt;@GauravXB&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;This is because you are using the EVAL version of the SAF library, which is available for free.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1781528505723.png" style="width: 517px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/389009i601852FF9385499D/image-dimensions/517x460?v=v2" width="517" height="460" role="button" title="danielmartynek_0-1781528505723.png" alt="danielmartynek_0-1781528505723.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The header files are only included in the FULL version of the library, which is a paid (premium) software package.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/software/functional-safety-software/s32-safety-software-framework-saf-and-safety-peripheral-drivers-spd:SAF" target="_blank"&gt;https://www.nxp.com/design/design-center/software/functional-safety-software/s32-safety-software-framework-saf-and-safety-peripheral-drivers-spd:SAF&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 15 Jun 2026 13:02:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Build-Error-in-1500V-BMS-Reference-Application-SAF-Library/m-p/2381351#M59273</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2026-06-15T13:02:06Z</dc:date>
    </item>
  </channel>
</rss>