<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: WDOG cannot use 8-bit sequence refresh</title>
    <link>https://community.nxp.com/t5/S32K/WDOG-cannot-use-8-bit-sequence-refresh/m-p/2381320#M59269</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/254513"&gt;@GXY&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The WDOG supports an 8-bit refresh sequence, but it is highly timing-sensitive. Even if standard C code generates STRB instructions, the sequence can fail due to additional stack accesses or address reloads inserted between the byte writes. Using a compact GCC inline assembly block helps ensure the 8-bit refresh executes reliably.&lt;/P&gt;
&lt;BLOCKQUOTE&gt;&lt;LI-CODE lang="c"&gt;static inline void WDOG_Refresh8_AsmInline(void)
{
 __asm volatile(
 // "mrs r2, PRIMASK \n"
 // "cpsid i \n"
 // "dsb \n"

 "ldr r0, =0x40052004 \n"

 "movs r1, #0xA6 \n"
 "strb r1, [r0, #1] \n"

 "movs r1, #0x02 \n"
 "strb r1, [r0, #0] \n"

 "movs r1, #0xB4 \n"
 "strb r1, [r0, #1] \n"

 "movs r1, #0x80 \n"
 "strb r1, [r0, #0] \n"

 // "dsb \n"
 // "isb \n"
 // "msr PRIMASK, r2 \n"
 );
}&lt;/LI-CODE&gt;&lt;/BLOCKQUOTE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
    <pubDate>Mon, 15 Jun 2026 11:00:25 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2026-06-15T11:00:25Z</dc:date>
    <item>
      <title>WDOG cannot use 8-bit sequence refresh</title>
      <link>https://community.nxp.com/t5/S32K/WDOG-cannot-use-8-bit-sequence-refresh/m-p/2363091#M58461</link>
      <description>&lt;P&gt;I am unable to use 4 8-bit writes to refresh the watchdog of S32K144. Both 16 bit and 32-bit are acceptable, but 8-bit is not. I tried the 8-bit writing method in the picture, but it all failedThe original manual is as follows:&lt;/P&gt;&lt;P&gt;The refresh write sequence can be&lt;BR /&gt;• either two 16-bit writes ( 0xA602, 0xB480) or four 8-bit writes (0xA6, 0x02, 0xB4,&lt;BR /&gt;0x80) if WDOG_CS[CMD32EN] is 0;&lt;BR /&gt;• one 32-bit write (0xB480_A602) if WDOG_CS[CMD32EN] is 1.&lt;BR /&gt;to the CNT register. Both methods must occur before the WDG timeout; otherwise, the&lt;BR /&gt;watchdog resets the MCU.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 11 May 2026 03:42:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/WDOG-cannot-use-8-bit-sequence-refresh/m-p/2363091#M58461</guid>
      <dc:creator>GXY</dc:creator>
      <dc:date>2026-05-11T03:42:12Z</dc:date>
    </item>
    <item>
      <title>Re: WDOG cannot use 8-bit sequence refresh</title>
      <link>https://community.nxp.com/t5/S32K/WDOG-cannot-use-8-bit-sequence-refresh/m-p/2364476#M58534</link>
      <description>&lt;P&gt;Before starting the refresh sequence, disable the global&lt;BR /&gt;interrupts. Otherwise, an interrupt could effectively invalidate&lt;BR /&gt;the refresh sequence, if the interrupt occurs before the refresh&lt;BR /&gt;writes finish. After the sequence finishes, restore the global&lt;BR /&gt;interrupt control state.&amp;nbsp; FYI for interrupt checking&lt;/P&gt;</description>
      <pubDate>Wed, 13 May 2026 04:35:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/WDOG-cannot-use-8-bit-sequence-refresh/m-p/2364476#M58534</guid>
      <dc:creator>db16122</dc:creator>
      <dc:date>2026-05-13T04:35:51Z</dc:date>
    </item>
    <item>
      <title>Re: WDOG cannot use 8-bit sequence refresh</title>
      <link>https://community.nxp.com/t5/S32K/WDOG-cannot-use-8-bit-sequence-refresh/m-p/2365277#M58577</link>
      <description>&lt;P&gt;I confirm that the switch was interrupted before and after feeding the dog. In the same scenario, only changing the feeding sequence and using the 16 bit feeding method succeeded, but the 8-bit feeding method failed, and adjusting the order of the 8-bit feeding sequence did not work.&lt;/P&gt;</description>
      <pubDate>Thu, 14 May 2026 06:42:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/WDOG-cannot-use-8-bit-sequence-refresh/m-p/2365277#M58577</guid>
      <dc:creator>GXY</dc:creator>
      <dc:date>2026-05-14T06:42:40Z</dc:date>
    </item>
    <item>
      <title>Re: WDOG cannot use 8-bit sequence refresh</title>
      <link>https://community.nxp.com/t5/S32K/WDOG-cannot-use-8-bit-sequence-refresh/m-p/2381320#M59269</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/254513"&gt;@GXY&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The WDOG supports an 8-bit refresh sequence, but it is highly timing-sensitive. Even if standard C code generates STRB instructions, the sequence can fail due to additional stack accesses or address reloads inserted between the byte writes. Using a compact GCC inline assembly block helps ensure the 8-bit refresh executes reliably.&lt;/P&gt;
&lt;BLOCKQUOTE&gt;&lt;LI-CODE lang="c"&gt;static inline void WDOG_Refresh8_AsmInline(void)
{
 __asm volatile(
 // "mrs r2, PRIMASK \n"
 // "cpsid i \n"
 // "dsb \n"

 "ldr r0, =0x40052004 \n"

 "movs r1, #0xA6 \n"
 "strb r1, [r0, #1] \n"

 "movs r1, #0x02 \n"
 "strb r1, [r0, #0] \n"

 "movs r1, #0xB4 \n"
 "strb r1, [r0, #1] \n"

 "movs r1, #0x80 \n"
 "strb r1, [r0, #0] \n"

 // "dsb \n"
 // "isb \n"
 // "msr PRIMASK, r2 \n"
 );
}&lt;/LI-CODE&gt;&lt;/BLOCKQUOTE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Mon, 15 Jun 2026 11:00:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/WDOG-cannot-use-8-bit-sequence-refresh/m-p/2381320#M59269</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2026-06-15T11:00:25Z</dc:date>
    </item>
  </channel>
</rss>