<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Unable to Configure Platform Module in EB tresos AutoCore Template Project in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Unable-to-Configure-Platform-Module-in-EB-tresos-AutoCore/m-p/2379384#M59176</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/244803"&gt;@GaneshBhagwat&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Still, EB tresos is not an NXP product.&lt;BR /&gt;Could you please specify which NXP RTD revision and S32K3xx part number you are using?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 10 Jun 2026 08:33:01 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2026-06-10T08:33:01Z</dc:date>
    <item>
      <title>Unable to Configure Platform Module in EB tresos AutoCore Template Project</title>
      <link>https://community.nxp.com/t5/S32K/Unable-to-Configure-Platform-Module-in-EB-tresos-AutoCore/m-p/2378398#M59115</link>
      <description>&lt;P&gt;&lt;STRONG&gt;Subject: Unable to Configure Platform Module in EB tresos AutoCore Template Project&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Hi NXP Experts,&lt;/P&gt;&lt;P&gt;I am working with EB tresos and would like to use both the RTE and other AUTOSAR software layers provided by the AutoCore project template. I am able to generate the configuration successfully and the project builds and runs as expected.&lt;/P&gt;&lt;P&gt;However, I am encountering an issue with the &lt;STRONG&gt;Platform&lt;/STRONG&gt; module configuration.&lt;/P&gt;&lt;P&gt;When I create a project using the &lt;STRONG&gt;AutoCore Template for CORTEXM-S32K35x&lt;/STRONG&gt;, I can add the Platform module, but its configuration parameters are not available for editing. The configuration view appears restricted, and I cannot access the settings that I need to modify.&lt;/P&gt;&lt;P&gt;In contrast, when I create a &lt;STRONG&gt;blank project for CORTEXM-S32K3xx&lt;/STRONG&gt;, I can access and edit all Platform module configuration parameters without any issues.&lt;/P&gt;&lt;P&gt;My primary requirement is to configure &lt;STRONG&gt;interrupt-related settings&lt;/STRONG&gt; within the Platform module for my application.&lt;/P&gt;&lt;P&gt;I have attached screenshots showing both scenarios:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;P&gt;AutoCore Template project – Platform configuration is not editable.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Blank S32K3xx project – Platform configuration is fully accessible and editable.&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;I would appreciate your guidance on the following questions:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;Is the limited Platform configuration a known restriction or expected behavior of the AutoCore Template?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Can the Platform module be used together with AUTOSAR OS in the AutoCore environment, or are there any limitations or dependencies that prevent this?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;What is the recommended method for configuring interrupts when using the AutoCore Template?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Is there an AutoCore Template available for the generic &lt;STRONG&gt;CORTEXM-S32K3xx&lt;/STRONG&gt; platform, similar to the one provided for &lt;STRONG&gt;CORTEXM-S32K35x&lt;/STRONG&gt;?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Are there any detailed application notes, example projects, or reference guides that demonstrate the integration and usage of AUTOSAR OS with the AutoCore Template?&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;If additional project information or configuration details are required, I would be happy to provide them.&lt;/P&gt;&lt;P&gt;Thank you for your support.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ganesh&lt;/P&gt;</description>
      <pubDate>Mon, 08 Jun 2026 14:33:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Unable-to-Configure-Platform-Module-in-EB-tresos-AutoCore/m-p/2378398#M59115</guid>
      <dc:creator>GaneshBhagwat</dc:creator>
      <dc:date>2026-06-08T14:33:21Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to Configure Platform Module in EB tresos AutoCore Template Project</title>
      <link>https://community.nxp.com/t5/S32K/Unable-to-Configure-Platform-Module-in-EB-tresos-AutoCore/m-p/2378977#M59143</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/244803"&gt;@GaneshBhagwat&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I understand:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;In a blank S32K3xx project, the Platform module is fully editable&lt;/LI&gt;
&lt;LI&gt;In the AutoCore template project, the same module is restricted&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;A success in a blank project proves that the NXP RTD driver plugins and configuration parameters are valid. The failure inside the template indicates a template integration or module conflict, which is maintained and delivered by Elektrobit,&amp;nbsp;therefore, this should be handled by Elektrobit support, not NXP.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
      <pubDate>Tue, 09 Jun 2026 10:42:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Unable-to-Configure-Platform-Module-in-EB-tresos-AutoCore/m-p/2378977#M59143</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2026-06-09T10:42:42Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to Configure Platform Module in EB tresos AutoCore Template Project</title>
      <link>https://community.nxp.com/t5/S32K/Unable-to-Configure-Platform-Module-in-EB-tresos-AutoCore/m-p/2379089#M59151</link>
      <description>&lt;P&gt;Hello Daniel,&lt;/P&gt;&lt;P&gt;Thank you for the clarification.&lt;/P&gt;&lt;P&gt;However, the issue does not appear to be limited to the AutoCore template. I can reproduce the same behavior in a project created without the AutoCore template when selecting the &lt;STRONG&gt;CORTEXM-S32K35x&lt;/STRONG&gt; target.&lt;/P&gt;&lt;P&gt;Since the restriction is also present outside the AutoCore environment, could you please have a look and advise if there are any known limitations, configuration dependencies, or checks that I can perform to further investigate the issue?&lt;/P&gt;&lt;P&gt;Any guidance on possible root causes or debugging steps would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Ganesh&lt;/P&gt;</description>
      <pubDate>Tue, 09 Jun 2026 14:52:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Unable-to-Configure-Platform-Module-in-EB-tresos-AutoCore/m-p/2379089#M59151</guid>
      <dc:creator>GaneshBhagwat</dc:creator>
      <dc:date>2026-06-09T14:52:32Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to Configure Platform Module in EB tresos AutoCore Template Project</title>
      <link>https://community.nxp.com/t5/S32K/Unable-to-Configure-Platform-Module-in-EB-tresos-AutoCore/m-p/2379090#M59152</link>
      <description>&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;</description>
      <pubDate>Tue, 09 Jun 2026 14:54:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Unable-to-Configure-Platform-Module-in-EB-tresos-AutoCore/m-p/2379090#M59152</guid>
      <dc:creator>GaneshBhagwat</dc:creator>
      <dc:date>2026-06-09T14:54:42Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to Configure Platform Module in EB tresos AutoCore Template Project</title>
      <link>https://community.nxp.com/t5/S32K/Unable-to-Configure-Platform-Module-in-EB-tresos-AutoCore/m-p/2379384#M59176</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/244803"&gt;@GaneshBhagwat&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Still, EB tresos is not an NXP product.&lt;BR /&gt;Could you please specify which NXP RTD revision and S32K3xx part number you are using?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 10 Jun 2026 08:33:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Unable-to-Configure-Platform-Module-in-EB-tresos-AutoCore/m-p/2379384#M59176</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2026-06-10T08:33:01Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to Configure Platform Module in EB tresos AutoCore Template Project</title>
      <link>https://community.nxp.com/t5/S32K/Unable-to-Configure-Platform-Module-in-EB-tresos-AutoCore/m-p/2379504#M59182</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thank you for your response.&lt;/P&gt;&lt;P&gt;Regarding your question, I am primarily using RTD 5 in my projects. However, to investigate this issue further, I also installed and tested RTD 4, RTD 6, and RTD 7. I observed the same behavior across all RTD versions.&lt;/P&gt;&lt;P&gt;The screenshot attached in my previous reply was taken using RTD 6.&lt;/P&gt;&lt;P&gt;Since the issue is reproducible across multiple RTD releases, I am trying to understand whether this behavior is related to the selected target/platform configuration (CORTEXM-S32K35x) rather than a specific RTD version.&lt;/P&gt;&lt;P&gt;Could you please advise:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;Which specific S32K35x devices are expected to support full Platform module configuration within EB tresos?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Is there any known limitation or dependency when using the CORTEXM-S32K35x target that would cause the Platform configuration to be restricted or hidden?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Are interrupt-related Platform configurations expected to be managed through another module (for example, OS or Mcu configuration) when targeting S32K35x devices?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Is there a recommended reference project or example configuration that demonstrates the expected Platform module setup for S32K35x devices?&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;My goal is mainly to configure interrupt handling for the application, so any guidance on the recommended approach for S32K35x would be very helpful.&lt;/P&gt;&lt;P&gt;Thank you for your support and assistance.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Ganesh&lt;/P&gt;</description>
      <pubDate>Wed, 10 Jun 2026 11:19:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Unable-to-Configure-Platform-Module-in-EB-tresos-AutoCore/m-p/2379504#M59182</guid>
      <dc:creator>GaneshBhagwat</dc:creator>
      <dc:date>2026-06-10T11:19:15Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to Configure Platform Module in EB tresos AutoCore Template Project</title>
      <link>https://community.nxp.com/t5/S32K/Unable-to-Configure-Platform-Module-in-EB-tresos-AutoCore/m-p/2379526#M59183</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/244803"&gt;@GaneshBhagwat&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I'm looking at S32K358 RTD 6.0.0 examples imported to EB Tresos 29, they are all configured with target CORTEXM/S32K3xx, and the Platform driver can be reconfigured. Also, I don't see target&amp;nbsp;CORTEXM/S32K35x to be available in Tresos for new projects.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1781092959699.png" style="width: 761px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/388539iD2BCBE31F81FB2CC/image-dimensions/761x623?v=v2" width="761" height="623" role="button" title="danielmartynek_0-1781092959699.png" alt="danielmartynek_0-1781092959699.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
      <pubDate>Wed, 10 Jun 2026 12:06:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Unable-to-Configure-Platform-Module-in-EB-tresos-AutoCore/m-p/2379526#M59183</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2026-06-10T12:06:47Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to Configure Platform Module in EB tresos AutoCore Template Project</title>
      <link>https://community.nxp.com/t5/S32K/Unable-to-Configure-Platform-Module-in-EB-tresos-AutoCore/m-p/2380876#M59245</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thank you for your response and for checking the RTD 6.0.0 examples.&lt;/P&gt;&lt;P&gt;Yes, this is also what I observed. The Platform module is configurable when using the CORTEXM/S32K3xx target, but it is not accessible when using the CORTEXM/S32K35x target. This behavior is not limited to RTD 6; I observed the same restriction with other RTD versions as well.&lt;/P&gt;&lt;P&gt;My initial reason for trying the CORTEXM/S32K35x target was because it is used by the AutoCore template. However, while investigating further, I noticed that the OS configuration available under the CORTEXM/S32K35x target already contains ISR-related configuration options.&lt;/P&gt;&lt;P&gt;Based on this observation, I was wondering if the Platform module configuration is intentionally restricted for this target because interrupt configuration and management are expected to be handled through the AUTOSAR OS ISR configuration instead.&lt;/P&gt;&lt;P&gt;Could you please confirm if this understanding is correct?&lt;/P&gt;&lt;P&gt;Additionally, if there are any example projects, application notes, or reference documents showing how ISR configuration is intended to be done with AUTOSAR OS on the S32K35x platform, it would be extremely helpful. Any guidance on how to initialize and configure OS ISRs in this environment would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thank you again for your support and assistance.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Ganesh&lt;/P&gt;</description>
      <pubDate>Fri, 12 Jun 2026 14:44:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Unable-to-Configure-Platform-Module-in-EB-tresos-AutoCore/m-p/2380876#M59245</guid>
      <dc:creator>GaneshBhagwat</dc:creator>
      <dc:date>2026-06-12T14:44:04Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to Configure Platform Module in EB tresos AutoCore Template Project</title>
      <link>https://community.nxp.com/t5/S32K/Unable-to-Configure-Platform-Module-in-EB-tresos-AutoCore/m-p/2381948#M59293</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/244803"&gt;@GaneshBhagwat&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;As I said, I don't see any problem with NXP SW.&amp;nbsp;&lt;BR /&gt;The restriction appears when using the AutoCore template or the CORTEXM-S32K35x target, indicating that the limitation is introduced by the EB tresos project template or target integration and this is&amp;nbsp;maintained by Elektrobit.&amp;nbsp;Therefore, Elektrobit is the correct point of contact.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;
&lt;DIV style="font-family: 'Segoe UI'; font-size: 14px; font-style: normal; font-weight: 400; line-height: 20px;"&gt;&amp;nbsp;&lt;/DIV&gt;</description>
      <pubDate>Tue, 16 Jun 2026 11:48:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Unable-to-Configure-Platform-Module-in-EB-tresos-AutoCore/m-p/2381948#M59293</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2026-06-16T11:48:24Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to Configure Platform Module in EB tresos AutoCore Template Project</title>
      <link>https://community.nxp.com/t5/S32K/Unable-to-Configure-Platform-Module-in-EB-tresos-AutoCore/m-p/2382488#M59325</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your clarification and for checking the NXP RTD examples.&lt;/P&gt;&lt;P&gt;Understood. Based on your feedback, it seems the restriction is related to the EB tresos template/target integration rather than the NXP RTD package itself. I will follow up with Elektrobit regarding the CORTEXM-S32K35x target configuration and the AutoCore template behavior.&lt;/P&gt;&lt;P&gt;During my investigation, I also noticed that when using this configuration, the OS task initialization is not behaving as expected and the OS task is failing during startup. Since the ISR-related configuration is available through the OS module for this target, I was trying to understand whether this is the intended configuration flow or if there are additional dependencies in the template integration.&lt;/P&gt;&lt;P&gt;I will investigate further from the EB side. Thank you again for your support.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Ganesh&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jun 2026 10:42:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Unable-to-Configure-Platform-Module-in-EB-tresos-AutoCore/m-p/2382488#M59325</guid>
      <dc:creator>GaneshBhagwat</dc:creator>
      <dc:date>2026-06-17T10:42:42Z</dc:date>
    </item>
  </channel>
</rss>