<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K314 Simulate IIC using GPIO</title>
    <link>https://community.nxp.com/t5/S32K/S32K314-Simulate-IIC-using-GPIO/m-p/2378523#M59118</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/263142"&gt;@Joker_Y&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The RTD package provides two examples: "I2c_Example_S32K3xx" and "I2c_Ip_Example_S32K3xx" (where xx corresponds to the specific S32K3 derivative). Both examples implement communication between an LPI2C instance and an emulated I2C interface using FlexIO.&lt;/P&gt;
&lt;P&gt;Currently, there are no examples specifically available for the S32K314 device. However, the example provided for the S32K344 can be used as a good reference for your application.&lt;/P&gt;
&lt;P&gt;For guidance on how to create a project based on these examples, please refer to:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-S32-Design-Studio-Create-a-New-S32DS-Project-from-Example/ta-p/1098969" target="_blank" rel="noopener"&gt;HOWTO: S32 Design Studio - Create a New S32DS Project from Example&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 08 Jun 2026 18:27:17 GMT</pubDate>
    <dc:creator>VaneB</dc:creator>
    <dc:date>2026-06-08T18:27:17Z</dc:date>
    <item>
      <title>S32K314 Simulate IIC using GPIO</title>
      <link>https://community.nxp.com/t5/S32K/S32K314-Simulate-IIC-using-GPIO/m-p/2375734#M58992</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;我在使用S32K314，172管脚封装，这三个管脚做模拟IIC的时候，PTD13用作SDA数据管脚，发现MCU无法将SDA配置成开漏输入，导致IIC设备无法拉低SDA。请问应该怎么解决？&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Joker_Y_0-1780480319081.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/387680iFDA408C7C10CF472/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Joker_Y_0-1780480319081.png" alt="Joker_Y_0-1780480319081.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Joker_Y_1-1780480548110.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/387686i737CA1F50B9DF73C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Joker_Y_1-1780480548110.png" alt="Joker_Y_1-1780480548110.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Joker_Y_2-1780480652479.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/387687iDCD8CFEDD1D86643/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Joker_Y_2-1780480652479.png" alt="Joker_Y_2-1780480652479.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Joker_Y_3-1780480658189.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/387688iD42A9FB4AA0B55D9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Joker_Y_3-1780480658189.png" alt="Joker_Y_3-1780480658189.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Joker_Y_4-1780480838753.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/387690iF7802081CD65EE51/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Joker_Y_4-1780480838753.png" alt="Joker_Y_4-1780480838753.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;在绿色波形箭头位置，我将蓝色的SDA设置为了输入模式，此时应该由外部设备拉低SDA，但实际上并没有被拉低，请问这是为什么？&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 03 Jun 2026 10:05:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K314-Simulate-IIC-using-GPIO/m-p/2375734#M58992</guid>
      <dc:creator>Joker_Y</dc:creator>
      <dc:date>2026-06-03T10:05:41Z</dc:date>
    </item>
    <item>
      <title>Re: S32K314 Simulate IIC using GPIO</title>
      <link>https://community.nxp.com/t5/S32K/S32K314-Simulate-IIC-using-GPIO/m-p/2376093#M58997</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/263142"&gt;@Joker_Y&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There is no dedicated open-drain configuration available in the SIUL2 module. However, when a pin is configured (muxed) to a peripheral that supports open-drain behavior like LPI2C the pin will behave accordingly and can be used in open-drain mode with other devices.&lt;/P&gt;
&lt;P&gt;In these situations, the actual behavior comes from how the peripheral (e.g., LPI2C) is configured rather than SIUL2 itself.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="VaneB_0-1780518215080.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/387754i8BA6E14589EE4ED9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="VaneB_0-1780518215080.png" alt="VaneB_0-1780518215080.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;You can configure the following options in the Pins Tool and Siul2 Port driver:&lt;/P&gt;
&lt;UL class="lia-list-style-type-circle"&gt;
&lt;LI&gt;Enable/disable the input buffer&lt;/LI&gt;
&lt;LI&gt;Enable/disable the output buffer&lt;/LI&gt;
&lt;LI&gt;Configure internal pull-up or pull-down&lt;/LI&gt;
&lt;/UL&gt;
&lt;DIV&gt;Please note that S32K3 devices already include a native LPI2C designed to handle I2C communication. While it is technically possible to emulate I2C via GPIO using custom software, this approach falls outside the scope of our support. As a result, we are unable to guarantee its functionality or performance.&lt;/DIV&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
      <pubDate>Wed, 03 Jun 2026 20:26:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K314-Simulate-IIC-using-GPIO/m-p/2376093#M58997</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2026-06-03T20:26:58Z</dc:date>
    </item>
    <item>
      <title>Re: S32K314 Simulate IIC using GPIO</title>
      <link>https://community.nxp.com/t5/S32K/S32K314-Simulate-IIC-using-GPIO/m-p/2376432#M59003</link>
      <description>&lt;P&gt;Hi,&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201913" target="_blank" rel="noopener"&gt;&lt;SPAN class=""&gt;VaneB&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;请问在使用过程中（程序允许过程中），Enable/disable the input bufferEnable/disable the output bufferConfigure internal pull-up or pull-down这些应该怎么操作？你们有没有GPIO模拟软件IIC的demo，可以发一下吗？谢谢&lt;/P&gt;</description>
      <pubDate>Thu, 04 Jun 2026 05:50:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K314-Simulate-IIC-using-GPIO/m-p/2376432#M59003</guid>
      <dc:creator>Joker_Y</dc:creator>
      <dc:date>2026-06-04T05:50:56Z</dc:date>
    </item>
    <item>
      <title>Re: S32K314 Simulate IIC using GPIO</title>
      <link>https://community.nxp.com/t5/S32K/S32K314-Simulate-IIC-using-GPIO/m-p/2377686#M59070</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/263142"&gt;@Joker_Y&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;When adding a pin in the Pin tool within the configuration tools, several parameters become available, such as Direction, Safe Mode Control, and Pull Select, among others. These parameters are presented as drop-down lists, allowing you to select the appropriate configuration for each pin.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="VaneB_0-1780680202789.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/388076i226BF8F64613DADD/image-size/medium?v=v2&amp;amp;px=400" role="button" title="VaneB_0-1780680202789.png" alt="VaneB_0-1780680202789.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;All selected configurations are applied to the pins during initialization when calling Port_Init() or Siul2_Port_Ip_Init().&lt;/P&gt;
&lt;P&gt;Regarding a demo for emulating I2C via GPIO, we currently do not provide such an example. As mentioned previously, S32K3 devices include a native LPI2C peripheral, which is specifically designed to handle I2C communication&lt;/P&gt;
&lt;P&gt;If emulation is required, examples using FlexIO for I2C emulation are available as an alternative approach.&lt;/P&gt;</description>
      <pubDate>Fri, 05 Jun 2026 17:23:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K314-Simulate-IIC-using-GPIO/m-p/2377686#M59070</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2026-06-05T17:23:44Z</dc:date>
    </item>
    <item>
      <title>Re: S32K314 Simulate IIC using GPIO</title>
      <link>https://community.nxp.com/t5/S32K/S32K314-Simulate-IIC-using-GPIO/m-p/2377792#M59076</link>
      <description>&lt;P&gt;Hi,&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201913" target="_blank"&gt;&lt;SPAN class=""&gt;VaneB&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;我在使用IO模拟IIC过程中发现，当配置为Input模式的时候，发现外部芯片的SDA管脚无法拉低NXP芯片的管脚。您说的&lt;SPAN&gt;FlexIO for I2C的demo麻烦提供一下谢谢。&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 06 Jun 2026 07:44:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K314-Simulate-IIC-using-GPIO/m-p/2377792#M59076</guid>
      <dc:creator>Joker_Y</dc:creator>
      <dc:date>2026-06-06T07:44:22Z</dc:date>
    </item>
    <item>
      <title>Re: S32K314 Simulate IIC using GPIO</title>
      <link>https://community.nxp.com/t5/S32K/S32K314-Simulate-IIC-using-GPIO/m-p/2378523#M59118</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/263142"&gt;@Joker_Y&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The RTD package provides two examples: "I2c_Example_S32K3xx" and "I2c_Ip_Example_S32K3xx" (where xx corresponds to the specific S32K3 derivative). Both examples implement communication between an LPI2C instance and an emulated I2C interface using FlexIO.&lt;/P&gt;
&lt;P&gt;Currently, there are no examples specifically available for the S32K314 device. However, the example provided for the S32K344 can be used as a good reference for your application.&lt;/P&gt;
&lt;P&gt;For guidance on how to create a project based on these examples, please refer to:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-S32-Design-Studio-Create-a-New-S32DS-Project-from-Example/ta-p/1098969" target="_blank" rel="noopener"&gt;HOWTO: S32 Design Studio - Create a New S32DS Project from Example&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 08 Jun 2026 18:27:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K314-Simulate-IIC-using-GPIO/m-p/2378523#M59118</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2026-06-08T18:27:17Z</dc:date>
    </item>
    <item>
      <title>Re: S32K314 Simulate IIC using GPIO</title>
      <link>https://community.nxp.com/t5/S32K/S32K314-Simulate-IIC-using-GPIO/m-p/2379025#M59148</link>
      <description>&lt;P&gt;好的，谢谢&lt;/P&gt;</description>
      <pubDate>Tue, 09 Jun 2026 12:02:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K314-Simulate-IIC-using-GPIO/m-p/2379025#M59148</guid>
      <dc:creator>Joker_Y</dc:creator>
      <dc:date>2026-06-09T12:02:19Z</dc:date>
    </item>
  </channel>
</rss>