<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ADKP Password Change in S32K</title>
    <link>https://community.nxp.com/t5/S32K/ADKP-Password-Change/m-p/2378390#M59112</link>
    <description>&lt;P&gt;No, it is not possible to change or reset the ADKP after Configuration Lock when the device is in IN_FIELD, as ADKP is a one-time programmable attribute.&lt;BR /&gt;It is also not possible to change the lifecycle from IN_FIELD back to CUST_DEL, since lifecycle transitions are one-way and irreversible.&lt;/P&gt;</description>
    <pubDate>Mon, 08 Jun 2026 14:10:17 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2026-06-08T14:10:17Z</dc:date>
    <item>
      <title>ADKP Password Change</title>
      <link>https://community.nxp.com/t5/S32K/ADKP-Password-Change/m-p/2378175#M59100</link>
      <description>&lt;P&gt;Hello NXP,&lt;BR /&gt;We are using the S32K312 board.&lt;BR /&gt;We would like to know whether it is possible to change (or reset) the previously configured ADKP after Configuration Lock when the Life-Cycle is in the In-Field state.&lt;/P&gt;&lt;P&gt;Additionally, we would like to know whether it is possible to change the Life-Cycle from IN_FIELD to CUST_DEL.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;@&lt;A href="mailto:bi.moon@partron.co.kr" target="_blank"&gt;bi.moon@partron.co.kr&lt;/A&gt;&lt;/P&gt;&lt;P&gt;@&lt;A href="mailto:dwyun@partron.co.kr" target="_blank"&gt;dwyun@partron.co.kr&lt;/A&gt;&lt;/P&gt;&lt;P&gt;@&lt;A href="mailto:cb.an@partron.co.kr" target="_blank"&gt;cb.an@partron.co.kr&lt;/A&gt;&lt;/P&gt;&lt;P&gt;@&lt;A href="mailto:pyoleo0079@partron.co.kr" target="_blank"&gt;pyoleo0079@partron.co.kr&lt;/A&gt;&lt;/P&gt;&lt;P&gt;@&lt;A href="mailto:inbae.jeong@mobis.com" target="_blank"&gt;inbae.jeong@mobis.com&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 08 Jun 2026 08:13:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ADKP-Password-Change/m-p/2378175#M59100</guid>
      <dc:creator>Gitae</dc:creator>
      <dc:date>2026-06-08T08:13:53Z</dc:date>
    </item>
    <item>
      <title>Re: ADKP Password Change</title>
      <link>https://community.nxp.com/t5/S32K/ADKP-Password-Change/m-p/2378390#M59112</link>
      <description>&lt;P&gt;No, it is not possible to change or reset the ADKP after Configuration Lock when the device is in IN_FIELD, as ADKP is a one-time programmable attribute.&lt;BR /&gt;It is also not possible to change the lifecycle from IN_FIELD back to CUST_DEL, since lifecycle transitions are one-way and irreversible.&lt;/P&gt;</description>
      <pubDate>Mon, 08 Jun 2026 14:10:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ADKP-Password-Change/m-p/2378390#M59112</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2026-06-08T14:10:17Z</dc:date>
    </item>
  </channel>
</rss>