<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K388 Hardware Specs Verification — RAM/ROM/Cache Sizes, Bus Connections, Power, NVIC &amp;amp; Watchdog in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K388-Hardware-Specs-Verification-RAM-ROM-Cache-Sizes-Bus/m-p/2377218#M59047</link>
    <description>&lt;P&gt;&lt;SPAN&gt;I am documenting the S32K388 hardware architecture for our project and have compiled the specifications below based on the Reference Manual (RM). However, I have&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="s32k388.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/387982iE0DF4890F027CDC2/image-size/large?v=v2&amp;amp;px=999" role="button" title="s32k388.png" alt="s32k388.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;s32k388.png&lt;/span&gt;&lt;/span&gt; uncertainties that I need to verify with the community. I would appreciate confirmation or pointers to the exact RM chapters.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 05 Jun 2026 05:45:04 GMT</pubDate>
    <dc:creator>xlele</dc:creator>
    <dc:date>2026-06-05T05:45:04Z</dc:date>
    <item>
      <title>S32K388 Hardware Specs Verification — RAM/ROM/Cache Sizes, Bus Connections, Power, NVIC &amp; Watchdog</title>
      <link>https://community.nxp.com/t5/S32K/S32K388-Hardware-Specs-Verification-RAM-ROM-Cache-Sizes-Bus/m-p/2377218#M59047</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I am documenting the S32K388 hardware architecture for our project and have compiled the specifications below based on the Reference Manual (RM). However, I have&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="s32k388.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/387982iE0DF4890F027CDC2/image-size/large?v=v2&amp;amp;px=999" role="button" title="s32k388.png" alt="s32k388.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;s32k388.png&lt;/span&gt;&lt;/span&gt; uncertainties that I need to verify with the community. I would appreciate confirmation or pointers to the exact RM chapters.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 05 Jun 2026 05:45:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K388-Hardware-Specs-Verification-RAM-ROM-Cache-Sizes-Bus/m-p/2377218#M59047</guid>
      <dc:creator>xlele</dc:creator>
      <dc:date>2026-06-05T05:45:04Z</dc:date>
    </item>
    <item>
      <title>Re: S32K388 Hardware Specs Verification — RAM/ROM/Cache Sizes, Bus Connections, Power, NVIC &amp; Wa</title>
      <link>https://community.nxp.com/t5/S32K/S32K388-Hardware-Specs-Verification-RAM-ROM-Cache-Sizes-Bus/m-p/2377661#M59069</link>
      <description>&lt;P&gt;The provided table is mostly correct in terms of memory sizes (8 MB PFLASH, 128 KB DFLASH, ~1.125 MB SRAM including ~384 KB TCM, and 16 KB I/D cache per core).&lt;/P&gt;
&lt;P&gt;However, some points need clarification:&lt;/P&gt;
&lt;P&gt;- Flash does not operate at a fixed “250 MHz”. Its performance depends on wait states and controller configuration, not a simple frequency.&lt;BR /&gt;- Access to Flash and SRAM is through the system interconnect (AXBS crossbar), while TCM is directly connected to the core and runs at core frequency.&lt;BR /&gt;- The “64-bit XBAR” description is an oversimplification; the architecture uses a multi-layer crossbar with multiple masters and ports.&lt;BR /&gt;- The stated 12-cycle interrupt latency corresponds to the theoretical Cortex-M7 minimum. Actual latency is higher depending on system conditions.&lt;BR /&gt;- There is no EWM module on S32K3 devices; the primary watchdog is SWT.&lt;/P&gt;
&lt;P&gt;For performance analysis, it is important to distinguish between TCM (deterministic, core-coupled), SRAM (via interconnect), and Flash (via controller with latency).&lt;/P&gt;</description>
      <pubDate>Fri, 05 Jun 2026 15:37:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K388-Hardware-Specs-Verification-RAM-ROM-Cache-Sizes-Bus/m-p/2377661#M59069</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2026-06-05T15:37:49Z</dc:date>
    </item>
  </channel>
</rss>