<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: FRDM-A-S32K358 question</title>
    <link>https://community.nxp.com/t5/S32K/FRDM-A-S32K358-question/m-p/2377167#M59043</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;I compared the &lt;STRONG&gt;S32K3X8EVB-Q289 Hardware User Manual&lt;/STRONG&gt; with the initial version of the &lt;STRONG&gt;FRDM-A-S32K358 development board&lt;/STRONG&gt; Hardware User Manual.&lt;/P&gt;
&lt;P&gt;Unfortunately, the &lt;STRONG&gt;FRDM-A-S32K358&lt;/STRONG&gt; only has one CAN interface, with the &lt;STRONG&gt;TJA1043&lt;/STRONG&gt; used as the CAN transceiver. Unlike the &lt;STRONG&gt;S32K3X8EVB-Q289&lt;/STRONG&gt;, which has two CAN interfaces, both using the &lt;STRONG&gt;TJA1153&lt;/STRONG&gt; as the CAN transceiver.&lt;/P&gt;
&lt;P&gt;UART TTL can be directly derived from the LPUART pins of the S32K358, so I am certain that both evaluation boards have more than 2 UART TTL channels.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Fri, 05 Jun 2026 03:01:42 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2026-06-05T03:01:42Z</dc:date>
    <item>
      <title>FRDM-A-S32K358 question</title>
      <link>https://community.nxp.com/t5/S32K/FRDM-A-S32K358-question/m-p/2376522#M59011</link>
      <description>&lt;P&gt;I am considering purchasing the FRDM-A-S32K358 board, but I need to know if it supports SD card functionality, two CAN channels, and two UARTs (TTL). If not, I confirmed that the S32K3X8EVB-Q289 supports these features, but I am only considering it because it is too expensive. If the FRDM-A-S32K358 has these capabilities, I plan to purchase that one. Please confirm this for me.&lt;/P&gt;</description>
      <pubDate>Thu, 04 Jun 2026 07:09:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FRDM-A-S32K358-question/m-p/2376522#M59011</guid>
      <dc:creator>SSSkkkmolea</dc:creator>
      <dc:date>2026-06-04T07:09:09Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-A-S32K358 question</title>
      <link>https://community.nxp.com/t5/S32K/FRDM-A-S32K358-question/m-p/2377167#M59043</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;I compared the &lt;STRONG&gt;S32K3X8EVB-Q289 Hardware User Manual&lt;/STRONG&gt; with the initial version of the &lt;STRONG&gt;FRDM-A-S32K358 development board&lt;/STRONG&gt; Hardware User Manual.&lt;/P&gt;
&lt;P&gt;Unfortunately, the &lt;STRONG&gt;FRDM-A-S32K358&lt;/STRONG&gt; only has one CAN interface, with the &lt;STRONG&gt;TJA1043&lt;/STRONG&gt; used as the CAN transceiver. Unlike the &lt;STRONG&gt;S32K3X8EVB-Q289&lt;/STRONG&gt;, which has two CAN interfaces, both using the &lt;STRONG&gt;TJA1153&lt;/STRONG&gt; as the CAN transceiver.&lt;/P&gt;
&lt;P&gt;UART TTL can be directly derived from the LPUART pins of the S32K358, so I am certain that both evaluation boards have more than 2 UART TTL channels.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 05 Jun 2026 03:01:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FRDM-A-S32K358-question/m-p/2377167#M59043</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2026-06-05T03:01:42Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-A-S32K358 question</title>
      <link>https://community.nxp.com/t5/S32K/FRDM-A-S32K358-question/m-p/2377174#M59045</link>
      <description>Hello i register company email&lt;BR /&gt;</description>
      <pubDate>Fri, 05 Jun 2026 03:13:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FRDM-A-S32K358-question/m-p/2377174#M59045</guid>
      <dc:creator>wj_kwak</dc:creator>
      <dc:date>2026-06-05T03:13:05Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-A-S32K358 question</title>
      <link>https://community.nxp.com/t5/S32K/FRDM-A-S32K358-question/m-p/2382773#M59339</link>
      <description>&lt;P&gt;The AE team informed me that the &lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/FRDM-A-S32K358" target="_self"&gt;FRDM-A-S32K358 webpage&lt;/A&gt; has been updated and the &lt;A href="https://www.nxp.com/webapp/Download?colCode=FRDM-A-S32K358-DESIGN-FILES" target="_self"&gt;FRDM-A-S32K358 Design Files&lt;/A&gt; can now be downloaded.&lt;/P&gt;</description>
      <pubDate>Thu, 18 Jun 2026 00:41:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FRDM-A-S32K358-question/m-p/2382773#M59339</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2026-06-18T00:41:37Z</dc:date>
    </item>
  </channel>
</rss>