<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Question on the functional difference between FRDM-A-S32K358 and S32K3X8EVB-Q289 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Question-on-the-functional-difference-between-FRDM-A-S32K358-and/m-p/2376611#M59017</link>
    <description>&lt;P&gt;Our company has an NDA in place. It seems likely that this is possible, but can you confirm if they will process it immediately if I request it via a support ticket?&lt;/P&gt;</description>
    <pubDate>Thu, 04 Jun 2026 08:32:25 GMT</pubDate>
    <dc:creator>SSSkkkmolea</dc:creator>
    <dc:date>2026-06-04T08:32:25Z</dc:date>
    <item>
      <title>Question on the functional difference between FRDM-A-S32K358 and S32K3X8EVB-Q289</title>
      <link>https://community.nxp.com/t5/S32K/Question-on-the-functional-difference-between-FRDM-A-S32K358-and/m-p/2376361#M59001</link>
      <description>&lt;P&gt;I am considering purchasing either the FRDM-A-S32K358 or the S32K3X8EVB-Q289 model. However, what are the hardware differences between the S32K3X8EVB-Q289 and the FRDM-A-S32K358?&lt;/P&gt;&lt;P&gt;I was told in a previous question that the SD card function is implemented on the FRDM-A-S32K358. I want to know if the other pins or features like CAN communication are present on the board. I want to know if they are implemented exactly the same way as the S32K3X8EVB-Q289. I would also like to know if there are any software differences. Or is there a separate circuit diagram? It would be easier for me to make a decision based on that.&lt;/P&gt;</description>
      <pubDate>Thu, 04 Jun 2026 03:05:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Question-on-the-functional-difference-between-FRDM-A-S32K358-and/m-p/2376361#M59001</guid>
      <dc:creator>SSSkkkmolea</dc:creator>
      <dc:date>2026-06-04T03:05:29Z</dc:date>
    </item>
    <item>
      <title>Re: Question on the functional difference between FRDM-A-S32K358 and S32K3X8EVB-Q289</title>
      <link>https://community.nxp.com/t5/S32K/Question-on-the-functional-difference-between-FRDM-A-S32K358-and/m-p/2376602#M59015</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Since this FRDM-A-S32K358 has not yet been officially released, the schematics or hardware manuals are not available for download at this time.&lt;/P&gt;
&lt;P&gt;Could you please provide your project and company information separately? Have you signed an &lt;A href="https://www.nxp.com/support/support:SUPPORTHOME?tid=sbmenu" target="_self"&gt;NDA&lt;/A&gt;? This would allow me to contact internal team to obtain information about the development board in advance.&lt;/P&gt;
&lt;P&gt;Currently, I can tell you that the FRDM-A-S32K358 has a CAN interface:&lt;BR /&gt;&lt;FONT color="#808080"&gt;This board integrates NXP’s TJA1043 CAN transceiver, with its output routed to connector J15.&lt;/FONT&gt;&lt;BR /&gt;CAN0_RX PTA6&lt;BR /&gt;CAN0_TX PTA7&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;I can only see the initial version of the &lt;STRONG&gt;UM12541 FRDM-A-S32K358 development board&lt;/STRONG&gt; internally at this time. I've attached the document's bookmarks to give you a general overview of its features. However, more detailed information will likely require you to sign an NDA or wait for the official release of the FRDM.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="bookmark UM12541 FRDM-A-S32K358 development board.png" style="width: 320px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/387872iAAAF7DF99E20B204/image-size/large?v=v2&amp;amp;px=999" role="button" title="bookmark UM12541 FRDM-A-S32K358 development board.png" alt="bookmark UM12541 FRDM-A-S32K358 development board.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 04 Jun 2026 08:26:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Question-on-the-functional-difference-between-FRDM-A-S32K358-and/m-p/2376602#M59015</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2026-06-04T08:26:12Z</dc:date>
    </item>
    <item>
      <title>Re: Question on the functional difference between FRDM-A-S32K358 and S32K3X8EVB-Q289</title>
      <link>https://community.nxp.com/t5/S32K/Question-on-the-functional-difference-between-FRDM-A-S32K358-and/m-p/2376611#M59017</link>
      <description>&lt;P&gt;Our company has an NDA in place. It seems likely that this is possible, but can you confirm if they will process it immediately if I request it via a support ticket?&lt;/P&gt;</description>
      <pubDate>Thu, 04 Jun 2026 08:32:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Question-on-the-functional-difference-between-FRDM-A-S32K358-and/m-p/2376611#M59017</guid>
      <dc:creator>SSSkkkmolea</dc:creator>
      <dc:date>2026-06-04T08:32:25Z</dc:date>
    </item>
    <item>
      <title>Re: Question on the functional difference between FRDM-A-S32K358 and S32K3X8EVB-Q289</title>
      <link>https://community.nxp.com/t5/S32K/Question-on-the-functional-difference-between-FRDM-A-S32K358-and/m-p/2376615#M59018</link>
      <description>&lt;P&gt;You are currently using a gmail account and the company information is not visible in the system. Please also provide me with the NDA number separately so I can have a colleague check if the NDA is still valid.&lt;/P&gt;</description>
      <pubDate>Thu, 04 Jun 2026 08:35:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Question-on-the-functional-difference-between-FRDM-A-S32K358-and/m-p/2376615#M59018</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2026-06-04T08:35:06Z</dc:date>
    </item>
  </channel>
</rss>