<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Do you have the FRDM-A-S32K358 Arduino shield?</title>
    <link>https://community.nxp.com/t5/S32K/Do-you-have-the-FRDM-A-S32K358-Arduino-shield/m-p/2376406#M59002</link>
    <description>&lt;P&gt;I am planning to buy the FRDM-A-S32K358, but there are no datasheets or schematics available. I would like to know if an Arduino shield is available, if it has fewer pins than the S32k3X8EVB-Q289, or if there are significant hardware differences between the boards themselves. Are there no schematic diagrams available? Or perhaps a DSN file?&lt;/P&gt;</description>
    <pubDate>Thu, 04 Jun 2026 04:30:27 GMT</pubDate>
    <dc:creator>SSSkkkmolea</dc:creator>
    <dc:date>2026-06-04T04:30:27Z</dc:date>
    <item>
      <title>Do you have the FRDM-A-S32K358 Arduino shield?</title>
      <link>https://community.nxp.com/t5/S32K/Do-you-have-the-FRDM-A-S32K358-Arduino-shield/m-p/2376406#M59002</link>
      <description>&lt;P&gt;I am planning to buy the FRDM-A-S32K358, but there are no datasheets or schematics available. I would like to know if an Arduino shield is available, if it has fewer pins than the S32k3X8EVB-Q289, or if there are significant hardware differences between the boards themselves. Are there no schematic diagrams available? Or perhaps a DSN file?&lt;/P&gt;</description>
      <pubDate>Thu, 04 Jun 2026 04:30:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Do-you-have-the-FRDM-A-S32K358-Arduino-shield/m-p/2376406#M59002</guid>
      <dc:creator>SSSkkkmolea</dc:creator>
      <dc:date>2026-06-04T04:30:27Z</dc:date>
    </item>
    <item>
      <title>Re: Do you have the FRDM-A-S32K358 Arduino shield?</title>
      <link>https://community.nxp.com/t5/S32K/Do-you-have-the-FRDM-A-S32K358-Arduino-shield/m-p/2376447#M59004</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;1. Arduino Compatibility&lt;/STRONG&gt;&lt;BR /&gt;The FRDM-A-S32K358 is part of the NXP FRDM Automotive ecosystem and is designed with ease of prototyping in mind.&lt;/P&gt;
&lt;P&gt;The board provides Arduino-compatible headers, enabling the use of standard Arduino shields for rapid application development.&lt;/P&gt;
&lt;P&gt;For reference, the S32K3X8EVB-Q289 evaluation board also supports an Arduino-compatible pin layout.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/S32K3X8EVB-Q289" target="_blank"&gt;https://www.nxp.com/design/design-center/development-boards-and-designs/S32K3X8EVB-Q289&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;2. Pin Availability&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;It is important to distinguish between:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;MCU capability (S32K358 device) vs.&lt;/LI&gt;
&lt;LI&gt;Accessible pins on the evaluation board&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;While the S32K358 MCU supports a high number of GPIOs (depending on package)&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;The S32K3X8EVB-Q289 is a full evaluation board providing broad access to MCU pins through multiple connectors and expansion interfaces.&lt;/LI&gt;
&lt;LI&gt;The FRDM-A-S32K358, by design, is a compact and cost-optimized board, and therefore exposes a reduced subset of pins, primarily through Arduino-compatible headers.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;As a result, not all MCU pins or peripheral signals are available externally on the FRDM board.&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;3. Hardware Differences Between FRDM and EVB&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;The two boards target different use cases:&lt;/P&gt;
&lt;P&gt;FRDM-A-S32K358&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Compact, low-cost&lt;/LI&gt;
&lt;LI&gt;Rapid prototyping, software development&lt;/LI&gt;
&lt;LI&gt;Arduino shields&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;S32K3X8EVB-Q289&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Full evaluation platform&lt;/LI&gt;
&lt;LI&gt;Full hardware evaluation and validation&lt;/LI&gt;
&lt;LI&gt;Arduino + additional connectors and interfaces&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;The S32K3X8EVB-Q289 typically integrates a broader range of external interfaces, connectors, and measurement capabilities, making it more suitable for detailed hardware evaluation and system validation.&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;4. Schematics and Design Files&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;The product is relatively new and I do not see any dedicated documentation here on the public web page.&lt;/P&gt;
&lt;P&gt;You can either wait for update of the page or request it by NXP support ticket at NXP.com.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 04 Jun 2026 06:25:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Do-you-have-the-FRDM-A-S32K358-Arduino-shield/m-p/2376447#M59004</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2026-06-04T06:25:52Z</dc:date>
    </item>
    <item>
      <title>Re: Do you have the FRDM-A-S32K358 Arduino shield?</title>
      <link>https://community.nxp.com/t5/S32K/Do-you-have-the-FRDM-A-S32K358-Arduino-shield/m-p/2376454#M59006</link>
      <description>&lt;P&gt;&lt;SPAN&gt;For S32K358, there are 3 types of demo board on the official website as below, which one you are talking about?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;RD-K358BMU&amp;nbsp; &amp;nbsp;RD-BESSK358BMU&amp;nbsp; &amp;nbsp;EVBMA6X02BMU&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;It seems there are no arduino connector&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 04 Jun 2026 06:31:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Do-you-have-the-FRDM-A-S32K358-Arduino-shield/m-p/2376454#M59006</guid>
      <dc:creator>db16122</dc:creator>
      <dc:date>2026-06-04T06:31:32Z</dc:date>
    </item>
    <item>
      <title>Re: Do you have the FRDM-A-S32K358 Arduino shield?</title>
      <link>https://community.nxp.com/t5/S32K/Do-you-have-the-FRDM-A-S32K358-Arduino-shield/m-p/2378261#M59107</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;S32K3X8EVB-Q289&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/S32K3X8EVB-Q289" target="_blank"&gt;https://www.nxp.com/design/design-center/development-boards-and-designs/S32K3X8EVB-Q289&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;The boards you listed are not equivalent general-purpose evaluation boards, but rather application-specific reference designs focused on battery management systems (BMS).&lt;/P&gt;
&lt;P&gt;As I have express in the post above.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 08 Jun 2026 09:33:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Do-you-have-the-FRDM-A-S32K358-Arduino-shield/m-p/2378261#M59107</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2026-06-08T09:33:11Z</dc:date>
    </item>
  </channel>
</rss>