<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K148-Q176 FreeRTOS official example Project in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K148-Q176-FreeRTOS-official-example-Project/m-p/997371#M5900</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,Petr,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;This problem is not about software(code). I check the connection of switch 3 and 4 . There are some hardware problems. These two switch cannot work. I have already contactednxp after-sales service department staff.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Liu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Feb 2020 04:48:28 GMT</pubDate>
    <dc:creator>carolineliu_wiw</dc:creator>
    <dc:date>2020-02-24T04:48:28Z</dc:date>
    <item>
      <title>S32K148-Q176 FreeRTOS official example Project</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-Q176-FreeRTOS-official-example-Project/m-p/997369#M5898</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I' m working with s32k148-q176 EVB, I try to test FreeRTOS explame project,“freertos_s32k148”. But when i press the Button sw4(PIN： PTC13), the LED has no change. I add one parameter “ctr” in Interrupt function "vPort_C_ISRHandler()" ,which is in rtos.c file. I open Real Time Expressions, want to check if the interrupt ISR execute or not. When i press the Button sw4，my parameter “ctr ” is still 0.&lt;/P&gt;&lt;P&gt;I have no idea, how to solve it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is Debug window.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/102448iB734B230DDAC80CD/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can&amp;nbsp;anyone help me？&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Liu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Feb 2020 02:01:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-Q176-FreeRTOS-official-example-Project/m-p/997369#M5898</guid>
      <dc:creator>carolineliu_wiw</dc:creator>
      <dc:date>2020-02-21T02:01:28Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148-Q176 FreeRTOS official example Project</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-Q176-FreeRTOS-official-example-Project/m-p/997370#M5899</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried this demo example and add a variable similarly&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/102491i9ADC3E4474C00DA2/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/102534i7A1DB240C44D7EBA/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When press SW4 red LED is ON and I see&amp;nbsp;vPort_C_ISRHandler_cnt updating in Real Time Expression window.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/102589i2D60442BD79C0D3D/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Be sure you do not halt the Expression Values Refresh.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Feb 2020 13:27:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-Q176-FreeRTOS-official-example-Project/m-p/997370#M5899</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2020-02-21T13:27:27Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148-Q176 FreeRTOS official example Project</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-Q176-FreeRTOS-official-example-Project/m-p/997371#M5900</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,Petr,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;This problem is not about software(code). I check the connection of switch 3 and 4 . There are some hardware problems. These two switch cannot work. I have already contactednxp after-sales service department staff.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Liu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Feb 2020 04:48:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-Q176-FreeRTOS-official-example-Project/m-p/997371#M5900</guid>
      <dc:creator>carolineliu_wiw</dc:creator>
      <dc:date>2020-02-24T04:48:28Z</dc:date>
    </item>
  </channel>
</rss>