<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックCSEC</title>
    <link>https://community.nxp.com/t5/S32K/CSEC/m-p/996751#M5890</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Target is S32K148, ONCE I ENABLED THE PARTION AND CSEC (FCCOB [2] = 0x03;)&lt;/P&gt;&lt;P&gt;Do I NEED IT D TO THIS INITIALIZATION ACROSS EVERY POWER ON REST?&lt;/P&gt;&lt;P&gt;which NONE VOULITILE REGISTER&amp;nbsp; I need to check if don't have to&amp;nbsp; this,?&lt;/P&gt;&lt;P&gt;I know once the part is partitioned , I don't have to it on every power up, however I am NOT certain about the CSEC ENABLING ACROSS POWE ON RESET.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;THANKS,&lt;/P&gt;&lt;P&gt;kOOROSH HAJIANI&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Mar 2020 22:13:39 GMT</pubDate>
    <dc:creator>hajianik</dc:creator>
    <dc:date>2020-03-05T22:13:39Z</dc:date>
    <item>
      <title>CSEC</title>
      <link>https://community.nxp.com/t5/S32K/CSEC/m-p/996751#M5890</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Target is S32K148, ONCE I ENABLED THE PARTION AND CSEC (FCCOB [2] = 0x03;)&lt;/P&gt;&lt;P&gt;Do I NEED IT D TO THIS INITIALIZATION ACROSS EVERY POWER ON REST?&lt;/P&gt;&lt;P&gt;which NONE VOULITILE REGISTER&amp;nbsp; I need to check if don't have to&amp;nbsp; this,?&lt;/P&gt;&lt;P&gt;I know once the part is partitioned , I don't have to it on every power up, however I am NOT certain about the CSEC ENABLING ACROSS POWE ON RESET.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;THANKS,&lt;/P&gt;&lt;P&gt;kOOROSH HAJIANI&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Mar 2020 22:13:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CSEC/m-p/996751#M5890</guid>
      <dc:creator>hajianik</dc:creator>
      <dc:date>2020-03-05T22:13:39Z</dc:date>
    </item>
    <item>
      <title>Re: CSEC</title>
      <link>https://community.nxp.com/t5/S32K/CSEC/m-p/996752#M5891</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;there's an application note including SW examples which provides more details:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=AN5401"&gt;https://www.nxp.com/webapp/Download?colCode=AN5401&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=AN5401SW&amp;amp;docLang=en"&gt;https://www.nxp.com/webapp/Download?colCode=AN5401SW&amp;amp;docLang=en&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Initialization (partition and initial loading of keys) is supposed to be done only once - in factory. See example 1_Configure_part_and_Load_keys in the app note.&lt;/P&gt;&lt;P&gt;It's even not possible to do the partitioning again. First it is necessary to delete the partition (there's a special procedure for this - see 5_Resetting_flash_to_the_factory_state), then it is necessary to do mass erase and then you can do the partitioning again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Mar 2020 07:44:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CSEC/m-p/996752#M5891</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2020-03-06T07:44:26Z</dc:date>
    </item>
  </channel>
</rss>