<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: FreeRTOS 2.0.0 is not available</title>
    <link>https://community.nxp.com/t5/S32K/FreeRTOS-2-0-0-is-not-available/m-p/2371573#M58894</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You cannot see the product because it is archived. It means there can be bugs in it, that will not be fixed. We usually recommend that customers use the newer version.&lt;/P&gt;
&lt;P&gt;However, if you insist on testing the older version, then&amp;nbsp;&lt;SPAN&gt;please wait while I contact the internal team to inquire how to add the software to your account.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Wed, 27 May 2026 01:34:15 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2026-05-27T01:34:15Z</dc:date>
    <item>
      <title>FreeRTOS 2.0.0 is not available</title>
      <link>https://community.nxp.com/t5/S32K/FreeRTOS-2-0-0-is-not-available/m-p/2371436#M58889</link>
      <description>&lt;P&gt;I am setting up&amp;nbsp;MR-CANHUBK344s with the S32 design example project. I have found the downloads for S32K3 RTD AUTOSAR 4.4 version 2.0.0 and S32K3xx development package Version 3.4.3, but the FreeRTOS for S32K3 2.0.0 is no longer available for download. The closest I find is 2.0.1 which does not work.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The file needed is&amp;nbsp;SW32K3_FreeRTOS_10.4.6_2.0.0_D2204.zip&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can someone share the link to this version?&lt;/P&gt;</description>
      <pubDate>Tue, 26 May 2026 17:25:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FreeRTOS-2-0-0-is-not-available/m-p/2371436#M58889</guid>
      <dc:creator>commando_j</dc:creator>
      <dc:date>2026-05-26T17:25:45Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS 2.0.0 is not available</title>
      <link>https://community.nxp.com/t5/S32K/FreeRTOS-2-0-0-is-not-available/m-p/2371573#M58894</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You cannot see the product because it is archived. It means there can be bugs in it, that will not be fixed. We usually recommend that customers use the newer version.&lt;/P&gt;
&lt;P&gt;However, if you insist on testing the older version, then&amp;nbsp;&lt;SPAN&gt;please wait while I contact the internal team to inquire how to add the software to your account.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 27 May 2026 01:34:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FreeRTOS-2-0-0-is-not-available/m-p/2371573#M58894</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2026-05-27T01:34:15Z</dc:date>
    </item>
  </channel>
</rss>