<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Software Selectable CAN Termination in S32K344</title>
    <link>https://community.nxp.com/t5/S32K/Software-Selectable-CAN-Termination-in-S32K344/m-p/2369153#M58763</link>
    <description>&lt;P class=""&gt;&lt;SPAN&gt;I am using FRDM-A-S32K344 with RTD 3.0.0.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;I want to know whether CAN termination resistor can be enabled or disabled through software in S32K344.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Does S32K344 support this internally, or do we need external hardware control&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Also, could you please explain how CAN termination is normally designed between the MCU and CAN transceiver, and how software-controlled CAN termination can be implemented?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 21 May 2026 06:00:11 GMT</pubDate>
    <dc:creator>ganavi1</dc:creator>
    <dc:date>2026-05-21T06:00:11Z</dc:date>
    <item>
      <title>Software Selectable CAN Termination in S32K344</title>
      <link>https://community.nxp.com/t5/S32K/Software-Selectable-CAN-Termination-in-S32K344/m-p/2369153#M58763</link>
      <description>&lt;P class=""&gt;&lt;SPAN&gt;I am using FRDM-A-S32K344 with RTD 3.0.0.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN&gt;I want to know whether CAN termination resistor can be enabled or disabled through software in S32K344.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Does S32K344 support this internally, or do we need external hardware control&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Also, could you please explain how CAN termination is normally designed between the MCU and CAN transceiver, and how software-controlled CAN termination can be implemented?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 21 May 2026 06:00:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Software-Selectable-CAN-Termination-in-S32K344/m-p/2369153#M58763</guid>
      <dc:creator>ganavi1</dc:creator>
      <dc:date>2026-05-21T06:00:11Z</dc:date>
    </item>
    <item>
      <title>Re: Software Selectable CAN Termination in S32K344</title>
      <link>https://community.nxp.com/t5/S32K/Software-Selectable-CAN-Termination-in-S32K344/m-p/2369925#M58796</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;there is no direct support for software‑selectable CAN termination in S32K3 MCUs or in our standard CAN transceivers.&lt;/SPAN&gt;&lt;/P&gt;
&lt;DIV&gt;
&lt;P&gt;The typical connection is: MCU (FlexCAN TX/RX) ↔ CAN transceiver ↔ CANH/CANL bus, with termination resistor(s) placed on the bus side.&lt;/P&gt;
&lt;P&gt;Standard high‑speed CAN/CAN FD requires two 120 Ω resistors (or split termination: 2×60 Ω with a capacitor to ground), located at each end of the bus backbone. Each ECU node in between are usually not terminated.&lt;/P&gt;
&lt;P&gt;If software‑selectable termination is required, it must be implemented using external hardware, typically a GPIO‑controlled analog switch, FET, or relay that inserts or removes the termination resistor.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;
&lt;/DIV&gt;</description>
      <pubDate>Fri, 22 May 2026 04:53:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Software-Selectable-CAN-Termination-in-S32K344/m-p/2369925#M58796</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2026-05-22T04:53:04Z</dc:date>
    </item>
    <item>
      <title>Re: Software Selectable CAN Termination in S32K344</title>
      <link>https://community.nxp.com/t5/S32K/Software-Selectable-CAN-Termination-in-S32K344/m-p/2369936#M58800</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Thanks for your reply&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 22 May 2026 05:24:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Software-Selectable-CAN-Termination-in-S32K344/m-p/2369936#M58800</guid>
      <dc:creator>ganavi1</dc:creator>
      <dc:date>2026-05-22T05:24:37Z</dc:date>
    </item>
  </channel>
</rss>