<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Download HSE Firmware using a Jlink-Segger Script</title>
    <link>https://community.nxp.com/t5/S32K/Download-HSE-Firmware-using-a-Jlink-Segger-Script/m-p/2368525#M58746</link>
    <description>&lt;P&gt;Hi there&lt;/P&gt;&lt;P&gt;I Need to Download FW into S32k310&amp;nbsp;&lt;/P&gt;&lt;P&gt;At the moment I use a NXP demo&amp;nbsp;HSE_FW_INSTALL&amp;nbsp; ported on s32k310.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I Notice that a Trace32 Practice Script can be used for the purpose.&lt;/P&gt;&lt;P&gt;Is it possible to create a Segger Jlink script&amp;nbsp; for this?&lt;/P&gt;&lt;P&gt;Which are the steps to do?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I need a faster process for mass production.&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Fabio&lt;/P&gt;</description>
    <pubDate>Wed, 20 May 2026 14:35:32 GMT</pubDate>
    <dc:creator>FabioG</dc:creator>
    <dc:date>2026-05-20T14:35:32Z</dc:date>
    <item>
      <title>Download HSE Firmware using a Jlink-Segger Script</title>
      <link>https://community.nxp.com/t5/S32K/Download-HSE-Firmware-using-a-Jlink-Segger-Script/m-p/2368525#M58746</link>
      <description>&lt;P&gt;Hi there&lt;/P&gt;&lt;P&gt;I Need to Download FW into S32k310&amp;nbsp;&lt;/P&gt;&lt;P&gt;At the moment I use a NXP demo&amp;nbsp;HSE_FW_INSTALL&amp;nbsp; ported on s32k310.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I Notice that a Trace32 Practice Script can be used for the purpose.&lt;/P&gt;&lt;P&gt;Is it possible to create a Segger Jlink script&amp;nbsp; for this?&lt;/P&gt;&lt;P&gt;Which are the steps to do?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I need a faster process for mass production.&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Fabio&lt;/P&gt;</description>
      <pubDate>Wed, 20 May 2026 14:35:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Download-HSE-Firmware-using-a-Jlink-Segger-Script/m-p/2368525#M58746</guid>
      <dc:creator>FabioG</dc:creator>
      <dc:date>2026-05-20T14:35:32Z</dc:date>
    </item>
    <item>
      <title>Re: Download HSE Firmware using a Jlink-Segger Script</title>
      <link>https://community.nxp.com/t5/S32K/Download-HSE-Firmware-using-a-Jlink-Segger-Script/m-p/2369543#M58780</link>
      <description>&lt;DIV style="font-family: 'Segoe UI'; font-size: 14px; font-style: normal; font-weight: 400; line-height: 20px;"&gt;
&lt;P&gt;At the moment, we do not have a ready-made solution or reference flow for HSE FW installation using SEGGER J-Link.&lt;/P&gt;
&lt;P&gt;The available and validated methods are TRACE32 Practice scripts, which are officially supported for this purpose, and HSE Demo applications, which are debugger-independent and can be ported and used to perform the installation.&lt;/P&gt;
&lt;P&gt;If you plan to use J-Link, a custom scripting solution would need to be developed on your side, based on the generic HSE installation sequence (UTEST flag programming, FW image download, reset), as NXP does not currently provide a dedicated J-Link script for this use case.&lt;/P&gt;
&lt;P&gt;For SEGGER-specific guidance, you may refer to their documentation or contact their support: &lt;A href="https://www.segger.com/support/" target="_blank"&gt;https://www.segger.com/support/&lt;/A&gt;&lt;/P&gt;
&lt;/DIV&gt;</description>
      <pubDate>Thu, 21 May 2026 11:30:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Download-HSE-Firmware-using-a-Jlink-Segger-Script/m-p/2369543#M58780</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2026-05-21T11:30:13Z</dc:date>
    </item>
  </channel>
</rss>