<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Debug S32K324 multi-core projects compiled with GHS using PE in S32DS.</title>
    <link>https://community.nxp.com/t5/S32K/Debug-S32K324-multi-core-projects-compiled-with-GHS-using-PE-in/m-p/2367336#M58692</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to consult about a relatively urgent issue:&lt;/P&gt;&lt;P&gt;How to configure settings to support multi-core debugging when debugging the S32K324 multi-core project via Processor Expert in S32DS?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Tue, 19 May 2026 06:53:18 GMT</pubDate>
    <dc:creator>yin2</dc:creator>
    <dc:date>2026-05-19T06:53:18Z</dc:date>
    <item>
      <title>Debug S32K324 multi-core projects compiled with GHS using PE in S32DS.</title>
      <link>https://community.nxp.com/t5/S32K/Debug-S32K324-multi-core-projects-compiled-with-GHS-using-PE-in/m-p/2367336#M58692</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to consult about a relatively urgent issue:&lt;/P&gt;&lt;P&gt;How to configure settings to support multi-core debugging when debugging the S32K324 multi-core project via Processor Expert in S32DS?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Tue, 19 May 2026 06:53:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Debug-S32K324-multi-core-projects-compiled-with-GHS-using-PE-in/m-p/2367336#M58692</guid>
      <dc:creator>yin2</dc:creator>
      <dc:date>2026-05-19T06:53:18Z</dc:date>
    </item>
    <item>
      <title>Re: Debug S32K324 multi-core projects compiled with GHS using PE in S32DS.</title>
      <link>https://community.nxp.com/t5/S32K/Debug-S32K324-multi-core-projects-compiled-with-GHS-using-PE-in/m-p/2367941#M58711</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/261440"&gt;@yin2&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Could you share which version of S32DS + RTD you are using? Since you've mentioned Processor Expert, then you may be using a legacy product.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There are some useful documents in community:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;&lt;A href="https://www.google.com/url?sa=t&amp;amp;rct=j&amp;amp;q=&amp;amp;esrc=s&amp;amp;source=web&amp;amp;cd=&amp;amp;cad=rja&amp;amp;uact=8&amp;amp;ved=2ahUKEwjnpsaXucaUAxX3kGoFHV72NcIQFnoECB4QAQ&amp;amp;url=https%3A%2F%2Fcommunity.nxp.com%2Fpwmxy87654%2Fattachments%2Fpwmxy87654%2Fs32ds%2540tkb%2F583%2F1%2FS32K324_Dual_Core_P%2526E%2520Multilink_S32DS.pdf&amp;amp;usg=AOvVaw1qV_gt6_9yUNVyao_g8tFM&amp;amp;opi=89978449" target="_self"&gt;S32K324 DUAL CORES DEBUG WITH P&amp;amp;E MULTILINK&lt;/A&gt;&amp;nbsp;&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-debug-multi-core-project-in-S32-Design-studio/ta-p/1128130" target="_blank"&gt;HOWTO: debug multi-core project in S32 Design studio&lt;/A&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;The process is fairly simple; create 2 (or the number of cores needed) debug configurations and include them in a launch group. Keep in mind that the secondary core needs to be enabled, either by the debugger, or by the boot core.&lt;/P&gt;
&lt;P&gt;You can also refer to the Whiteboard example package:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/S32K324-Multi-Core-Example-Project-based-on-Whiteboard/m-p/1515429" target="_blank"&gt;Solved: S32K324 Multi-Core Example Project based on Whiteboard - NXP Community&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
      <pubDate>Tue, 19 May 2026 22:58:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Debug-S32K324-multi-core-projects-compiled-with-GHS-using-PE-in/m-p/2367941#M58711</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2026-05-19T22:58:10Z</dc:date>
    </item>
  </channel>
</rss>