<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K144 ERM module issue in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-ERM-module-issue/m-p/995005#M5866</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, viewer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Recently I have used S32K144 chip's ERM module but have some questions.&lt;/P&gt;&lt;P&gt;The ERM module reports a non-correctable error and the address point to an unused place.&lt;/P&gt;&lt;P&gt;Below is the debug window message.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The attach is my project's .ld file and .map&amp;nbsp; file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/102408iB7E59215ECBD7D99/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The address 0x1FFFEB40 is not a address I have used.&lt;/P&gt;&lt;P&gt;And I have used the function "Debug_Watchpoint_And_Trace" (config as below) could catch the problem when the error occurred. I think it means nothing have accessed this address include pc pointer and all registers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I know a case that no registers and pc pointer&amp;nbsp;use the address but the address is accessed.That is when the cpu load the assembly , not only the current used instruction but also more instructions which will be used later will be load to "fifo". That means there is a case that an address is not used now but it has been accessed(this issue would cause a ERM error too, while the code is running in ram, but I have been resolve it).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So if there have the possible of the ERM error's reporting is because of the address in ram is pre-loaded in some case which is similar with the pre-load the assembly instructions? Or another issue cause the ERM error's reporting?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The attach files is my project's compiling map file and the ld file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 20 Feb 2020 10:26:40 GMT</pubDate>
    <dc:creator>chongrui_lu</dc:creator>
    <dc:date>2020-02-20T10:26:40Z</dc:date>
    <item>
      <title>S32K144 ERM module issue</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-ERM-module-issue/m-p/995005#M5866</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, viewer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Recently I have used S32K144 chip's ERM module but have some questions.&lt;/P&gt;&lt;P&gt;The ERM module reports a non-correctable error and the address point to an unused place.&lt;/P&gt;&lt;P&gt;Below is the debug window message.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The attach is my project's .ld file and .map&amp;nbsp; file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/102408iB7E59215ECBD7D99/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The address 0x1FFFEB40 is not a address I have used.&lt;/P&gt;&lt;P&gt;And I have used the function "Debug_Watchpoint_And_Trace" (config as below) could catch the problem when the error occurred. I think it means nothing have accessed this address include pc pointer and all registers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I know a case that no registers and pc pointer&amp;nbsp;use the address but the address is accessed.That is when the cpu load the assembly , not only the current used instruction but also more instructions which will be used later will be load to "fifo". That means there is a case that an address is not used now but it has been accessed(this issue would cause a ERM error too, while the code is running in ram, but I have been resolve it).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So if there have the possible of the ERM error's reporting is because of the address in ram is pre-loaded in some case which is similar with the pre-load the assembly instructions? Or another issue cause the ERM error's reporting?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The attach files is my project's compiling map file and the ld file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Feb 2020 10:26:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-ERM-module-issue/m-p/995005#M5866</guid>
      <dc:creator>chongrui_lu</dc:creator>
      <dc:date>2020-02-20T10:26:40Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 ERM module issue</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-ERM-module-issue/m-p/995006#M5867</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/chongrui.lu@harman.com"&gt;chongrui.lu@harman.com&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;I understand that it is executing a function in the SRAM_L region when this ECC error is detected.&lt;/P&gt;&lt;P&gt;It could be because the code from the fault address is prefetched.&lt;/P&gt;&lt;P&gt;If the code was executed, you would see a fault exception not only&amp;nbsp;this ERM error.&lt;/P&gt;&lt;P&gt;Where is the SRAM function located?&lt;/P&gt;&lt;P&gt;If you can reproduce this error, please check if the&amp;nbsp;application initializes the whole SRAM during the startup.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;BR, Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Feb 2020 13:16:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-ERM-module-issue/m-p/995006#M5867</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2020-02-24T13:16:19Z</dc:date>
    </item>
  </channel>
</rss>