<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPUART receive function not working (LPUART_DRV_ReceiveData) with SDK 3.0.0 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/LPUART-receive-function-not-working-LPUART-DRV-ReceiveData-with/m-p/994877#M5861</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jorge,&lt;/P&gt;&lt;P&gt;          Thanks for the reply.I used LPUART2 module because initially&lt;/P&gt;&lt;P&gt;LPUART was not working properly with LPUART 1 using eval board(this is with&lt;/P&gt;&lt;P&gt;respect to normal echo example Iam telling without using processor&lt;/P&gt;&lt;P&gt;expert.).So i used LPUART2 instance with processor expert also. Are you&lt;/P&gt;&lt;P&gt;able to receive back whatever you are sending from serial terminal when you&lt;/P&gt;&lt;P&gt;tested?Also is there any issue if I use LPUART2 instance?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 01 Nov 2019 04:53:17 GMT</pubDate>
    <dc:creator>anoop_radhakris</dc:creator>
    <dc:date>2019-11-01T04:53:17Z</dc:date>
    <item>
      <title>LPUART receive function not working (LPUART_DRV_ReceiveData) with SDK 3.0.0</title>
      <link>https://community.nxp.com/t5/S32K/LPUART-receive-function-not-working-LPUART-DRV-ReceiveData-with/m-p/994877#M5861</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jorge,&lt;/P&gt;&lt;P&gt;          Thanks for the reply.I used LPUART2 module because initially&lt;/P&gt;&lt;P&gt;LPUART was not working properly with LPUART 1 using eval board(this is with&lt;/P&gt;&lt;P&gt;respect to normal echo example Iam telling without using processor&lt;/P&gt;&lt;P&gt;expert.).So i used LPUART2 instance with processor expert also. Are you&lt;/P&gt;&lt;P&gt;able to receive back whatever you are sending from serial terminal when you&lt;/P&gt;&lt;P&gt;tested?Also is there any issue if I use LPUART2 instance?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Nov 2019 04:53:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPUART-receive-function-not-working-LPUART-DRV-ReceiveData-with/m-p/994877#M5861</guid>
      <dc:creator>anoop_radhakris</dc:creator>
      <dc:date>2019-11-01T04:53:17Z</dc:date>
    </item>
    <item>
      <title>Re: LPUART receive function not working (LPUART_DRV_ReceiveData) with SDK 3.0.0</title>
      <link>https://community.nxp.com/t5/S32K/LPUART-receive-function-not-working-LPUART-DRV-ReceiveData-with/m-p/994878#M5862</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Anoop,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I checked the examples for LPUART for the S32K144 available in S32DS (with and without PE) and everything works well.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, I'm able to use LPUART2 instance without any issue.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm not sure what is not working on your side.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Nov 2019 14:58:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPUART-receive-function-not-working-LPUART-DRV-ReceiveData-with/m-p/994878#M5862</guid>
      <dc:creator>dianabatrlova</dc:creator>
      <dc:date>2019-11-06T14:58:23Z</dc:date>
    </item>
  </channel>
</rss>