<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Using HW_average,HW_Comparison and getting channel result with help of ADC PAL</title>
    <link>https://community.nxp.com/t5/S32K/Using-HW-average-HW-Comparison-and-getting-channel-result-with/m-p/993777#M5854</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;Petr,&lt;/P&gt;&lt;P&gt;Thanks for the reply&amp;nbsp;&lt;/P&gt;&lt;P&gt;As per use case&amp;nbsp;we want to use grouping feature as well as&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;HW average/compare, what will be the best suited approach.&lt;/SPAN&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 Jan 2020 06:30:52 GMT</pubDate>
    <dc:creator>shubhendu_shukl</dc:creator>
    <dc:date>2020-01-27T06:30:52Z</dc:date>
    <item>
      <title>Using HW_average,HW_Comparison and getting channel result with help of ADC PAL</title>
      <link>https://community.nxp.com/t5/S32K/Using-HW-average-HW-Comparison-and-getting-channel-result-with/m-p/993775#M5852</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are using multiple ADC inputs in our customized board, Now to read the values from All these pins we are planning to use ADC Pal, But for higher accuracy we need to integrate HW_Average and HW_Comparison&amp;nbsp;&lt;/P&gt;&lt;P&gt;how can we use the same with ADC Pal example&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jan 2020 09:37:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Using-HW-average-HW-Comparison-and-getting-channel-result-with/m-p/993775#M5852</guid>
      <dc:creator>shubhendu_shukl</dc:creator>
      <dc:date>2020-01-23T09:37:40Z</dc:date>
    </item>
    <item>
      <title>Re: Using HW_average,HW_Comparison and getting channel result with help of ADC PAL</title>
      <link>https://community.nxp.com/t5/S32K/Using-HW-average-HW-Comparison-and-getting-channel-result-with/m-p/993776#M5853</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the ADC&amp;nbsp;PAL driver does not provide setting for HW average/compare functions. The ADC driver offers both the average&amp;nbsp;and compare functionality.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jan 2020 06:07:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Using-HW-average-HW-Comparison-and-getting-channel-result-with/m-p/993776#M5853</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2020-01-27T06:07:32Z</dc:date>
    </item>
    <item>
      <title>Re: Using HW_average,HW_Comparison and getting channel result with help of ADC PAL</title>
      <link>https://community.nxp.com/t5/S32K/Using-HW-average-HW-Comparison-and-getting-channel-result-with/m-p/993777#M5854</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;Petr,&lt;/P&gt;&lt;P&gt;Thanks for the reply&amp;nbsp;&lt;/P&gt;&lt;P&gt;As per use case&amp;nbsp;we want to use grouping feature as well as&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;HW average/compare, what will be the best suited approach.&lt;/SPAN&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jan 2020 06:30:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Using-HW-average-HW-Comparison-and-getting-channel-result-with/m-p/993777#M5854</guid>
      <dc:creator>shubhendu_shukl</dc:creator>
      <dc:date>2020-01-27T06:30:52Z</dc:date>
    </item>
    <item>
      <title>Re: Using HW_average,HW_Comparison and getting channel result with help of ADC PAL</title>
      <link>https://community.nxp.com/t5/S32K/Using-HW-average-HW-Comparison-and-getting-channel-result-with/m-p/993778#M5855</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To do a conversion of multiple channels it is ideally to use HW triggering through a PDB module, while back to back mechanism can be done too.&amp;nbsp;&lt;BR /&gt;You can refer to example posted on comunity;&amp;nbsp;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-343295"&gt;https://community.nxp.com/docs/DOC-343295&lt;/A&gt;&lt;/P&gt;&lt;P&gt;If HW average/compare is enabled, it is active for all the channels measured, which extends a conversion time, so&amp;nbsp;trigger time generation must be properly configured.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jan 2020 08:43:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Using-HW-average-HW-Comparison-and-getting-channel-result-with/m-p/993778#M5855</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2020-01-29T08:43:38Z</dc:date>
    </item>
  </channel>
</rss>