<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K116 CAN Clock Tolerance</title>
    <link>https://community.nxp.com/t5/S32K/S32K116-CAN-Clock-Tolerance/m-p/2363695#M58502</link>
    <description>&lt;P&gt;The datasheet of S32K116 motioned clock tolerance is 48M +/- 1%. But one of our customers requires 0.5% tolerance on CAN clock.&lt;BR /&gt;I have seen similar discussion recommending external oscillator:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K/CAN-FD-clocked-by-FIRC/m-p/879378#M4033" target="_blank"&gt;https://community.nxp.com/t5/S32K/CAN-FD-clocked-by-FIRC/m-p/879378#M4033&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;However, we prefer not to use&amp;nbsp;external oscillator. and i am wondering&lt;BR /&gt;-- if there is any calibration or Trim we can apply one of these internal Clock and eventually achieve 0.5% tolerance on CAN?&lt;BR /&gt;-- if there is any&amp;nbsp;variant of S32K116 with better/custom factory trim and achieve 0.5% tolerance?&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 12 May 2026 03:27:18 GMT</pubDate>
    <dc:creator>Sid_Zhou</dc:creator>
    <dc:date>2026-05-12T03:27:18Z</dc:date>
    <item>
      <title>S32K116 CAN Clock Tolerance</title>
      <link>https://community.nxp.com/t5/S32K/S32K116-CAN-Clock-Tolerance/m-p/2363695#M58502</link>
      <description>&lt;P&gt;The datasheet of S32K116 motioned clock tolerance is 48M +/- 1%. But one of our customers requires 0.5% tolerance on CAN clock.&lt;BR /&gt;I have seen similar discussion recommending external oscillator:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K/CAN-FD-clocked-by-FIRC/m-p/879378#M4033" target="_blank"&gt;https://community.nxp.com/t5/S32K/CAN-FD-clocked-by-FIRC/m-p/879378#M4033&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;However, we prefer not to use&amp;nbsp;external oscillator. and i am wondering&lt;BR /&gt;-- if there is any calibration or Trim we can apply one of these internal Clock and eventually achieve 0.5% tolerance on CAN?&lt;BR /&gt;-- if there is any&amp;nbsp;variant of S32K116 with better/custom factory trim and achieve 0.5% tolerance?&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 12 May 2026 03:27:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K116-CAN-Clock-Tolerance/m-p/2363695#M58502</guid>
      <dc:creator>Sid_Zhou</dc:creator>
      <dc:date>2026-05-12T03:27:18Z</dc:date>
    </item>
    <item>
      <title>Re: S32K116 CAN Clock Tolerance</title>
      <link>https://community.nxp.com/t5/S32K/S32K116-CAN-Clock-Tolerance/m-p/2363807#M58508</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;DIV&gt;On S32K116, CAN clock accuracy of ±0.5% &lt;STRONG&gt;cannot be guaranteed&lt;/STRONG&gt; using internal oscillators alone. The internal FIRC is specified at ±1% over voltage and temperature, and no runtime calibration or factory trim variant exists to improve this. To meet ±0.5% reliably and compliantly, an external oscillator or crystal via SOSC is required, to be used as CAN PE clock.&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;BR, Petr&lt;/DIV&gt;</description>
      <pubDate>Tue, 12 May 2026 07:14:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K116-CAN-Clock-Tolerance/m-p/2363807#M58508</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2026-05-12T07:14:13Z</dc:date>
    </item>
  </channel>
</rss>