<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32N55 CHIP.SecureChallenge() returns &amp;quot;device unlock failed&amp;quot; on OEM_OPEN LC</title>
    <link>https://community.nxp.com/t5/S32K/S32N55-CHIP-SecureChallenge-returns-quot-device-unlock-failed/m-p/2363370#M58482</link>
    <description>&lt;P&gt;Thank you for your response, Chenyin.&lt;/P&gt;&lt;P&gt;I understand that under OEM_OPEN LC, debug access is granted&lt;BR /&gt;by default without authentication.&lt;/P&gt;&lt;P&gt;However, I have a follow-up question:&lt;/P&gt;&lt;P&gt;CHIP.SecureChallenge(0) is supposed to read UID[63:0],&lt;BR /&gt;which should be accessible regardless of LC state.&lt;BR /&gt;But it returns "device unlock failed" even under OEM_OPEN.&lt;/P&gt;&lt;P&gt;Is this expected behavior?&lt;BR /&gt;If so, how should we read the UID (128-bit) and Challenge&lt;BR /&gt;(256-bit) for future OEM_CLOSED testing without&lt;BR /&gt;CHIP.SecureChallenge()?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
    <pubDate>Mon, 11 May 2026 10:50:08 GMT</pubDate>
    <dc:creator>EddiePark</dc:creator>
    <dc:date>2026-05-11T10:50:08Z</dc:date>
    <item>
      <title>S32N55 CHIP.SecureChallenge() returns "device unlock failed" on OEM_OPEN LC</title>
      <link>https://community.nxp.com/t5/S32K/S32N55-CHIP-SecureChallenge-returns-quot-device-unlock-failed/m-p/2363092#M58462</link>
      <description>&lt;P&gt;Environment:&lt;BR /&gt;- Device: S32N55 EVB&lt;BR /&gt;- HSE FW: 1.0.24.0&lt;BR /&gt;- GrayVIP: 1.0.22&lt;BR /&gt;- T32: [버전]&lt;BR /&gt;- LC: OEM_OPEN&lt;/P&gt;&lt;P&gt;Symptoms:&lt;BR /&gt;ADKP (HSE_OTP_FOEM_ADKP_ATTR_ID, 52U) is programmed (confirmed via&lt;BR /&gt;GetAttribute → SHA3_384 hash returned).&lt;BR /&gt;However, CHIP.SecureChallenge(0) in Lauterbach T32 returns&lt;BR /&gt;"device unlock failed".&lt;/P&gt;&lt;P&gt;CMM sequence:&lt;BR /&gt;SYStem.Down&lt;BR /&gt;SYStem.CPU S32N55-M7-FSS&lt;BR /&gt;SYStem.CONFIG DEBUGPORTTYPE JTAG&lt;BR /&gt;SYStem.Option DUALPORT ON&lt;BR /&gt;SYStem.MemAccess DAP&lt;BR /&gt;SYStem.JtagClock 10MHz&lt;BR /&gt;SYStem.Mode PREPARE&lt;BR /&gt;&amp;amp;UID0=FORMAT.HEX(16.,CHIP.SecureChallenge(0)) ← fails here&lt;/P&gt;&lt;P&gt;Questions:&lt;BR /&gt;1. Is CHIP.SecureChallenge() expected to work on OEM_OPEN LC,&lt;BR /&gt;or is OEM_CLOSED required?&lt;/P&gt;&lt;P&gt;2. Is MCK (HSE_OTP_FOEM_MCK_ATTR_ID, 51U) required before&lt;BR /&gt;CHIP.SecureChallenge() can generate a Challenge?&lt;/P&gt;&lt;P&gt;3. What is the exact prerequisite for CHIP.SecureChallenge()&lt;BR /&gt;to return a valid Challenge on S32N55?&lt;/P&gt;&lt;P&gt;4. Is volkano.exe (SDAF package) required for Response calculation,&lt;BR /&gt;or can it be implemented with AES-ECB using ADKP directly?&lt;/P&gt;</description>
      <pubDate>Mon, 11 May 2026 03:42:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32N55-CHIP-SecureChallenge-returns-quot-device-unlock-failed/m-p/2363092#M58462</guid>
      <dc:creator>EddiePark</dc:creator>
      <dc:date>2026-05-11T03:42:33Z</dc:date>
    </item>
    <item>
      <title>Re: S32N55 CHIP.SecureChallenge() returns "device unlock failed" on OEM_OPEN LC</title>
      <link>https://community.nxp.com/t5/S32K/S32N55-CHIP-SecureChallenge-returns-quot-device-unlock-failed/m-p/2363189#M58466</link>
      <description>&lt;P&gt;Additional questions:&lt;/P&gt;&lt;P&gt;5. CHIP.SecureChallenge(0) reads UID[63:0] according to T32 documentation.&lt;BR /&gt;The fact that even UID reading fails with "device unlock failed" suggests&lt;BR /&gt;SDC-600 handshake itself is not completing.&lt;BR /&gt;Does T32 CHIP.SecureChallenge() automatically handle the SDC-600&lt;BR /&gt;Init sequence (LPH2RA_FLAG, IDR_FLAG, Protocol ID) and&lt;BR /&gt;Start Command (0x00, 0xEB, 0xCD, 0x5D)?&lt;BR /&gt;Or does this need to be triggered manually before calling&lt;BR /&gt;CHIP.SecureChallenge()?&lt;/P&gt;&lt;P&gt;6. Is ODAK (HSE_OTP_FOEM_ODAK_ATTR_ID, 54U) required in addition to ADKP&lt;BR /&gt;for Challenge-Response mode?&lt;BR /&gt;Currently only ADKP (52U) is programmed.&lt;/P&gt;&lt;P&gt;7. What OTP keys are required to be programmed before&lt;BR /&gt;CHIP.SecureChallenge() can return a valid Challenge on S32N55?&lt;BR /&gt;(MCK=51U, ADKP=52U, ODAK=54U?)&lt;/P&gt;</description>
      <pubDate>Mon, 11 May 2026 07:01:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32N55-CHIP-SecureChallenge-returns-quot-device-unlock-failed/m-p/2363189#M58466</guid>
      <dc:creator>EddiePark</dc:creator>
      <dc:date>2026-05-11T07:01:53Z</dc:date>
    </item>
    <item>
      <title>Re: S32N55 CHIP.SecureChallenge() returns "device unlock failed" on OEM_OPEN LC</title>
      <link>https://community.nxp.com/t5/S32K/S32N55-CHIP-SecureChallenge-returns-quot-device-unlock-failed/m-p/2363248#M58476</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243574"&gt;@EddiePark&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your post.&lt;/P&gt;
&lt;P&gt;1. Regarding with the questions raised, as what my colleague had mentioned in your another thread,&amp;nbsp; in the NXP community we can only help you with fully launched products, but S32N55 is still a pre-production chip,&amp;nbsp; I suggest contacting your NXP representative/distributor for closer help for urgency topics.&lt;/P&gt;
&lt;P&gt;2. Since currently there is still no S32N board in community, I suggest posting new threads in &lt;A href="https://community.nxp.com/t5/S32G/bd-p/S32G" target="_self"&gt;S32G&lt;/A&gt; instead of this board next time.&lt;/P&gt;
&lt;P&gt;3. I will try investigating and collecting some inputs internally for your issues if possible, but it may take some time and may not fully solve your issue, I apologize in advance.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Mon, 11 May 2026 08:46:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32N55-CHIP-SecureChallenge-returns-quot-device-unlock-failed/m-p/2363248#M58476</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2026-05-11T08:46:35Z</dc:date>
    </item>
    <item>
      <title>Re: S32N55 CHIP.SecureChallenge() returns "device unlock failed" on OEM_OPEN LC</title>
      <link>https://community.nxp.com/t5/S32K/S32N55-CHIP-SecureChallenge-returns-quot-device-unlock-failed/m-p/2363365#M58481</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243574"&gt;@EddiePark&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Under&amp;nbsp;&lt;SPAN&gt;OEM_OPEN LC, the FSS is open to the debug capabilities by default, secure debug is not needed for accessing FSS.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Chenyin&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 11 May 2026 10:44:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32N55-CHIP-SecureChallenge-returns-quot-device-unlock-failed/m-p/2363365#M58481</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2026-05-11T10:44:35Z</dc:date>
    </item>
    <item>
      <title>Re: S32N55 CHIP.SecureChallenge() returns "device unlock failed" on OEM_OPEN LC</title>
      <link>https://community.nxp.com/t5/S32K/S32N55-CHIP-SecureChallenge-returns-quot-device-unlock-failed/m-p/2363370#M58482</link>
      <description>&lt;P&gt;Thank you for your response, Chenyin.&lt;/P&gt;&lt;P&gt;I understand that under OEM_OPEN LC, debug access is granted&lt;BR /&gt;by default without authentication.&lt;/P&gt;&lt;P&gt;However, I have a follow-up question:&lt;/P&gt;&lt;P&gt;CHIP.SecureChallenge(0) is supposed to read UID[63:0],&lt;BR /&gt;which should be accessible regardless of LC state.&lt;BR /&gt;But it returns "device unlock failed" even under OEM_OPEN.&lt;/P&gt;&lt;P&gt;Is this expected behavior?&lt;BR /&gt;If so, how should we read the UID (128-bit) and Challenge&lt;BR /&gt;(256-bit) for future OEM_CLOSED testing without&lt;BR /&gt;CHIP.SecureChallenge()?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Mon, 11 May 2026 10:50:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32N55-CHIP-SecureChallenge-returns-quot-device-unlock-failed/m-p/2363370#M58482</guid>
      <dc:creator>EddiePark</dc:creator>
      <dc:date>2026-05-11T10:50:08Z</dc:date>
    </item>
    <item>
      <title>Re: S32N55 CHIP.SecureChallenge() returns "device unlock failed" on OEM_OPEN LC</title>
      <link>https://community.nxp.com/t5/S32K/S32N55-CHIP-SecureChallenge-returns-quot-device-unlock-failed/m-p/2364967#M58554</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243574"&gt;@EddiePark&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your reply.&lt;/P&gt;
&lt;P&gt;1.&amp;nbsp;Currently, from available S32N55 documentation released, I feel sorry that it is still lacking of details for the secure debug topic, thus we may not provide accurate feedback in short period.&lt;/P&gt;
&lt;P&gt;2. As what we had mentioned, the S32N55 is still in pre-production phase, it is currently not targeted supporting it via the community, I suggest directly contacting your NXP representative for further support.&lt;/P&gt;
&lt;P&gt;Truly apologize for your inconvenience.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 13 May 2026 14:51:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32N55-CHIP-SecureChallenge-returns-quot-device-unlock-failed/m-p/2364967#M58554</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2026-05-13T14:51:09Z</dc:date>
    </item>
  </channel>
</rss>