<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックNeed full RTD source package and decouple example for FRDM-S32K344 — India developer</title>
    <link>https://community.nxp.com/t5/S32K/Need-full-RTD-source-package-and-decouple-example-for-FRDM/m-p/2363098#M58464</link>
    <description>&lt;P&gt;Hello NXP team,&lt;/P&gt;&lt;P&gt;I have FRDM-S32K344 with S32DS 3.6.6. I have a working&lt;BR /&gt;dual-core project on S32K328 with RTD 7.0.0 and want to&lt;BR /&gt;use S32K344 in decoupled dual-core mode.&lt;/P&gt;&lt;P&gt;Two requests:&lt;/P&gt;&lt;P&gt;1. Full RTD source package for S32K344 — Package Manager&lt;BR /&gt;only shows DS_updatesite.zip, not full source tree.&lt;/P&gt;&lt;P&gt;2. Access to Example_S32K344_decouple_RTD400_Ip_C40_DS35&lt;BR /&gt;project to write UTEST DCF record (LOCKSTEP_EN=0).&lt;/P&gt;&lt;P&gt;My UTEST address 0x1B000780 is blank and verified ready.&lt;/P&gt;&lt;P&gt;Board: FRDM-S32K344&lt;BR /&gt;IDE: S32DS 3.6.6&lt;BR /&gt;Debugger: PE Micro onboard&lt;BR /&gt;Location: India&lt;/P&gt;&lt;P&gt;Please advise or connect me to India FAE.&lt;BR /&gt;Thank you.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;RTD/LOCKSTEP/NXPS32K344&lt;/P&gt;&lt;P class=""&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 11 May 2026 04:25:48 GMT</pubDate>
    <dc:creator>ashwin95raghavan</dc:creator>
    <dc:date>2026-05-11T04:25:48Z</dc:date>
    <item>
      <title>Need full RTD source package and decouple example for FRDM-S32K344 — India developer</title>
      <link>https://community.nxp.com/t5/S32K/Need-full-RTD-source-package-and-decouple-example-for-FRDM/m-p/2363098#M58464</link>
      <description>&lt;P&gt;Hello NXP team,&lt;/P&gt;&lt;P&gt;I have FRDM-S32K344 with S32DS 3.6.6. I have a working&lt;BR /&gt;dual-core project on S32K328 with RTD 7.0.0 and want to&lt;BR /&gt;use S32K344 in decoupled dual-core mode.&lt;/P&gt;&lt;P&gt;Two requests:&lt;/P&gt;&lt;P&gt;1. Full RTD source package for S32K344 — Package Manager&lt;BR /&gt;only shows DS_updatesite.zip, not full source tree.&lt;/P&gt;&lt;P&gt;2. Access to Example_S32K344_decouple_RTD400_Ip_C40_DS35&lt;BR /&gt;project to write UTEST DCF record (LOCKSTEP_EN=0).&lt;/P&gt;&lt;P&gt;My UTEST address 0x1B000780 is blank and verified ready.&lt;/P&gt;&lt;P&gt;Board: FRDM-S32K344&lt;BR /&gt;IDE: S32DS 3.6.6&lt;BR /&gt;Debugger: PE Micro onboard&lt;BR /&gt;Location: India&lt;/P&gt;&lt;P&gt;Please advise or connect me to India FAE.&lt;BR /&gt;Thank you.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;RTD/LOCKSTEP/NXPS32K344&lt;/P&gt;&lt;P class=""&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 11 May 2026 04:25:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Need-full-RTD-source-package-and-decouple-example-for-FRDM/m-p/2363098#M58464</guid>
      <dc:creator>ashwin95raghavan</dc:creator>
      <dc:date>2026-05-11T04:25:48Z</dc:date>
    </item>
    <item>
      <title>Re: Need full RTD source package and decouple example for FRDM-S32K344 — India developer</title>
      <link>https://community.nxp.com/t5/S32K/Need-full-RTD-source-package-and-decouple-example-for-FRDM/m-p/2363209#M58471</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;DIV&gt;1) once you add/install RTD updatesite within S32DS, the RTD source code is visible within S32DS installation folder, e.g.&amp;nbsp;&lt;BR clear="none" /&gt;c:\NXP\S32DS.3.6.5_RTD700\S32DS\software\PlatformSDK_S32K3\RTD&lt;BR clear="none" /&gt;Also you have a possibility to download standalone RTD version. Within NXP Automotive Package Manager if you selecetd whole RTD package it would contain *.exe file as well (e.g.&amp;nbsp;SW32K3_S32M27x_RTD_R23-11_7.0.0_QLP03_D2512.exe , which is a standalone installation, usable for Tresos usage etc.&lt;BR clear="none" /&gt;This is also available from your SW library account&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-STDSW-D" shape="rect" target="_blank"&gt;https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-STDSW-D&lt;/A&gt;&lt;/DIV&gt;
&lt;DIV&gt;Go to Automotive SW - S32K3/S32M27x - Real-Time Drivers for Cortex-M&amp;nbsp; and select the RTD version you need.&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;2) The project you mentioned can be downloaded directly from&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-decouple-RTD400-Ip-C40-DS35/ta-p/1866329" shape="rect" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-decouple-RTD400-Ip-C40-DS35/ta-p/1866329&lt;/A&gt;&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;BR, Petr&lt;/DIV&gt;</description>
      <pubDate>Mon, 11 May 2026 07:31:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Need-full-RTD-source-package-and-decouple-example-for-FRDM/m-p/2363209#M58471</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2026-05-11T07:31:12Z</dc:date>
    </item>
  </channel>
</rss>