<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K394 BIST/STCU reset behavior after normal self-test completion in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K394-BIST-STCU-reset-behavior-after-normal-self-test/m-p/2360267#M58356</link>
    <description>&lt;P&gt;Hello Team.&lt;/P&gt;&lt;P&gt;We are using S32K394 with S32K3 SAF 1.0.5 and reviewing S32K3_SAF_BIST_UM Rev. 11.0.&lt;/P&gt;&lt;P&gt;From the SAF BIST documentation, we understand that:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Normal online/runtime BIST execution ends with functional reset.&lt;/LI&gt;&lt;LI&gt;Destructive reset is mentioned only for configured unrecoverable LBIST/MBIST fault cases&lt;/LI&gt;&lt;LI&gt;We do find an explicit documentation that normal STCU self-test completion can be configured to use RESET_b and cause POR / destructive reset. [Reference: S32K396RM.pdf, Rev 4 11/2024 -&amp;nbsp; Section : 29.2.3.2 Chip action after reset event - NOTE]&lt;/LI&gt;&lt;LI&gt;Could you please advise/clarify&amp;nbsp;which registers / fields / module configuration are used to configure RESET_b assertion?&lt;BR /&gt;We would appreciate a register-level or reference-manual-level pointer for S32K394.&lt;/LI&gt;&lt;/OL&gt;</description>
    <pubDate>Tue, 05 May 2026 04:15:31 GMT</pubDate>
    <dc:creator>SBalaji</dc:creator>
    <dc:date>2026-05-05T04:15:31Z</dc:date>
    <item>
      <title>S32K394 BIST/STCU reset behavior after normal self-test completion</title>
      <link>https://community.nxp.com/t5/S32K/S32K394-BIST-STCU-reset-behavior-after-normal-self-test/m-p/2360267#M58356</link>
      <description>&lt;P&gt;Hello Team.&lt;/P&gt;&lt;P&gt;We are using S32K394 with S32K3 SAF 1.0.5 and reviewing S32K3_SAF_BIST_UM Rev. 11.0.&lt;/P&gt;&lt;P&gt;From the SAF BIST documentation, we understand that:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Normal online/runtime BIST execution ends with functional reset.&lt;/LI&gt;&lt;LI&gt;Destructive reset is mentioned only for configured unrecoverable LBIST/MBIST fault cases&lt;/LI&gt;&lt;LI&gt;We do find an explicit documentation that normal STCU self-test completion can be configured to use RESET_b and cause POR / destructive reset. [Reference: S32K396RM.pdf, Rev 4 11/2024 -&amp;nbsp; Section : 29.2.3.2 Chip action after reset event - NOTE]&lt;/LI&gt;&lt;LI&gt;Could you please advise/clarify&amp;nbsp;which registers / fields / module configuration are used to configure RESET_b assertion?&lt;BR /&gt;We would appreciate a register-level or reference-manual-level pointer for S32K394.&lt;/LI&gt;&lt;/OL&gt;</description>
      <pubDate>Tue, 05 May 2026 04:15:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K394-BIST-STCU-reset-behavior-after-normal-self-test/m-p/2360267#M58356</guid>
      <dc:creator>SBalaji</dc:creator>
      <dc:date>2026-05-05T04:15:31Z</dc:date>
    </item>
    <item>
      <title>Re: S32K394 BIST/STCU reset behavior after normal self-test completion</title>
      <link>https://community.nxp.com/t5/S32K/S32K394-BIST-STCU-reset-behavior-after-normal-self-test/m-p/2360325#M58358</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/260349"&gt;@SBalaji&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1: Yes.&lt;/P&gt;
&lt;P&gt;2: Yes.&lt;/P&gt;
&lt;P&gt;3: Even when the reset_b assertion is enabled, it remains a functional reset, not a destructive reset or power‑on reset (POR).&lt;BR /&gt;All functional resets assert reset_b. The only exception is STCU2 ST_DONE, where this behavior is configurable.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1777968407058.png" style="width: 616px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/384317i31AC5FF84A5B029A/image-dimensions/616x561?v=v2" width="616" height="561" role="button" title="danielmartynek_0-1777968407058.png" alt="danielmartynek_0-1777968407058.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;4: Refer to the Reference manual,&amp;nbsp;&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Section 49.1.13 Self-Test programming sequence.&amp;nbsp;Step 5. Configure ERCTRL[ERASSERT] register bit in MC_RGM to achieve desired behaviour of Reset Pin as documented in Reset Section and Pad States Section.&lt;/LI&gt;
&lt;LI&gt;Table 22. SELFTEST(MC_RGM.ERCTRL[ERASSERT] configured as 1).&lt;/LI&gt;
&lt;LI&gt;29.10.1 Reset pin control during self-test&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 05 May 2026 08:13:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K394-BIST-STCU-reset-behavior-after-normal-self-test/m-p/2360325#M58358</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2026-05-05T08:13:25Z</dc:date>
    </item>
  </channel>
</rss>