<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: [URGENT] S32N55 Secure Debug Implementation - SDAF volkano.exe Issue and HSE2 FW RM Request in S32K</title>
    <link>https://community.nxp.com/t5/S32K/URGENT-S32N55-Secure-Debug-Implementation-SDAF-volkano-exe-Issue/m-p/2360243#M58355</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243574"&gt;@EddiePark&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Thanks for reaching out to us. I understand the urgency of your questions, and thus I want to make it clear that I won't be able to help you with everything regarding the S32N55, since it is a pre-production chip,&amp;nbsp; in the NXP community we can only help you with fully launched products. You can contact your NXP representative/distributor for closer help on this topic.&lt;/P&gt;
&lt;P&gt;Furthermore, I do not know the procedure to secure debug with TRACE32, I can share this &lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Secure-Debugging-from-S32DS-IDE-with-S32-Debugger-and-S32/ta-p/1964462" target="_blank"&gt;post&lt;/A&gt;&amp;nbsp;which describes how to do it with S32 Design Studio. However, for the S32N55 the steps may differ a bit since it is quite a newer chip, I cannot offer you definitive information as I mentioned above. You can also check this other &lt;A href="https://community.nxp.com/t5/S32G/How-can-I-find-the-page-that-includes-the-Secure-Keys-Registry/td-p/2140833" target="_blank"&gt;conversation&lt;/A&gt;, which has a similar topic.&lt;/P&gt;
&lt;P&gt;For better support on how to do it in TRACE32 I would recommend you to contact&amp;nbsp;&lt;A href="https://www.lauterbach.com/" target="_blank"&gt;lauterbach&lt;/A&gt;&amp;nbsp;in parallel.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please note that I cannot test the ADKP functionality since I am not authorized to modify any OTP configuration of the test boards we have.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Let me know if I can help you with anything else.&lt;/P&gt;</description>
    <pubDate>Mon, 04 May 2026 23:40:55 GMT</pubDate>
    <dc:creator>alejandro_e</dc:creator>
    <dc:date>2026-05-04T23:40:55Z</dc:date>
    <item>
      <title>[URGENT] S32N55 Secure Debug Implementation - SDAF volkano.exe Issue and HSE2 FW RM Request</title>
      <link>https://community.nxp.com/t5/S32K/URGENT-S32N55-Secure-Debug-Implementation-SDAF-volkano-exe-Issue/m-p/2359843#M58329</link>
      <description>&lt;P&gt;Dear NXP Support Team,&lt;/P&gt;&lt;P&gt;I am currently working on a customer project involving the S32N55 platform with a tight delivery schedule, and I urgently need your support on the following topics related to Secure Debug implementation. Your prompt response would be greatly appreciated.&lt;/P&gt;&lt;P&gt;---&lt;/P&gt;&lt;P&gt;[Topic 1] SDAF volkano.exe - Unable to load crypto library&lt;/P&gt;&lt;P&gt;Environment:&lt;BR /&gt;- TRACE32 Package: trace32_n_2026_04_000189919_nxp_s32n55_conf&lt;BR /&gt;- SDAF Version: 1.1.0 RTM&lt;BR /&gt;- Host OS: Windows 10 x64&lt;/P&gt;&lt;P&gt;Symptom:&lt;BR /&gt;All volkano.exe commands (e.g. generate_wrapkey, discover) fail with the following error:&lt;BR /&gt;**error** Unable to load crypto library&lt;/P&gt;&lt;P&gt;Steps already taken:&lt;BR /&gt;- Copied libeay32.dll and ssleay32.dll (OpenSSL 1.0.2s Win64) into the sdaf folder&lt;BR /&gt;- Confirmed VC++ 2017 Redistributable (14.16.27052) is already installed&lt;BR /&gt;- Confirmed volkano.exe is a 64-bit binary&lt;/P&gt;&lt;P&gt;Questions:&lt;BR /&gt;1. Are there any additional DLLs or middleware required to run volkano.exe?&lt;BR /&gt;2. Is a physical SmartCard and card reader mandatory for volkano.exe to function?&lt;BR /&gt;3. If a SmartCard is required, could you please advise on the compatible SmartCard model and the middleware installation procedure?&lt;BR /&gt;4. Is there a way to use volkano.exe in local storage mode without a SmartCard for development purposes?&lt;/P&gt;&lt;P&gt;---&lt;/P&gt;&lt;P&gt;[Topic 2] Secure Debug Implementation - ADKP Provisioning and Challenge/Response Flow&lt;/P&gt;&lt;P&gt;For our customer project, we are implementing Secure Debug for the S32N55 in OEM_CLOSED lifecycle using the FSS debug domain with Challenge/Response (C/R) authorization mode (HSE_OWNER_DEBUG_AUTH_CR, default mode).&lt;/P&gt;&lt;P&gt;Our current understanding of the flow is as follows:&lt;BR /&gt;1. Provision ADKP (32-byte symmetric secret) into OTP fuses via HSE2 SetAttribute (HSE_OTP_FOEM_ADKP_ATTR_ID)&lt;BR /&gt;2. Advance lifecycle to OEM_CLOSED&lt;BR /&gt;3. At debug time, TRACE32 reads UID and 256-bit Challenge via CHIP.SecureChallenge()&lt;BR /&gt;4. volkano.exe computes the Response using the provisioned ADKP&lt;BR /&gt;5. TRACE32 connects via SYStem.Option KEYCODE&lt;/P&gt;&lt;P&gt;Questions:&lt;BR /&gt;1. Could you confirm that the above flow is correct for S32N55 FSS Secure Debug?&lt;BR /&gt;2. What is the exact cryptographic algorithm used to compute the C/R Response from the ADKP and Challenge? (e.g. AES-ECB)&lt;BR /&gt;3. Is there any additional configuration required beyond ADKP provisioning (e.g. FOEM_Debug_Auth_Mode fuse setting) to enable C/R mode?&lt;BR /&gt;4. Is the MCK (HSE_OTP_FOEM_MCK_ATTR_ID) required for Secure Debug?&lt;BR /&gt;5. Could you please share the HSE2 Firmware Reference Manual for S32N55, specifically the chapter covering the Secure Debug Challenge/Response algorithm and ADKP provisioning details? We understand that the C/R Response calculation algorithm may be documented in the HSE-H/M RM (as in the case of S32G2), but we are not certain whether the same algorithm applies to S32N55 HSE2. Clarification on this point would also be greatly appreciated.&lt;/P&gt;&lt;P&gt;This is a critical blocker for our customer project delivery. We would greatly appreciate a response at your earliest convenience.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Eddie Park&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 03 May 2026 06:42:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/URGENT-S32N55-Secure-Debug-Implementation-SDAF-volkano-exe-Issue/m-p/2359843#M58329</guid>
      <dc:creator>EddiePark</dc:creator>
      <dc:date>2026-05-03T06:42:22Z</dc:date>
    </item>
    <item>
      <title>Re: [URGENT] S32N55 Secure Debug Implementation - SDAF volkano.exe Issue and HSE2 FW RM Request</title>
      <link>https://community.nxp.com/t5/S32K/URGENT-S32N55-Secure-Debug-Implementation-SDAF-volkano-exe-Issue/m-p/2360243#M58355</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243574"&gt;@EddiePark&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Thanks for reaching out to us. I understand the urgency of your questions, and thus I want to make it clear that I won't be able to help you with everything regarding the S32N55, since it is a pre-production chip,&amp;nbsp; in the NXP community we can only help you with fully launched products. You can contact your NXP representative/distributor for closer help on this topic.&lt;/P&gt;
&lt;P&gt;Furthermore, I do not know the procedure to secure debug with TRACE32, I can share this &lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Secure-Debugging-from-S32DS-IDE-with-S32-Debugger-and-S32/ta-p/1964462" target="_blank"&gt;post&lt;/A&gt;&amp;nbsp;which describes how to do it with S32 Design Studio. However, for the S32N55 the steps may differ a bit since it is quite a newer chip, I cannot offer you definitive information as I mentioned above. You can also check this other &lt;A href="https://community.nxp.com/t5/S32G/How-can-I-find-the-page-that-includes-the-Secure-Keys-Registry/td-p/2140833" target="_blank"&gt;conversation&lt;/A&gt;, which has a similar topic.&lt;/P&gt;
&lt;P&gt;For better support on how to do it in TRACE32 I would recommend you to contact&amp;nbsp;&lt;A href="https://www.lauterbach.com/" target="_blank"&gt;lauterbach&lt;/A&gt;&amp;nbsp;in parallel.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please note that I cannot test the ADKP functionality since I am not authorized to modify any OTP configuration of the test boards we have.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Let me know if I can help you with anything else.&lt;/P&gt;</description>
      <pubDate>Mon, 04 May 2026 23:40:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/URGENT-S32N55-Secure-Debug-Implementation-SDAF-volkano-exe-Issue/m-p/2360243#M58355</guid>
      <dc:creator>alejandro_e</dc:creator>
      <dc:date>2026-05-04T23:40:55Z</dc:date>
    </item>
  </channel>
</rss>