<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Inquiry regarding AUTOSAR OS/RTE availability for S32K144 and recommended Hybrid workflow</title>
    <link>https://community.nxp.com/t5/S32K/Inquiry-regarding-AUTOSAR-OS-RTE-availability-for-S32K144-and/m-p/2359122#M58297</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am currently working on an AUTOSAR-based project using the &lt;STRONG&gt;S32K144EVB&lt;/STRONG&gt;. I am utilizing the &lt;STRONG&gt;RTD (Real-Time Drivers)&lt;/STRONG&gt; provided by NXP through &lt;STRONG&gt;EB tresos&lt;/STRONG&gt; for MCAL-level configurations.&lt;/P&gt;&lt;P&gt;However, I have noticed that while RTD is provided, a standard-compliant &lt;STRONG&gt;AUTOSAR OS and RTE&lt;/STRONG&gt; do not seem to be included in the free software package. Instead, FreeRTOS is often used in the examples.&lt;/P&gt;&lt;P&gt;I would like to clarify the following two points:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;1. Availability of Free/Open-source AUTOSAR OS and RTE:&lt;/STRONG&gt; Does NXP provide a standard-compliant AUTOSAR OS and RTE for the S32K1 series as a free or open-source package? If not, are there any recommended third-party open-source alternatives that are compatible with NXP RTD?&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;2. Recommended Workflow for "AUTOSAR-inspired" Architecture:&lt;/STRONG&gt; If a standard OS/RTE is not provided for free, is the following "Hybrid" approach considered the best practice for prototyping?&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;MCAL: Using NXP RTD (configured via EB tresos).&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;OS: Integrating FreeRTOS manually within S32DS.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;RTE/Service Layer: Manually implementing an abstraction layer (RTE-like interfaces and SchM critical sections).&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;If there is a more efficient or recommended way to achieve a "standard-like" architecture without a commercial stack, please let me know.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;jipoman&lt;/P&gt;</description>
    <pubDate>Thu, 30 Apr 2026 09:05:16 GMT</pubDate>
    <dc:creator>jipoman</dc:creator>
    <dc:date>2026-04-30T09:05:16Z</dc:date>
    <item>
      <title>Inquiry regarding AUTOSAR OS/RTE availability for S32K144 and recommended Hybrid workflow</title>
      <link>https://community.nxp.com/t5/S32K/Inquiry-regarding-AUTOSAR-OS-RTE-availability-for-S32K144-and/m-p/2359122#M58297</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am currently working on an AUTOSAR-based project using the &lt;STRONG&gt;S32K144EVB&lt;/STRONG&gt;. I am utilizing the &lt;STRONG&gt;RTD (Real-Time Drivers)&lt;/STRONG&gt; provided by NXP through &lt;STRONG&gt;EB tresos&lt;/STRONG&gt; for MCAL-level configurations.&lt;/P&gt;&lt;P&gt;However, I have noticed that while RTD is provided, a standard-compliant &lt;STRONG&gt;AUTOSAR OS and RTE&lt;/STRONG&gt; do not seem to be included in the free software package. Instead, FreeRTOS is often used in the examples.&lt;/P&gt;&lt;P&gt;I would like to clarify the following two points:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;1. Availability of Free/Open-source AUTOSAR OS and RTE:&lt;/STRONG&gt; Does NXP provide a standard-compliant AUTOSAR OS and RTE for the S32K1 series as a free or open-source package? If not, are there any recommended third-party open-source alternatives that are compatible with NXP RTD?&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;2. Recommended Workflow for "AUTOSAR-inspired" Architecture:&lt;/STRONG&gt; If a standard OS/RTE is not provided for free, is the following "Hybrid" approach considered the best practice for prototyping?&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;MCAL: Using NXP RTD (configured via EB tresos).&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;OS: Integrating FreeRTOS manually within S32DS.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;RTE/Service Layer: Manually implementing an abstraction layer (RTE-like interfaces and SchM critical sections).&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;If there is a more efficient or recommended way to achieve a "standard-like" architecture without a commercial stack, please let me know.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;jipoman&lt;/P&gt;</description>
      <pubDate>Thu, 30 Apr 2026 09:05:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Inquiry-regarding-AUTOSAR-OS-RTE-availability-for-S32K144-and/m-p/2359122#M58297</guid>
      <dc:creator>jipoman</dc:creator>
      <dc:date>2026-04-30T09:05:16Z</dc:date>
    </item>
    <item>
      <title>Re: Inquiry regarding AUTOSAR OS/RTE availability for S32K144 and recommended Hybrid workflow</title>
      <link>https://community.nxp.com/t5/S32K/Inquiry-regarding-AUTOSAR-OS-RTE-availability-for-S32K144-and/m-p/2359475#M58317</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/261369"&gt;@jipoman&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The RTE module included in the RTD package is provided as a support stub only and does not support configuration. It is intended solely for testing purposes.&lt;/P&gt;
&lt;P&gt;For a fully functional and configurable RTE solution, you will need to obtain a compatible package from a third‑party vendor, such as Elektrobit (EB), Vector, or other AUTOSAR tool providers.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
      <pubDate>Thu, 30 Apr 2026 20:58:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Inquiry-regarding-AUTOSAR-OS-RTE-availability-for-S32K144-and/m-p/2359475#M58317</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2026-04-30T20:58:33Z</dc:date>
    </item>
  </channel>
</rss>