<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Segger Jlink compatibility for Secure Debug/ Lifecycle updates of S32K324 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Segger-Jlink-compatibility-for-Secure-Debug-Lifecycle-updates-of/m-p/2359010#M58291</link>
    <description>&lt;P&gt;HSE_DEMOAPP_S32K3XX only works with T32 but mentioned HSE examples are code based and may run with any debugger.&lt;/P&gt;
&lt;P&gt;There are also examples S32K344_HSE_FW_INSTALL and S32K344_HSE_FW_UPDATE in HSE examples package:&lt;BR /&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=S32K3_HSE_DemoExamples" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=S32K3_HSE_DemoExamples&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;It is basically the same functionality ported to the code debugger independent&lt;/P&gt;
&lt;P&gt;Quoting "c:\NXP\S32K3_HSE_DemoExamples_1_0_0\S32K3_HSE_DemoExamples\Readme.md":&lt;BR /&gt;'The purpose of this project is to provide different use-case scenarios and examples to showcase the capabilities of the HSE FW in different devices. This is a port of the well known HSE DEMO APP which requires T32 Lauterbach in order to work, in this case we are working with PEmicro and Design Studio as this two tools work well with eachother allowing debugging directly using Design Studio IDE.'&lt;/P&gt;</description>
    <pubDate>Thu, 30 Apr 2026 06:50:27 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2026-04-30T06:50:27Z</dc:date>
    <item>
      <title>Segger Jlink compatibility for Secure Debug/ Lifecycle updates of S32K324</title>
      <link>https://community.nxp.com/t5/S32K/Segger-Jlink-compatibility-for-Secure-Debug-Lifecycle-updates-of/m-p/2354735#M58122</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are using S32K3 and now want to install HSE FW. Can you confirm if Segger JLink supports secure Debug using Challenge/Response authentication. If not then what are the other options?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Anil&lt;/P&gt;</description>
      <pubDate>Wed, 22 Apr 2026 13:25:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Segger-Jlink-compatibility-for-Secure-Debug-Lifecycle-updates-of/m-p/2354735#M58122</guid>
      <dc:creator>anilsp31PA</dc:creator>
      <dc:date>2026-04-22T13:25:42Z</dc:date>
    </item>
    <item>
      <title>Re: Segger Jlink compatibility for Secure Debug/ Lifecycle updates of S32K324</title>
      <link>https://community.nxp.com/t5/S32K/Segger-Jlink-compatibility-for-Secure-Debug-Lifecycle-updates-of/m-p/2355197#M58139</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229232"&gt;@anilsp31PA&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;This is a screenshot from Segger's web&amp;nbsp;&lt;A href="https://kb.segger.com/NXP_S32K3xx" target="_blank"&gt;https://kb.segger.com/NXP_S32K3xx&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="lukaszadrapa_0-1776943251999.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/383328iE90F018EDB0574C8/image-size/medium?v=v2&amp;amp;px=400" role="button" title="lukaszadrapa_0-1776943251999.png" alt="lukaszadrapa_0-1776943251999.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;lukaszadrapa_0-1776943251999.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;So, it's not supported.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;An option is either Pemicro or Lauterbach.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;In case of Pemicro, please read following article:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.pemicro.com/learningcenter/contents.cfm?content_id=82" target="_blank"&gt;https://www.pemicro.com/learningcenter/contents.cfm?content_id=82&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;In case of Lauterbach, there are some resources in HSE DemoApp (can be downloaded from the same place as HSE firmware).&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;You can take a look at scripts in HSE DemoApp at path like:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;c:\NXP\HSE_DEMOAPP_S32K358_0_2_55_0\demo_security_installer\scripts\&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;See the files:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;debug_App_ADKP.py&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;debug_authorization.cmm&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;adkp_key_input.txt&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;... or contact Lauterbach directly for help.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Lukas&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 23 Apr 2026 11:26:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Segger-Jlink-compatibility-for-Secure-Debug-Lifecycle-updates-of/m-p/2355197#M58139</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2026-04-23T11:26:12Z</dc:date>
    </item>
    <item>
      <title>Re: Segger Jlink compatibility for Secure Debug/ Lifecycle updates of S32K324</title>
      <link>https://community.nxp.com/t5/S32K/Segger-Jlink-compatibility-for-Secure-Debug-Lifecycle-updates-of/m-p/2356681#M58224</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;In continuing further on same topic. The Demo App source and documentation contains steps for HSE_FW installation using Trace32 only. Is there a separate document and code for using PE-Micro debugger? I see documentation and .cmm scripts supported by Trace&amp;nbsp; 32 only.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Anil&lt;/P&gt;</description>
      <pubDate>Mon, 27 Apr 2026 17:15:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Segger-Jlink-compatibility-for-Secure-Debug-Lifecycle-updates-of/m-p/2356681#M58224</guid>
      <dc:creator>anilsp31PA</dc:creator>
      <dc:date>2026-04-27T17:15:33Z</dc:date>
    </item>
    <item>
      <title>Re: Segger Jlink compatibility for Secure Debug/ Lifecycle updates of S32K324</title>
      <link>https://community.nxp.com/t5/S32K/Segger-Jlink-compatibility-for-Secure-Debug-Lifecycle-updates-of/m-p/2359010#M58291</link>
      <description>&lt;P&gt;HSE_DEMOAPP_S32K3XX only works with T32 but mentioned HSE examples are code based and may run with any debugger.&lt;/P&gt;
&lt;P&gt;There are also examples S32K344_HSE_FW_INSTALL and S32K344_HSE_FW_UPDATE in HSE examples package:&lt;BR /&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=S32K3_HSE_DemoExamples" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=S32K3_HSE_DemoExamples&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;It is basically the same functionality ported to the code debugger independent&lt;/P&gt;
&lt;P&gt;Quoting "c:\NXP\S32K3_HSE_DemoExamples_1_0_0\S32K3_HSE_DemoExamples\Readme.md":&lt;BR /&gt;'The purpose of this project is to provide different use-case scenarios and examples to showcase the capabilities of the HSE FW in different devices. This is a port of the well known HSE DEMO APP which requires T32 Lauterbach in order to work, in this case we are working with PEmicro and Design Studio as this two tools work well with eachother allowing debugging directly using Design Studio IDE.'&lt;/P&gt;</description>
      <pubDate>Thu, 30 Apr 2026 06:50:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Segger-Jlink-compatibility-for-Secure-Debug-Lifecycle-updates-of/m-p/2359010#M58291</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2026-04-30T06:50:27Z</dc:date>
    </item>
  </channel>
</rss>