<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K322: protect code/data flash read/write from host debugger in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K322-protect-code-data-flash-read-write-from-host-debugger/m-p/2356886#M58230</link>
    <description>&lt;P&gt;Hello Danial,&lt;/P&gt;&lt;P&gt;I was going through thread&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/How-to-set-S32K3-Host-debug-permanently-disabled/m-p/1564980" target="_blank"&gt;Solved: How to set S32K3_Host debug permanently disabled? - NXP Community&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I wanted to understand this and achieve and implement for my project(MCU S32K322, pFlash0 - bootloader, pFlash1-app, Core1-not used but DTCM1 is used), how/where can | start, guide me with some document, sample code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; regards&lt;/P&gt;&lt;P&gt;Abdullah A&lt;/P&gt;</description>
    <pubDate>Tue, 28 Apr 2026 04:51:04 GMT</pubDate>
    <dc:creator>AbdNxp</dc:creator>
    <dc:date>2026-04-28T04:51:04Z</dc:date>
    <item>
      <title>S32K322: protect code/data flash read/write from host debugger</title>
      <link>https://community.nxp.com/t5/S32K/S32K322-protect-code-data-flash-read-write-from-host-debugger/m-p/2356886#M58230</link>
      <description>&lt;P&gt;Hello Danial,&lt;/P&gt;&lt;P&gt;I was going through thread&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/How-to-set-S32K3-Host-debug-permanently-disabled/m-p/1564980" target="_blank"&gt;Solved: How to set S32K3_Host debug permanently disabled? - NXP Community&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I wanted to understand this and achieve and implement for my project(MCU S32K322, pFlash0 - bootloader, pFlash1-app, Core1-not used but DTCM1 is used), how/where can | start, guide me with some document, sample code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; regards&lt;/P&gt;&lt;P&gt;Abdullah A&lt;/P&gt;</description>
      <pubDate>Tue, 28 Apr 2026 04:51:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K322-protect-code-data-flash-read-write-from-host-debugger/m-p/2356886#M58230</guid>
      <dc:creator>AbdNxp</dc:creator>
      <dc:date>2026-04-28T04:51:04Z</dc:date>
    </item>
    <item>
      <title>Re: S32K322: protect code/data flash read/write from host debugger</title>
      <link>https://community.nxp.com/t5/S32K/S32K322-protect-code-data-flash-read-write-from-host-debugger/m-p/2357720#M58243</link>
      <description>&lt;P&gt;Hello&amp;nbsp;Abdullah,&lt;/P&gt;
&lt;P&gt;There are two ways to debug‑protect an S32K3xx MCU:&lt;/P&gt;
&lt;P&gt;With HSE: Install the HSE firmware, configure Secure Debug using an Application Debug Key/Password (ADKP), and advance the device lifecycle to enforce debug protection. For further details, please create a support ticket, as the HSE firmware and documentation are available under NDA only.&lt;/P&gt;
&lt;P&gt;Without HSE: Program a customer debug password into OTP (UTEST) and then advance the lifecycle to restrict or disable debug access.&lt;/P&gt;
&lt;P&gt;The non‑HSE debug protection mechanism is explained in detail here:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Restrict-the-debug-access-with-a-password-when-HSE-is-not/ta-p/1735073" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Restrict-the-debug-access-with-a-password-when-HSE-is-not/ta-p/1735073&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;DTCM1 backdoor access can be used by CM7_0 even if CM7_1 is not used; a simple example is available here:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K314-DTCM1-Backdoor-RTD201-DS34-v3/ta-p/1689350" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K314-DTCM1-Backdoor-RTD201-DS34-v3/ta-p/1689350&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 28 Apr 2026 11:32:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K322-protect-code-data-flash-read-write-from-host-debugger/m-p/2357720#M58243</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2026-04-28T11:32:28Z</dc:date>
    </item>
  </channel>
</rss>