<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic TJA1128_SPI Write and Read in S32K</title>
    <link>https://community.nxp.com/t5/S32K/TJA1128-SPI-Write-and-Read/m-p/990958#M5812</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. I have a question about&amp;nbsp;TJA1128 read/write operation through SPI interface,&lt;BR /&gt;I have checked datasheet, but not find read operation in that.&amp;nbsp;&lt;BR /&gt;If I want to read again CRC, what is the way that I could do that?&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;2. Aside to Write operation for CRC value,&lt;BR /&gt;I should enter configuration mode,&amp;nbsp;choose 0x30h of the address and set new data value.&lt;BR /&gt;Would it be correct if I want to change CRC value in TJA1128 IC?&lt;BR /&gt;&lt;BR /&gt;Sincerely Look forward to your kindly feedback!&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/102166i8B57039819B1F97A/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/102126iE7550ABECAE97B80/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/102082i449571568AB40FBE/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Feb 2020 09:03:29 GMT</pubDate>
    <dc:creator>samchin</dc:creator>
    <dc:date>2020-02-06T09:03:29Z</dc:date>
    <item>
      <title>TJA1128_SPI Write and Read</title>
      <link>https://community.nxp.com/t5/S32K/TJA1128-SPI-Write-and-Read/m-p/990958#M5812</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. I have a question about&amp;nbsp;TJA1128 read/write operation through SPI interface,&lt;BR /&gt;I have checked datasheet, but not find read operation in that.&amp;nbsp;&lt;BR /&gt;If I want to read again CRC, what is the way that I could do that?&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;2. Aside to Write operation for CRC value,&lt;BR /&gt;I should enter configuration mode,&amp;nbsp;choose 0x30h of the address and set new data value.&lt;BR /&gt;Would it be correct if I want to change CRC value in TJA1128 IC?&lt;BR /&gt;&lt;BR /&gt;Sincerely Look forward to your kindly feedback!&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/102166i8B57039819B1F97A/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/102126iE7550ABECAE97B80/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/102082i449571568AB40FBE/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Feb 2020 09:03:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/TJA1128-SPI-Write-and-Read/m-p/990958#M5812</guid>
      <dc:creator>samchin</dc:creator>
      <dc:date>2020-02-06T09:03:29Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1128_SPI Write and Read</title>
      <link>https://community.nxp.com/t5/S32K/TJA1128-SPI-Write-and-Read/m-p/990959#M5813</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) the RO bit in the first byte distinguish between read or write operation.&amp;nbsp;The first byte contains the 7-bit address along with a RO bit (the LSB). The&amp;nbsp;RO bit must be 0 to indicate a write operation (if this bit is 1, a read operation is assumed and any data on the SDI pin is ignored).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) the calculated CRC value must be written to CRC register when SBC configuration register (address 10h to 15h) are going to be programmed. the required steps are given in device datasheet or related Application Hint document (available through Docstore, I think).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Feb 2020 12:37:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/TJA1128-SPI-Write-and-Read/m-p/990959#M5813</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2020-02-07T12:37:39Z</dc:date>
    </item>
  </channel>
</rss>