<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: How to use multiple channel of  ADC of S32K144</title>
    <link>https://community.nxp.com/t5/S32K/How-to-use-multiple-channel-of-ADC-of-S32K144/m-p/659430#M581</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Kristi,&lt;/P&gt;&lt;P&gt;There is a dedicated result register(RA,RB.. and so on) for each channel of both ADC module(ADC0,ADC1).Once the conversion is completed for a channel result is stored in corresponding result register and COCO(conversion complete) bit is set in corresponding SC1 register.Once you read the result register COCO bit will automatically clear.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Nov 2016 05:44:36 GMT</pubDate>
    <dc:creator>nitinverma</dc:creator>
    <dc:date>2016-11-17T05:44:36Z</dc:date>
    <item>
      <title>How to use multiple channel of  ADC of S32K144</title>
      <link>https://community.nxp.com/t5/S32K/How-to-use-multiple-channel-of-ADC-of-S32K144/m-p/659422#M573</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Support Team,&lt;/P&gt;&lt;P&gt;&amp;nbsp; I am working on evaluation board.I wanted to configure ADC for Multiple channel(SC1A-SC1F)for ADC1.&amp;nbsp;Software trigger is configured&amp;nbsp;as ADC trigger.I configured 1st analog input over SC1A and then successively upto SC1F.&amp;nbsp;I am initiating conversion using SC1A and getting result in ADC_RA register but not getting anything other than 0 in SC1B-SC1F.Now I i am mapping 6 input over SC1A one by one after storing ADC_RA in some variable it is exhausting to the CPU.I wanted to use 6 different channel for 6 different analog inputs.Please help to resolve the problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Sep 2016 14:57:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-use-multiple-channel-of-ADC-of-S32K144/m-p/659422#M573</guid>
      <dc:creator>nitinverma</dc:creator>
      <dc:date>2016-09-28T14:57:22Z</dc:date>
    </item>
    <item>
      <title>Re: How to use multiple channel of  ADC of S32K144</title>
      <link>https://community.nxp.com/t5/S32K/How-to-use-multiple-channel-of-ADC-of-S32K144/m-p/659423#M574</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ADC doesn’t support the sequential conversion for multiple channels using a single software trigger. Moreover just a SC1A can be used for software trigger. None of the SC1B-SC1n registers are used for software trigger operation.&lt;/P&gt;&lt;P&gt;You should involve the PDB to trigger multiple channels.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Oct 2016 12:04:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-use-multiple-channel-of-ADC-of-S32K144/m-p/659423#M574</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2016-10-03T12:04:11Z</dc:date>
    </item>
    <item>
      <title>Re: How to use multiple channel of  ADC of S32K144</title>
      <link>https://community.nxp.com/t5/S32K/How-to-use-multiple-channel-of-ADC-of-S32K144/m-p/659424#M575</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Petr.&lt;/P&gt;&lt;P&gt;I did it using PDB.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Oct 2016 05:21:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-use-multiple-channel-of-ADC-of-S32K144/m-p/659424#M575</guid>
      <dc:creator>nitinverma</dc:creator>
      <dc:date>2016-10-12T05:21:33Z</dc:date>
    </item>
    <item>
      <title>Re: How to use multiple channel of  ADC of S32K144</title>
      <link>https://community.nxp.com/t5/S32K/How-to-use-multiple-channel-of-ADC-of-S32K144/m-p/659425#M576</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to trigger ADC0 and ADC1 with the same software trigger&amp;nbsp;(using TRGMUX)&amp;nbsp;as they can measure simultaneously ?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Oct 2016 07:11:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-use-multiple-channel-of-ADC-of-S32K144/m-p/659425#M576</guid>
      <dc:creator>stabilo</dc:creator>
      <dc:date>2016-10-12T07:11:49Z</dc:date>
    </item>
    <item>
      <title>Re: How to use multiple channel of  ADC of S32K144</title>
      <link>https://community.nxp.com/t5/S32K/How-to-use-multiple-channel-of-ADC-of-S32K144/m-p/659426#M577</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey I have the same problem, can you provide a sample example for continuous&amp;nbsp;trigger of 6 ADC channels or continous trigger after a delay?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Nov 2016 15:12:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-use-multiple-channel-of-ADC-of-S32K144/m-p/659426#M577</guid>
      <dc:creator>kristyballov</dc:creator>
      <dc:date>2016-11-14T15:12:12Z</dc:date>
    </item>
    <item>
      <title>Re: How to use multiple channel of  ADC of S32K144</title>
      <link>https://community.nxp.com/t5/S32K/How-to-use-multiple-channel-of-ADC-of-S32K144/m-p/659427#M578</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Did you get a solution? I wanted help with that too...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Nov 2016 15:14:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-use-multiple-channel-of-ADC-of-S32K144/m-p/659427#M578</guid>
      <dc:creator>kristyballov</dc:creator>
      <dc:date>2016-11-14T15:14:19Z</dc:date>
    </item>
    <item>
      <title>Re: How to use multiple channel of  ADC of S32K144</title>
      <link>https://community.nxp.com/t5/S32K/How-to-use-multiple-channel-of-ADC-of-S32K144/m-p/659428#M579</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kristi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you can refer here &lt;A href="https://community.nxp.com/docs/DOC-332749"&gt;https://community.nxp.com/docs/DOC-332749&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Nov 2016 07:23:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-use-multiple-channel-of-ADC-of-S32K144/m-p/659428#M579</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2016-11-15T07:23:14Z</dc:date>
    </item>
    <item>
      <title>Re: How to use multiple channel of  ADC of S32K144</title>
      <link>https://community.nxp.com/t5/S32K/How-to-use-multiple-channel-of-ADC-of-S32K144/m-p/659429#M580</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Petr,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am confused about how converted data is written on the Register, suppose I am using 6 channels suppose PTD2,PTA3,PTA2 of ADC1 and so on for ADC0... How is the result stored in the data result register according to the channels? Please help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Nov 2016 15:45:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-use-multiple-channel-of-ADC-of-S32K144/m-p/659429#M580</guid>
      <dc:creator>kristyballov</dc:creator>
      <dc:date>2016-11-16T15:45:58Z</dc:date>
    </item>
    <item>
      <title>Re: How to use multiple channel of  ADC of S32K144</title>
      <link>https://community.nxp.com/t5/S32K/How-to-use-multiple-channel-of-ADC-of-S32K144/m-p/659430#M581</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Kristi,&lt;/P&gt;&lt;P&gt;There is a dedicated result register(RA,RB.. and so on) for each channel of both ADC module(ADC0,ADC1).Once the conversion is completed for a channel result is stored in corresponding result register and COCO(conversion complete) bit is set in corresponding SC1 register.Once you read the result register COCO bit will automatically clear.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Nov 2016 05:44:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-use-multiple-channel-of-ADC-of-S32K144/m-p/659430#M581</guid>
      <dc:creator>nitinverma</dc:creator>
      <dc:date>2016-11-17T05:44:36Z</dc:date>
    </item>
    <item>
      <title>Re: How to use multiple channel of  ADC of S32K144</title>
      <link>https://community.nxp.com/t5/S32K/How-to-use-multiple-channel-of-ADC-of-S32K144/m-p/659431#M582</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;"ADC doesn’t support the sequential conversion for multiple channels using a single software trigger."&lt;/P&gt;&lt;P&gt;Then how "continuous conversion" (SC3-&amp;gt;ADCO) is supposed to work? Is it available only for one single channel (SC1A) in case of a SW trigger? And how it works in case of HW triggers where every channel has to be triggered separately anyway?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 May 2018 14:36:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-to-use-multiple-channel-of-ADC-of-S32K144/m-p/659431#M582</guid>
      <dc:creator>kubsztal</dc:creator>
      <dc:date>2018-05-16T14:36:55Z</dc:date>
    </item>
  </channel>
</rss>