<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K144H Cannot Establish Connect in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K144H-Cannot-Establish-Connect/m-p/2352985#M58033</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/261762"&gt;@Tom77854&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes, that's correct, empty chip will reset periodically. It was discussed here, for example:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K/S32K144-New-Empty-Chip-Resets-Automatically-in-a-Certain-Period/m-p/1577829/highlight/true#M19832" target="_blank"&gt;https://community.nxp.com/t5/S32K/S32K144-New-Empty-Chip-Resets-Automatically-in-a-Certain-Period/m-p/1577829/highlight/true#M19832&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;The reset signal works as pseudo open drain. Pull-up resistor will not prevent the device to pull the reset pin down.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;So, the chip is probably not empty. If the "unsecuring" does not work, mass erase may be disabled or CSEc may be enabled. In this case, there's no way to recover.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Do you know history of the chip? If the reset is not toggling, it's not brand new device.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
    <pubDate>Fri, 17 Apr 2026 11:51:20 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2026-04-17T11:51:20Z</dc:date>
    <item>
      <title>S32K144H Cannot Establish Connect</title>
      <link>https://community.nxp.com/t5/S32K/S32K144H-Cannot-Establish-Connect/m-p/2352071#M57998</link>
      <description>&lt;P&gt;Hello, guys.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Tom77854_0-1776325401466.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/382577i63BBC92F1797575E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Tom77854_0-1776325401466.png" alt="Tom77854_0-1776325401466.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Tom77854_0-1776325401466.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;l am meeting a problem. l have got some new S32K144H chip. It did not work like this when l try to connect it with j-flash. l cannot unlock it with normal methods.&lt;/P&gt;&lt;P&gt;l have never flash it. I heard a statement，like this&amp;nbsp;&lt;STRONG&gt;&lt;SPAN&gt;"When the chip is empty, the RESET pin will exhibit periodic pulses."&amp;nbsp;&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Is it correct? l test my board, reset pin is always high. There is a 5V pull-up on reset. Is this effect my result or this is not a empty chip.&amp;nbsp; May be others ever flash it?&lt;/P&gt;</description>
      <pubDate>Thu, 16 Apr 2026 08:07:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144H-Cannot-Establish-Connect/m-p/2352071#M57998</guid>
      <dc:creator>Tom77854</dc:creator>
      <dc:date>2026-04-16T08:07:52Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144H Cannot Establish Connect</title>
      <link>https://community.nxp.com/t5/S32K/S32K144H-Cannot-Establish-Connect/m-p/2352985#M58033</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/261762"&gt;@Tom77854&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes, that's correct, empty chip will reset periodically. It was discussed here, for example:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K/S32K144-New-Empty-Chip-Resets-Automatically-in-a-Certain-Period/m-p/1577829/highlight/true#M19832" target="_blank"&gt;https://community.nxp.com/t5/S32K/S32K144-New-Empty-Chip-Resets-Automatically-in-a-Certain-Period/m-p/1577829/highlight/true#M19832&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;The reset signal works as pseudo open drain. Pull-up resistor will not prevent the device to pull the reset pin down.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;So, the chip is probably not empty. If the "unsecuring" does not work, mass erase may be disabled or CSEc may be enabled. In this case, there's no way to recover.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Do you know history of the chip? If the reset is not toggling, it's not brand new device.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Fri, 17 Apr 2026 11:51:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144H-Cannot-Establish-Connect/m-p/2352985#M58033</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2026-04-17T11:51:20Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144H Cannot Establish Connect</title>
      <link>https://community.nxp.com/t5/S32K/S32K144H-Cannot-Establish-Connect/m-p/2353567#M58072</link>
      <description>&lt;P&gt;Thanks for your answer. l will contact supplier.&lt;/P&gt;</description>
      <pubDate>Mon, 20 Apr 2026 08:19:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144H-Cannot-Establish-Connect/m-p/2353567#M58072</guid>
      <dc:creator>Tom77854</dc:creator>
      <dc:date>2026-04-20T08:19:44Z</dc:date>
    </item>
  </channel>
</rss>