<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックUnable to use the strftime function defined in time file</title>
    <link>https://community.nxp.com/t5/S32K/Unable-to-use-the-strftime-function-defined-in-time-file/m-p/989750#M5798</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Iam working on s32k144 board using s32 design studio for ARM version 2018.R1. I was trying to use the function strftime defined in time.c file for getting the current time and date. But while using strftime in project, Iam getting an error message saying undefined reference to 'strftime'.When I checked the include path, Iam able to see the path for the file already included.I have attached the code which Iam trying.So kindly help me with this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Anoop&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Feb 2020 14:58:07 GMT</pubDate>
    <dc:creator>anoop_radhakris</dc:creator>
    <dc:date>2020-02-19T14:58:07Z</dc:date>
    <item>
      <title>Unable to use the strftime function defined in time file</title>
      <link>https://community.nxp.com/t5/S32K/Unable-to-use-the-strftime-function-defined-in-time-file/m-p/989750#M5798</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Iam working on s32k144 board using s32 design studio for ARM version 2018.R1. I was trying to use the function strftime defined in time.c file for getting the current time and date. But while using strftime in project, Iam getting an error message saying undefined reference to 'strftime'.When I checked the include path, Iam able to see the path for the file already included.I have attached the code which Iam trying.So kindly help me with this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Anoop&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Feb 2020 14:58:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Unable-to-use-the-strftime-function-defined-in-time-file/m-p/989750#M5798</guid>
      <dc:creator>anoop_radhakris</dc:creator>
      <dc:date>2020-02-19T14:58:07Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to use the strftime function defined in time file</title>
      <link>https://community.nxp.com/t5/S32K/Unable-to-use-the-strftime-function-defined-in-time-file/m-p/989751#M5799</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/anoop.radhskrishnan.nair.007@gmail.com" rel="noopener noreferrer" target="_blank"&gt;anoop.radhskrishnan.nair.007@gmail.com&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried this using the example lpuart_echo_s32k144 from the SDK (if you don't have the SDK please check the following &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-343020" rel="noopener noreferrer" target="_blank"&gt;link&lt;/A&gt;), adding the following code I didn't have problems with the route:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;  time_t rawtime&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
  &lt;SPAN class="keyword token"&gt;struct&lt;/SPAN&gt; tm &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;info&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
  &lt;SPAN class="keyword token"&gt;char&lt;/SPAN&gt; buffer&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;80&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

  &lt;SPAN class="token function"&gt;time&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;rawtime &lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

  info &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;localtime&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;rawtime &lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

  &lt;SPAN class="token function"&gt;strftime&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;buffer&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;80&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;&lt;SPAN class="string token"&gt;"%x - %I:%M%p"&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; info&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

  &lt;SPAN class="token function"&gt;LPUART_DRV_SendDataBlocking&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;INST_LPUART1&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;uint8_t &lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;buffer&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;80&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; TIMEOUT&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;SPAN class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;IMG alt="pastedImage_1.png" src="https://community.nxp.com/t5/image/serverpage/image-id/102585i44997DB2CFAAA45B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think this could be related to the project settings. Be sure that you're enabling the libraries (newlib/redlib).&lt;/P&gt;&lt;P&gt;&lt;SPAN class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;IMG alt="pastedImage_2.png" src="https://community.nxp.com/t5/image/serverpage/image-id/102587iBBBF7A56BE49FBEE/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For reference, I'm using&amp;nbsp;S32 Design Studio for ARM (Version: 2.2)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Nov 2020 14:31:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Unable-to-use-the-strftime-function-defined-in-time-file/m-p/989751#M5799</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2020-11-02T14:31:30Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to use the strftime function defined in time file</title>
      <link>https://community.nxp.com/t5/S32K/Unable-to-use-the-strftime-function-defined-in-time-file/m-p/989752#M5800</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alexis,&lt;/P&gt;&lt;P&gt;Thanks for your reply.I will try this and let you know.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Anoop&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 23 Feb 2020 06:19:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Unable-to-use-the-strftime-function-defined-in-time-file/m-p/989752#M5800</guid>
      <dc:creator>anoop_radhakris</dc:creator>
      <dc:date>2020-02-23T06:19:39Z</dc:date>
    </item>
  </channel>
</rss>