<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K344 Wake-Up sequence</title>
    <link>https://community.nxp.com/t5/S32K/S32K344-Wake-Up-sequence/m-p/2350172#M57905</link>
    <description>&lt;P&gt;Hi NXP Team,&lt;/P&gt;&lt;P&gt;I am currently implementing standby (low-power) mode and wake-up functionality on the S32K344 MCU.&lt;/P&gt;&lt;P&gt;I am able to successfully enter standby mode and wake up from it. However, after wake-up, the execution always restarts from the &lt;STRONG&gt;main()&lt;/STRONG&gt; function instead of resuming from the point where it entered standby mode.&lt;/P&gt;&lt;P&gt;My requirement is to resume execution from the exact point where the MCU entered standby mode, rather than restarting from main().&lt;/P&gt;&lt;P&gt;To address this, I referred to multiple community posts and the following NXP documentation:&lt;BR /&gt;“&lt;STRONG&gt;S32K3 Low Power Management AN and demos&lt;/STRONG&gt;”&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Low-Power-Management-AN-and-demos/ta-p/1527724" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Low-Power-Management-AN-and-demos/ta-p/1527724&lt;/A&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;I also studied the example project &lt;STRONG&gt;S32K344_RTC_StandbyRAM_Wkup_S32DS_3_4_RTD_LLD_2_0&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;From this, I understand that:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Up to 32KB of Standby RAM can be configured.&lt;/LI&gt;&lt;LI&gt;This Standby RAM is retained during standby mode.&lt;/LI&gt;&lt;LI&gt;It can be used to store variables or data across standby cycles.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;However, my goal is to resume execution flow from where it left off before entering standby, not just restore variables from Standby RAM. I could not find any clear guidance or solution for this requirement.&lt;/P&gt;&lt;P&gt;Could you please clarify:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Is it possible to resume execution from the exact point where the MCU entered standby mode on S32K344?&lt;/LI&gt;&lt;LI&gt;If not, what is the recommended approach to achieve similar behavior?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Any guidance or references would be very helpful.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
    <pubDate>Mon, 13 Apr 2026 13:08:07 GMT</pubDate>
    <dc:creator>Abinandhan</dc:creator>
    <dc:date>2026-04-13T13:08:07Z</dc:date>
    <item>
      <title>S32K344 Wake-Up sequence</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-Wake-Up-sequence/m-p/2350172#M57905</link>
      <description>&lt;P&gt;Hi NXP Team,&lt;/P&gt;&lt;P&gt;I am currently implementing standby (low-power) mode and wake-up functionality on the S32K344 MCU.&lt;/P&gt;&lt;P&gt;I am able to successfully enter standby mode and wake up from it. However, after wake-up, the execution always restarts from the &lt;STRONG&gt;main()&lt;/STRONG&gt; function instead of resuming from the point where it entered standby mode.&lt;/P&gt;&lt;P&gt;My requirement is to resume execution from the exact point where the MCU entered standby mode, rather than restarting from main().&lt;/P&gt;&lt;P&gt;To address this, I referred to multiple community posts and the following NXP documentation:&lt;BR /&gt;“&lt;STRONG&gt;S32K3 Low Power Management AN and demos&lt;/STRONG&gt;”&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Low-Power-Management-AN-and-demos/ta-p/1527724" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Low-Power-Management-AN-and-demos/ta-p/1527724&lt;/A&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;I also studied the example project &lt;STRONG&gt;S32K344_RTC_StandbyRAM_Wkup_S32DS_3_4_RTD_LLD_2_0&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;From this, I understand that:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Up to 32KB of Standby RAM can be configured.&lt;/LI&gt;&lt;LI&gt;This Standby RAM is retained during standby mode.&lt;/LI&gt;&lt;LI&gt;It can be used to store variables or data across standby cycles.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;However, my goal is to resume execution flow from where it left off before entering standby, not just restore variables from Standby RAM. I could not find any clear guidance or solution for this requirement.&lt;/P&gt;&lt;P&gt;Could you please clarify:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Is it possible to resume execution from the exact point where the MCU entered standby mode on S32K344?&lt;/LI&gt;&lt;LI&gt;If not, what is the recommended approach to achieve similar behavior?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Any guidance or references would be very helpful.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Mon, 13 Apr 2026 13:08:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-Wake-Up-sequence/m-p/2350172#M57905</guid>
      <dc:creator>Abinandhan</dc:creator>
      <dc:date>2026-04-13T13:08:07Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 Wake-Up sequence</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-Wake-Up-sequence/m-p/2350325#M57915</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/249590"&gt;@Abinandhan&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Low power mode transition works somewhat different in the K3 family, compared to the K1. S32K3 will always perform a reset sequence after waking up:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Julin_AragnM_0-1776111898879.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/382169i99FE1D60704C1C22/image-size/large?v=v2&amp;amp;px=999" role="button" title="Julin_AragnM_0-1776111898879.png" alt="Julin_AragnM_0-1776111898879.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;You can still send only the core to standby with WFI, though. For example, the &lt;STRONG&gt;CORE_STANDBY&lt;/STRONG&gt; mode in 'Power' driver does this:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/exiting-core-standby-mode-using-CAN-wakeup/td-p/1768231" target="_blank"&gt;exiting core standby mode using CAN wakeup - NXP Community&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Keep in mind that CORE_STANDBY only stops clock for the core, it has nothing to do with STANDBY mode. CORE_STANDBY mode can be useful for some use cases where all peripherals need to be up and only core is stopped for a while.&lt;/P&gt;
&lt;P&gt;STANDBY mode should be used instead to reduce current consumption.&lt;/P&gt;
&lt;P&gt;Alternatively, the K3 also supports a 'Fast Wakeup', where the MCU will enter a user-defined boot address, which you can use for time-critical issues. It is still recommended to jump to Reset_Handler after the user-defined address, in order to fully initialize the system.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Julin_AragnM_2-1776112111624.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/382171iBFC24D821C9FA87A/image-size/large?v=v2&amp;amp;px=999" role="button" title="Julin_AragnM_2-1776112111624.png" alt="Julin_AragnM_2-1776112111624.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
      <pubDate>Mon, 13 Apr 2026 20:29:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-Wake-Up-sequence/m-p/2350325#M57915</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2026-04-13T20:29:16Z</dc:date>
    </item>
  </channel>
</rss>