<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MC33772 &amp;amp; MC33774A based on RTD6.0.0 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/MC33772-amp-MC33774A-based-on-RTD6-0-0/m-p/2349035#M57843</link>
    <description>&lt;P&gt;BMS Gen2 SDK does not contain MC33774 anymore, if customer want the integration, please take774 sw component from Gen1 SDK release 1.0.3_P01. &amp;nbsp;Please refer to the Mixing_GEN2_and_GEN1_BMS_Drivers.docx I sent you.&lt;/P&gt;</description>
    <pubDate>Fri, 10 Apr 2026 08:17:17 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2026-04-10T08:17:17Z</dc:date>
    <item>
      <title>MC33772 &amp; MC33774A based on RTD6.0.0</title>
      <link>https://community.nxp.com/t5/S32K/MC33772-amp-MC33774A-based-on-RTD6-0-0/m-p/2338223#M57486</link>
      <description>&lt;P&gt;Hi:&lt;/P&gt;&lt;P&gt;Our environment : S32K358 + MC33772C + MC33774A&lt;/P&gt;&lt;P&gt;software : S32DS3.5 + RTD 3.0.0 + BMS SDK gen1&amp;nbsp; --&amp;gt; upgrade to S32DS3.6.4 + RTD 6.0.0 + BMS SDK gen2&lt;/P&gt;&lt;P&gt;Currently, we want to upgrade our RTD version from 3.0.0 to 6.0.0, NXP also release BMS SDK gen2 based on RTD6.0.0 that we can use. But I found that there are no MC33772 MC33774 MCAL driver in BMS SDK gen2. I also can't install SDK gen1 and gen2 in the same IDE.&lt;/P&gt;&lt;P&gt;I want to ask that if autosar version is same with RTD6.0.0, can I move 33772 or 33774 related MCAL driver and source code which generated from&amp;nbsp;RTD 3.0.0 environment into RTD 6.0.0 environment? Is it possible can work or is there any other way?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;BR, BillWen&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 24 Mar 2026 08:00:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MC33772-amp-MC33774A-based-on-RTD6-0-0/m-p/2338223#M57486</guid>
      <dc:creator>BillWen</dc:creator>
      <dc:date>2026-03-24T08:00:44Z</dc:date>
    </item>
    <item>
      <title>Re: MC33772 &amp; MC33774A based on RTD6.0.0</title>
      <link>https://community.nxp.com/t5/S32K/MC33772-amp-MC33774A-based-on-RTD6-0-0/m-p/2338950#M57523</link>
      <description>&lt;P&gt;Hi&amp;nbsp;BillWen,&lt;/P&gt;
&lt;P&gt;This is the question I am not able to answer on our support level. I have to escalate it to the BMS SW team. I am very sorry it will take unpredictable delay. As soon as I have answer I'll send it to you.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;/P&gt;</description>
      <pubDate>Wed, 25 Mar 2026 03:57:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MC33772-amp-MC33774A-based-on-RTD6-0-0/m-p/2338950#M57523</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2026-03-25T03:57:25Z</dc:date>
    </item>
    <item>
      <title>Re: MC33772 &amp; MC33774A based on RTD6.0.0</title>
      <link>https://community.nxp.com/t5/S32K/MC33772-amp-MC33774A-based-on-RTD6-0-0/m-p/2338981#M57525</link>
      <description>Hi Robin:&lt;BR /&gt;Really thanks for your help. Waiting for your good news.&lt;BR /&gt;In the meantime, I will try to integrate MC33772C and MC33774A Mcal driver from BMS SDK GEN1.&lt;BR /&gt;&lt;BR /&gt;Thanks&lt;BR /&gt;BR, BillWen</description>
      <pubDate>Wed, 25 Mar 2026 05:57:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MC33772-amp-MC33774A-based-on-RTD6-0-0/m-p/2338981#M57525</guid>
      <dc:creator>BillWen</dc:creator>
      <dc:date>2026-03-25T05:57:22Z</dc:date>
    </item>
    <item>
      <title>Re: MC33772 &amp; MC33774A based on RTD6.0.0</title>
      <link>https://community.nxp.com/t5/S32K/MC33772-amp-MC33774A-based-on-RTD6-0-0/m-p/2349035#M57843</link>
      <description>&lt;P&gt;BMS Gen2 SDK does not contain MC33774 anymore, if customer want the integration, please take774 sw component from Gen1 SDK release 1.0.3_P01. &amp;nbsp;Please refer to the Mixing_GEN2_and_GEN1_BMS_Drivers.docx I sent you.&lt;/P&gt;</description>
      <pubDate>Fri, 10 Apr 2026 08:17:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MC33772-amp-MC33774A-based-on-RTD6-0-0/m-p/2349035#M57843</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2026-04-10T08:17:17Z</dc:date>
    </item>
  </channel>
</rss>