<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: secure flash on s32k58</title>
    <link>https://community.nxp.com/t5/S32K/secure-flash-on-s32k58/m-p/2348760#M57819</link>
    <description>&lt;P&gt;dear Lukas&lt;/P&gt;&lt;P&gt;Thanks for your reply~&lt;/P&gt;&lt;P&gt;Is there example source code for HSE? It seems that HSE has the capability to generate and import keys, so it would be helpful to have example code and related references&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Bryan&lt;/P&gt;</description>
    <pubDate>Fri, 10 Apr 2026 01:47:29 GMT</pubDate>
    <dc:creator>bryan_hong</dc:creator>
    <dc:date>2026-04-10T01:47:29Z</dc:date>
    <item>
      <title>secure flash on s32k58</title>
      <link>https://community.nxp.com/t5/S32K/secure-flash-on-s32k58/m-p/2347930#M57804</link>
      <description>&lt;P&gt;dear nxp&lt;/P&gt;&lt;P&gt;Is secure flash supported on s32k358 ?&lt;/P&gt;&lt;P&gt;If so, Could you provide example for secure flash on s32k358 ?&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Bryan&lt;/P&gt;</description>
      <pubDate>Thu, 09 Apr 2026 06:30:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/secure-flash-on-s32k58/m-p/2347930#M57804</guid>
      <dc:creator>bryan_hong</dc:creator>
      <dc:date>2026-04-09T06:30:40Z</dc:date>
    </item>
    <item>
      <title>Re: secure flash on s32k58</title>
      <link>https://community.nxp.com/t5/S32K/secure-flash-on-s32k58/m-p/2348106#M57810</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/107445"&gt;@bryan_hong&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There’s no secure flash which could be used by user. When HSE firmware is installed, certain flash areas are allocated exclusively for HSE resources. These areas are sometimes called as secure flash but users can’t access it, it’s hidden for user.&lt;/P&gt;
&lt;P&gt;Users can import keys to HSE. These are stored to secure flash by HSE. This mechanism is dedicated to keys only, it is not recommended to use it for own data. This was already discussed here:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K/Store-User-Specific-value-in-the-secure-NVM/m-p/1856763/highlight/true#M34785" target="_blank"&gt;https://community.nxp.com/t5/S32K/Store-User-Specific-value-in-the-secure-NVM/m-p/1856763/highlight/true#M34785&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;As mentioned, usual approach is to encrypt data by a key stored in HSE and also use SMR services for verification of that area.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Thu, 09 Apr 2026 08:58:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/secure-flash-on-s32k58/m-p/2348106#M57810</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2026-04-09T08:58:22Z</dc:date>
    </item>
    <item>
      <title>Re: secure flash on s32k58</title>
      <link>https://community.nxp.com/t5/S32K/secure-flash-on-s32k58/m-p/2348760#M57819</link>
      <description>&lt;P&gt;dear Lukas&lt;/P&gt;&lt;P&gt;Thanks for your reply~&lt;/P&gt;&lt;P&gt;Is there example source code for HSE? It seems that HSE has the capability to generate and import keys, so it would be helpful to have example code and related references&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Bryan&lt;/P&gt;</description>
      <pubDate>Fri, 10 Apr 2026 01:47:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/secure-flash-on-s32k58/m-p/2348760#M57819</guid>
      <dc:creator>bryan_hong</dc:creator>
      <dc:date>2026-04-10T01:47:29Z</dc:date>
    </item>
    <item>
      <title>Re: secure flash on s32k58</title>
      <link>https://community.nxp.com/t5/S32K/secure-flash-on-s32k58/m-p/2349954#M57892</link>
      <description>&lt;P&gt;dear Lukas&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can we request technical support from NXP for securely operating an externally mounted flash?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Bryan&lt;/P&gt;</description>
      <pubDate>Mon, 13 Apr 2026 07:33:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/secure-flash-on-s32k58/m-p/2349954#M57892</guid>
      <dc:creator>bryan_hong</dc:creator>
      <dc:date>2026-04-13T07:33:45Z</dc:date>
    </item>
  </channel>
</rss>