<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックBootloader and debugging issues on the s32k311 chip</title>
    <link>https://community.nxp.com/t5/S32K/Bootloader-and-debugging-issues-on-the-s32k311-chip/m-p/2342064#M57597</link>
    <description>&lt;P&gt;s32ds：3.5.6&lt;BR /&gt;rtd：7.0.0&lt;/P&gt;&lt;P&gt;I encountered an issue while conducting a bootloader experiment using the s32k311 chip. I configured a regular CAN and attempted to verify that the program jumps from the BL program to the app. However, after adding the jump function, the CAN send function of the BL program stopped working. Unless I connect to J-Link for debugging, and once debugging starts, I always receive output from the debug print&lt;BR /&gt;Program received signal SIGTRAP, Trace/breakpoint trap.&lt;BR /&gt;0x20008008 in ?? ()&lt;BR /&gt;I would appreciate any possible assistance in solving this problem. Thank you&lt;/P&gt;</description>
    <pubDate>Mon, 30 Mar 2026 08:34:02 GMT</pubDate>
    <dc:creator>feixingren1</dc:creator>
    <dc:date>2026-03-30T08:34:02Z</dc:date>
    <item>
      <title>Bootloader and debugging issues on the s32k311 chip</title>
      <link>https://community.nxp.com/t5/S32K/Bootloader-and-debugging-issues-on-the-s32k311-chip/m-p/2342064#M57597</link>
      <description>&lt;P&gt;s32ds：3.5.6&lt;BR /&gt;rtd：7.0.0&lt;/P&gt;&lt;P&gt;I encountered an issue while conducting a bootloader experiment using the s32k311 chip. I configured a regular CAN and attempted to verify that the program jumps from the BL program to the app. However, after adding the jump function, the CAN send function of the BL program stopped working. Unless I connect to J-Link for debugging, and once debugging starts, I always receive output from the debug print&lt;BR /&gt;Program received signal SIGTRAP, Trace/breakpoint trap.&lt;BR /&gt;0x20008008 in ?? ()&lt;BR /&gt;I would appreciate any possible assistance in solving this problem. Thank you&lt;/P&gt;</description>
      <pubDate>Mon, 30 Mar 2026 08:34:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Bootloader-and-debugging-issues-on-the-s32k311-chip/m-p/2342064#M57597</guid>
      <dc:creator>feixingren1</dc:creator>
      <dc:date>2026-03-30T08:34:02Z</dc:date>
    </item>
    <item>
      <title>Re: Bootloader and debugging issues on the s32k311 chip</title>
      <link>https://community.nxp.com/t5/S32K/Bootloader-and-debugging-issues-on-the-s32k311-chip/m-p/2342173#M57606</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/260925"&gt;@feixingren1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I can see there’s no problem with the jump itself. But what I can see in main.c in the bootloader – you are jumping to the application without any de-initialization. This is usually the main source of troubles. I recommend:&lt;/P&gt;
&lt;OL&gt;
&lt;LI&gt;Jump to the application directly after reset. You can write some minimalist code to the startup files which will jump to the application based on some condition. Whenever the bootloader needs to jump to the application, it should just trigger software reset and then it will jump to the application right after reset before all the initialization. This is the most safe option.&lt;/LI&gt;
&lt;LI&gt;If you want to jump to the application later in the bootloader (once a lot of resources is initialized), it’s important to perform the de-initialization. Disable all interrupts (globally by the core, locally&amp;nbsp; by peripherals’ registers…), de-initialize peripherals etc.&amp;nbsp;The application either expects default reset conditions or it must be fully aware of features which are not in default reset state.&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Mon, 30 Mar 2026 12:08:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Bootloader-and-debugging-issues-on-the-s32k311-chip/m-p/2342173#M57606</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2026-03-30T12:08:25Z</dc:date>
    </item>
    <item>
      <title>Re: Bootloader and debugging issues on the s32k311 chip</title>
      <link>https://community.nxp.com/t5/S32K/Bootloader-and-debugging-issues-on-the-s32k311-chip/m-p/2342639#M57631</link>
      <description>thank you，I have already solved the problem</description>
      <pubDate>Tue, 31 Mar 2026 09:00:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Bootloader-and-debugging-issues-on-the-s32k311-chip/m-p/2342639#M57631</guid>
      <dc:creator>feixingren1</dc:creator>
      <dc:date>2026-03-31T09:00:24Z</dc:date>
    </item>
  </channel>
</rss>