<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Need help for programming S32K3X4EVB-T172 EVB by using JTAG connector in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Need-help-for-programming-S32K3X4EVB-T172-EVB-by-using-JTAG/m-p/2337591#M57449</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hello Team, &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am working on &lt;LI-PRODUCT title="S32K3X4EVB-T172" id="S32K3X4EVB-T172"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&amp;nbsp;EVB i have to program this board using JTAG connector. The Board has two connectors which has JTAG marking (J41 - 10 Pin &amp;amp; J12 - 20 Pin) from these two which connector i have use for programming and one more thing from S32K3X4EVB-T172 - Hardware User Manual i came to know that for 20 pin JTAG connector all trace signals are DISABLED as default configuration in S32K3X4EVB-T172, so does this condition plays any role in programming if yes what i have to do to make it enable&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 23 Mar 2026 11:14:57 GMT</pubDate>
    <dc:creator>MySterio_1</dc:creator>
    <dc:date>2026-03-23T11:14:57Z</dc:date>
    <item>
      <title>Need help for programming S32K3X4EVB-T172 EVB by using JTAG connector</title>
      <link>https://community.nxp.com/t5/S32K/Need-help-for-programming-S32K3X4EVB-T172-EVB-by-using-JTAG/m-p/2337591#M57449</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello Team, &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am working on &lt;LI-PRODUCT title="S32K3X4EVB-T172" id="S32K3X4EVB-T172"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&amp;nbsp;EVB i have to program this board using JTAG connector. The Board has two connectors which has JTAG marking (J41 - 10 Pin &amp;amp; J12 - 20 Pin) from these two which connector i have use for programming and one more thing from S32K3X4EVB-T172 - Hardware User Manual i came to know that for 20 pin JTAG connector all trace signals are DISABLED as default configuration in S32K3X4EVB-T172, so does this condition plays any role in programming if yes what i have to do to make it enable&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 23 Mar 2026 11:14:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Need-help-for-programming-S32K3X4EVB-T172-EVB-by-using-JTAG/m-p/2337591#M57449</guid>
      <dc:creator>MySterio_1</dc:creator>
      <dc:date>2026-03-23T11:14:57Z</dc:date>
    </item>
    <item>
      <title>Re: Need help for programming S32K3X4EVB-T172 EVB by using JTAG connector</title>
      <link>https://community.nxp.com/t5/S32K/Need-help-for-programming-S32K3X4EVB-T172-EVB-by-using-JTAG/m-p/2337853#M57466</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/260937"&gt;@MySterio_1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;As you mentioned, the S32K3X4EVB‑T172 includes two debug connectors: a 20‑pin and a 10‑pin header. The smaller 10‑pin connector is used by the on‑board K26 debugger, while the 20‑pin connector is intended for communication and debugging using an external debugger.&lt;/P&gt;
&lt;P&gt;For JTAG programming, no additional connections are required. Connecting the external debugger directly to the 20‑pin connector is sufficient for proper operation.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
      <pubDate>Mon, 23 Mar 2026 20:54:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Need-help-for-programming-S32K3X4EVB-T172-EVB-by-using-JTAG/m-p/2337853#M57466</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2026-03-23T20:54:25Z</dc:date>
    </item>
    <item>
      <title>Re: Need help for programming S32K3X4EVB-T172 EVB by using JTAG connector</title>
      <link>https://community.nxp.com/t5/S32K/Need-help-for-programming-S32K3X4EVB-T172-EVB-by-using-JTAG/m-p/2342210#M57612</link>
      <description>&lt;P&gt;Can you share more information about this 10 pin connector, is it require any specific software for programming, can we program it by using 10 pin connector from ic7 pro debugger adapter&lt;/P&gt;</description>
      <pubDate>Mon, 30 Mar 2026 13:40:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Need-help-for-programming-S32K3X4EVB-T172-EVB-by-using-JTAG/m-p/2342210#M57612</guid>
      <dc:creator>MySterio_1</dc:creator>
      <dc:date>2026-03-30T13:40:47Z</dc:date>
    </item>
    <item>
      <title>Re: Need help for programming S32K3X4EVB-T172 EVB by using JTAG connector</title>
      <link>https://community.nxp.com/t5/S32K/Need-help-for-programming-S32K3X4EVB-T172-EVB-by-using-JTAG/m-p/2342394#M57618</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/260937"&gt;@MySterio_1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Are you trying to update the OpenSDA firmware? As I mentioned earlier, the 10‑pin connector is only for the onboard debugger. If you want to program the MCU using an external debugger, you need to use the 20‑pin connector.&lt;/P&gt;
&lt;P&gt;About the adapter, I am not very familiar with that specific product, but I checked the iSYSTEM website and it looks like each adapter has a specific use. The one that matches the 20‑pin connector on the EVB should be the &lt;A href="https://www.isystem.com/downloads/user-manuals/active-probe-adapter-arm-jtag-20-pin.html" target="_blank" rel="noopener"&gt;ARM JTAG 20‑pin (2.54 mm) Adapter&lt;/A&gt;.&lt;/P&gt;</description>
      <pubDate>Mon, 30 Mar 2026 20:54:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Need-help-for-programming-S32K3X4EVB-T172-EVB-by-using-JTAG/m-p/2342394#M57618</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2026-03-30T20:54:55Z</dc:date>
    </item>
    <item>
      <title>Re: Need help for programming S32K3X4EVB-T172 EVB by using JTAG connector</title>
      <link>https://community.nxp.com/t5/S32K/Need-help-for-programming-S32K3X4EVB-T172-EVB-by-using-JTAG/m-p/2352717#M58024</link>
      <description>&lt;P&gt;Hello there,&lt;/P&gt;&lt;P&gt;I'm also currently struggling getting the board connected to an external debugger because the pin layout of J12 is not present in the S32K3X4EVB-T172 - Hardware User Manual.&lt;/P&gt;&lt;P&gt;Are you sure the&amp;nbsp;&lt;A href="https://www.isystem.com/downloads/user-manuals/active-probe-adapter-arm-jtag-20-pin.html" target="_blank"&gt;https://www.isystem.com/downloads/user-manuals/active-probe-adapter-arm-jtag-20-pin.html&lt;/A&gt;&amp;nbsp;adapter would fit?&amp;nbsp;&lt;/P&gt;&lt;P&gt;To me the connector looks too large given that there is a half-size 20-pin connector on the board (Samtec FTSH-110-01).&lt;/P&gt;&lt;P&gt;Or the rephrase this: Is J12 a MIPI20T connector (pinout as in&amp;nbsp;&lt;A href="https://repo.lauterbach.com/ad2729.html" target="_blank"&gt;https://repo.lauterbach.com/ad2729.html&lt;/A&gt;), a MIPI20D one (pinout as in&amp;nbsp;&lt;A href="https://repo.lauterbach.com/ad3770.html?product=la-3770" target="_blank"&gt;https://repo.lauterbach.com/ad3770.html?product=la-3770&lt;/A&gt;), or is this rather 1:1 (pinout as in&amp;nbsp;&lt;A href="https://repo.lauterbach.com/adidc20a.html?product=la-3255" target="_blank"&gt;https://repo.lauterbach.com/adidc20a.html?product=la-3255&lt;/A&gt;)?&lt;/P&gt;&lt;P&gt;Many thanks in advance!&lt;/P&gt;&lt;P&gt;Kind regards,&lt;BR /&gt;Gernot Gebhard&lt;/P&gt;</description>
      <pubDate>Fri, 17 Apr 2026 06:38:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Need-help-for-programming-S32K3X4EVB-T172-EVB-by-using-JTAG/m-p/2352717#M58024</guid>
      <dc:creator>GernotGebhard</dc:creator>
      <dc:date>2026-04-17T06:38:59Z</dc:date>
    </item>
    <item>
      <title>Re: Need help for programming S32K3X4EVB-T172 EVB by using JTAG connector</title>
      <link>https://community.nxp.com/t5/S32K/Need-help-for-programming-S32K3X4EVB-T172-EVB-by-using-JTAG/m-p/2361617#M58413</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;after some research I finally figured out which connector is the correct one to use with this EVB. First I measured which pins are connected to GND:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-center" image-alt="JTAG pins connected to GND" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/384601i7E637A279C279610/image-size/large?v=v2&amp;amp;px=999" role="button" title="s32k34x4evb_jtag.png" alt="JTAG pins connected to GND" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;JTAG pins connected to GND&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;This implies that the oddly numbered pins 3 to 19 are GND. This rules out the 1:1 pin layout as in&amp;nbsp;&lt;A href="https://repo.lauterbach.com/adidc20a.html?product=la-3255" target="_blank"&gt;https://repo.lauterbach.com/adidc20a.html?product=la-3255&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The EVB manual states&amp;nbsp;NOTE - JTAG – TRACE Signals&lt;/P&gt;&lt;P&gt;Due to the MCU ports used on the trace signals also are shared with other interfaces,&lt;BR /&gt;it is important to isolate these signals/interfaces for the J4-Cortex Debug D ETM&lt;BR /&gt;connector.&lt;/P&gt;&lt;P&gt;Those signals are TRACE_CLK, TRACE_D0, TRACE_D1, TRACE_D2 and TRACE_D3 which are only present in the MIPI20T layout (see&amp;nbsp;&lt;A href="https://repo.lauterbach.com/ad2729.html" target="_blank"&gt;https://repo.lauterbach.com/ad2729.html&lt;/A&gt;).&lt;/P&gt;&lt;P&gt;=&amp;gt; I've ordered the&amp;nbsp;&lt;A href="https://www.lauterbach.com/products/la-2729" target="_blank"&gt;LA-2729&lt;/A&gt;&amp;nbsp;adapter, removed the dead-pin and was able to successfully communicate with the board using Trace32.&lt;/P&gt;&lt;P&gt;Hope this helps anybody!&lt;/P&gt;</description>
      <pubDate>Thu, 07 May 2026 07:19:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Need-help-for-programming-S32K3X4EVB-T172-EVB-by-using-JTAG/m-p/2361617#M58413</guid>
      <dc:creator>GernotGebhard</dc:creator>
      <dc:date>2026-05-07T07:19:13Z</dc:date>
    </item>
  </channel>
</rss>