<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K344-WB internal memory management in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K344-WB-internal-memory-management/m-p/2334296#M57365</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/252154"&gt;@ganavi1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you are working with the RTD driver, the low‑level driver is the C40_Ip driver. For the high‑level driver, depending on the RTD version you are using, it may be either the Fls driver or the Mem_43_INFLS driver. Example codes are also included within the RTD package.&lt;/P&gt;
&lt;P&gt;Additionally, you may refer to Application Note &lt;A href="https://www.nxp.com/webapp/Download?colCode=AN13388" target="_blank" rel="noopener"&gt;AN13388: S32K3 Memories Guide&lt;/A&gt; for further guidance.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
    <pubDate>Tue, 17 Mar 2026 21:30:25 GMT</pubDate>
    <dc:creator>VaneB</dc:creator>
    <dc:date>2026-03-17T21:30:25Z</dc:date>
    <item>
      <title>S32K344-WB internal memory management</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-WB-internal-memory-management/m-p/2333944#M57358</link>
      <description>&lt;P&gt;How is internal memory accessed in the S32K344-WB? Which APIs are used, and how can data be stored in flash memory&lt;/P&gt;</description>
      <pubDate>Tue, 17 Mar 2026 09:09:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-WB-internal-memory-management/m-p/2333944#M57358</guid>
      <dc:creator>ganavi1</dc:creator>
      <dc:date>2026-03-17T09:09:51Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344-WB internal memory management</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-WB-internal-memory-management/m-p/2334296#M57365</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/252154"&gt;@ganavi1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you are working with the RTD driver, the low‑level driver is the C40_Ip driver. For the high‑level driver, depending on the RTD version you are using, it may be either the Fls driver or the Mem_43_INFLS driver. Example codes are also included within the RTD package.&lt;/P&gt;
&lt;P&gt;Additionally, you may refer to Application Note &lt;A href="https://www.nxp.com/webapp/Download?colCode=AN13388" target="_blank" rel="noopener"&gt;AN13388: S32K3 Memories Guide&lt;/A&gt; for further guidance.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
      <pubDate>Tue, 17 Mar 2026 21:30:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-WB-internal-memory-management/m-p/2334296#M57365</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2026-03-17T21:30:25Z</dc:date>
    </item>
  </channel>
</rss>