<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FLS_READ vs memcpy which one is better to use ? in S32K</title>
    <link>https://community.nxp.com/t5/S32K/FLS-READ-vs-memcpy-which-one-is-better-to-use/m-p/2334135#M57364</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I use a S32K358 with RTD 4.00_P20&lt;/P&gt;&lt;P&gt;my question is about reading data in program flash memory .&lt;/P&gt;&lt;P&gt;Do I need to use Fls_read or can I only used a memcpy ?&lt;BR /&gt;what are the cons and pro&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks you&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 17 Mar 2026 14:56:12 GMT</pubDate>
    <dc:creator>sobo</dc:creator>
    <dc:date>2026-03-17T14:56:12Z</dc:date>
    <item>
      <title>FLS_READ vs memcpy which one is better to use ?</title>
      <link>https://community.nxp.com/t5/S32K/FLS-READ-vs-memcpy-which-one-is-better-to-use/m-p/2334135#M57364</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I use a S32K358 with RTD 4.00_P20&lt;/P&gt;&lt;P&gt;my question is about reading data in program flash memory .&lt;/P&gt;&lt;P&gt;Do I need to use Fls_read or can I only used a memcpy ?&lt;BR /&gt;what are the cons and pro&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks you&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 17 Mar 2026 14:56:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FLS-READ-vs-memcpy-which-one-is-better-to-use/m-p/2334135#M57364</guid>
      <dc:creator>sobo</dc:creator>
      <dc:date>2026-03-17T14:56:12Z</dc:date>
    </item>
    <item>
      <title>Re: FLS_READ vs memcpy which one is better to use ?</title>
      <link>https://community.nxp.com/t5/S32K/FLS-READ-vs-memcpy-which-one-is-better-to-use/m-p/2335078#M57380</link>
      <description>&lt;P&gt;Use normal reads (memcpy() or direct pointer access) when you just need to read data from program flash.&lt;BR /&gt;Use Mem_43_INFLS_Read() when:&lt;/P&gt;
&lt;P&gt;Your project uses AUTOSAR MemIf / NvM / Fee&lt;BR /&gt;You need MemIf‑style asynchronous jobs and callbacks&lt;BR /&gt;You require AUTOSAR‑compliant memory access&lt;/P&gt;
&lt;P&gt;If you are not using MemIf/NvM/Fee, then Mem_43_INFLS_Read() adds unnecessary overhead — normal reads are simpler and faster.&lt;/P&gt;</description>
      <pubDate>Wed, 18 Mar 2026 10:45:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FLS-READ-vs-memcpy-which-one-is-better-to-use/m-p/2335078#M57380</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2026-03-18T10:45:35Z</dc:date>
    </item>
  </channel>
</rss>