<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: S32K3-HSE</title>
    <link>https://community.nxp.com/t5/S32K/S32K3-HSE/m-p/2333147#M57325</link>
    <description>&lt;P&gt;&lt;SPAN&gt;使用的调试器是PE，接上调试器后控制器就恢复正常了，可能是接上调试器让SBC处于调试模式，当控制器启动超过256ms后不会反复复位，然后软件就正常运行&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 16 Mar 2026 00:45:45 GMT</pubDate>
    <dc:creator>ALXY_WANG1</dc:creator>
    <dc:date>2026-03-16T00:45:45Z</dc:date>
    <item>
      <title>S32K3-HSE</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-HSE/m-p/2327536#M57155</link>
      <description>&lt;P&gt;当前我们使用S32K344设计VCU控制器，该项目首次使用HSE模块满足信息安全要求，使用的RTD为1.0.0，HSE为0.2.1.0版本。目前项目已进入小批量验证阶段，当前出现一个问题：偶发性出现上电后VCU无法启动，台架测试发现SBC供电均正常，REST引脚一直出现周期性的复位信号，周期约为200ms，拉低时长约8ms，目前怀疑大概率为上电后软件卡在HSE内核，应用核未运行起来，导致的喂狗超时复位，针对该现象是否有排查方式及相关验证方法&lt;/P&gt;</description>
      <pubDate>Fri, 06 Mar 2026 05:28:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-HSE/m-p/2327536#M57155</guid>
      <dc:creator>ALXY_WANG1</dc:creator>
      <dc:date>2026-03-06T05:28:32Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3-HSE</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-HSE/m-p/2328988#M57196</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/233082"&gt;@ALXY_WANG1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The RTD and HSE versions are quite outdated, I would consider to upgrade the software. Latest RTD version is currently 7.0.0 and HSE firmware version is currently 0.2.55.0.&lt;/P&gt;
&lt;P&gt;Is it possible to attach your debugger to the MCU? If so, could you read FES and DES registers in MC_RGM module? These registers contain the status of functional and destructive reset sources, so it should help to find the source of resets.&lt;/P&gt;
&lt;P&gt;What kind of debugger do you use? In case of Trace32, I would try to use simple script like this to attach to a running target and stop the execution in order to see the current state or where it hangs:&lt;/P&gt;
&lt;P&gt;sys.attach&lt;/P&gt;
&lt;P&gt;break&lt;/P&gt;
&lt;P&gt;To check if it is related to HSE, please provide content of HSE GPR register at 0x4039_C028 and also FSR and GSR registers from MU_0.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Mon, 09 Mar 2026 12:44:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-HSE/m-p/2328988#M57196</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2026-03-09T12:44:34Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3-HSE</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-HSE/m-p/2333147#M57325</link>
      <description>&lt;P&gt;&lt;SPAN&gt;使用的调试器是PE，接上调试器后控制器就恢复正常了，可能是接上调试器让SBC处于调试模式，当控制器启动超过256ms后不会反复复位，然后软件就正常运行&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 16 Mar 2026 00:45:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-HSE/m-p/2333147#M57325</guid>
      <dc:creator>ALXY_WANG1</dc:creator>
      <dc:date>2026-03-16T00:45:45Z</dc:date>
    </item>
  </channel>
</rss>