<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic control intterupt timer. in S32K</title>
    <link>https://community.nxp.com/t5/S32K/control-intterupt-timer/m-p/2325248#M57066</link>
    <description>&lt;P&gt;i am using s32ds, RTD version is 4.0.0. mcu is s32k314.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i use timer interrupt by PIT.&lt;/P&gt;&lt;P&gt;1. Is there a register to turn the interrupt timer on and off?&lt;/P&gt;&lt;P&gt;except by PIT function(ex,&amp;nbsp;&lt;SPAN&gt;Pit_Ip_StartChannel,&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;Pit_Ip_StopChannel)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2. i wanna make source code for control interrupt timer except PIT Function.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;like (&lt;SPAN class=""&gt;__asm&lt;/SPAN&gt; &lt;SPAN class=""&gt;volatile&lt;/SPAN&gt; (&lt;SPAN class=""&gt;"cpsid i"),&amp;nbsp;&lt;SPAN class=""&gt;__asm&lt;/SPAN&gt; &lt;SPAN class=""&gt;volatile&lt;/SPAN&gt; ("cpsie i")). but it is not work. how do i?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;thanks to help&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 03 Mar 2026 00:40:00 GMT</pubDate>
    <dc:creator>rlaxortn</dc:creator>
    <dc:date>2026-03-03T00:40:00Z</dc:date>
    <item>
      <title>control intterupt timer.</title>
      <link>https://community.nxp.com/t5/S32K/control-intterupt-timer/m-p/2325248#M57066</link>
      <description>&lt;P&gt;i am using s32ds, RTD version is 4.0.0. mcu is s32k314.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i use timer interrupt by PIT.&lt;/P&gt;&lt;P&gt;1. Is there a register to turn the interrupt timer on and off?&lt;/P&gt;&lt;P&gt;except by PIT function(ex,&amp;nbsp;&lt;SPAN&gt;Pit_Ip_StartChannel,&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;Pit_Ip_StopChannel)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2. i wanna make source code for control interrupt timer except PIT Function.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;like (&lt;SPAN class=""&gt;__asm&lt;/SPAN&gt; &lt;SPAN class=""&gt;volatile&lt;/SPAN&gt; (&lt;SPAN class=""&gt;"cpsid i"),&amp;nbsp;&lt;SPAN class=""&gt;__asm&lt;/SPAN&gt; &lt;SPAN class=""&gt;volatile&lt;/SPAN&gt; ("cpsie i")). but it is not work. how do i?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;thanks to help&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Mar 2026 00:40:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/control-intterupt-timer/m-p/2325248#M57066</guid>
      <dc:creator>rlaxortn</dc:creator>
      <dc:date>2026-03-03T00:40:00Z</dc:date>
    </item>
    <item>
      <title>Re: control intterupt timer.</title>
      <link>https://community.nxp.com/t5/S32K/control-intterupt-timer/m-p/2331839#M57303</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/249289"&gt;@rlaxortn&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can directly manipulate the PIT registers to disable the interrupt if you prefer not to use the APIs.&lt;/P&gt;
&lt;P&gt;Regarding the inline assembly instruction &lt;EM&gt;&lt;STRONG&gt;__asm volatile ("cpsid i");&lt;/STRONG&gt;&lt;/EM&gt;&amp;nbsp;On ARM Cortex‑M devices, this instruction sets the PRIMASK register, which globally disables all maskable interrupts. It does not disable an individual interrupt source.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
      <pubDate>Thu, 12 Mar 2026 20:23:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/control-intterupt-timer/m-p/2331839#M57303</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2026-03-12T20:23:22Z</dc:date>
    </item>
  </channel>
</rss>