<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K344 – Quadrature Encoder Example using LCU + eMIOS (RTD)</title>
    <link>https://community.nxp.com/t5/S32K/S32K344-Quadrature-Encoder-Example-using-LCU-eMIOS-RTD/m-p/2324364#M57032</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201913"&gt;@VaneB&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;I have a question regarding scalability.&lt;/P&gt;&lt;P&gt;From the documentation, it appears that the quadrature decoding method using &lt;STRONG&gt;LCU + eMIOS&lt;/STRONG&gt; relies on LCU LUT logic resources, which seem limited.&lt;/P&gt;&lt;P&gt;Could you please clarify:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;P&gt;How many quadrature encoders can realistically be implemented using LCU + eMIOS on the S32K344?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Is the number limited by the available LCU LUT channels?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;If LUT resources are limited, does this restrict the number of encoders that can be decoded using this hardware method?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Is there any recommended method or workaround to support &lt;STRONG&gt;up to 7 encoder channels&lt;/STRONG&gt; on this device?&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;I want to understand whether scaling to multiple encoders is feasible or if an alternative approach should be considered.&lt;/P&gt;</description>
    <pubDate>Fri, 27 Feb 2026 10:31:25 GMT</pubDate>
    <dc:creator>gayancho</dc:creator>
    <dc:date>2026-02-27T10:31:25Z</dc:date>
    <item>
      <title>S32K344 – Quadrature Encoder Example using LCU + eMIOS (RTD)</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-Quadrature-Encoder-Example-using-LCU-eMIOS-RTD/m-p/2322439#M56984</link>
      <description>&lt;P&gt;I am using S32K344 with PlatformSDK_S32K3 (RTD) and would like to implement a quadrature rotary encoder using LCU, TRGMUX, eMIOS edge counter.I could not find a complete RTD example project demonstrating full quadrature decoding (A/B phase, direction and position calculation).Could you please share a reference example project or application note compatible with RTD?&lt;/P&gt;</description>
      <pubDate>Wed, 25 Feb 2026 09:37:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-Quadrature-Encoder-Example-using-LCU-eMIOS-RTD/m-p/2322439#M56984</guid>
      <dc:creator>gayancho</dc:creator>
      <dc:date>2026-02-25T09:37:57Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 – Quadrature Encoder Example using LCU + eMIOS (RTD)</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-Quadrature-Encoder-Example-using-LCU-eMIOS-RTD/m-p/2323682#M57013</link>
      <description>&lt;P&gt;Also, could you confirm which eMIOS channel types are recommended for this use case?&lt;BR /&gt;Is it correct to use &lt;STRONG&gt;Type X or Type G channels&lt;/STRONG&gt; for pulse counting?&lt;/P&gt;</description>
      <pubDate>Thu, 26 Feb 2026 12:09:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-Quadrature-Encoder-Example-using-LCU-eMIOS-RTD/m-p/2323682#M57013</guid>
      <dc:creator>gayancho</dc:creator>
      <dc:date>2026-02-26T12:09:37Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 – Quadrature Encoder Example using LCU + eMIOS (RTD)</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-Quadrature-Encoder-Example-using-LCU-eMIOS-RTD/m-p/2323945#M57017</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/258551"&gt;@gayancho&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please refer to the &lt;A href="https://www.nxp.com/webapp/Download?colCode=AN13767" target="_blank" rel="noopener"&gt;AN13767&lt;/A&gt;: 3-phase Sensorless PMSM Motor Control Kit with S32K344 using RTD Low Level API Application Note, as well as &lt;A href="https://www.nxp.com/webapp/Download?colCode=AN13884" target="_blank" rel="noopener"&gt;AN13884&lt;/A&gt;:&amp;nbsp;3-phase Sensorless PMSM Motor Control Kit with S32K344 using RTD AUTOSAR API Application Note. These documents may serve as useful references for your application.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
      <pubDate>Thu, 26 Feb 2026 18:45:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-Quadrature-Encoder-Example-using-LCU-eMIOS-RTD/m-p/2323945#M57017</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2026-02-26T18:45:00Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 – Quadrature Encoder Example using LCU + eMIOS (RTD)</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-Quadrature-Encoder-Example-using-LCU-eMIOS-RTD/m-p/2324364#M57032</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201913"&gt;@VaneB&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;I have a question regarding scalability.&lt;/P&gt;&lt;P&gt;From the documentation, it appears that the quadrature decoding method using &lt;STRONG&gt;LCU + eMIOS&lt;/STRONG&gt; relies on LCU LUT logic resources, which seem limited.&lt;/P&gt;&lt;P&gt;Could you please clarify:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;P&gt;How many quadrature encoders can realistically be implemented using LCU + eMIOS on the S32K344?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Is the number limited by the available LCU LUT channels?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;If LUT resources are limited, does this restrict the number of encoders that can be decoded using this hardware method?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Is there any recommended method or workaround to support &lt;STRONG&gt;up to 7 encoder channels&lt;/STRONG&gt; on this device?&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;I want to understand whether scaling to multiple encoders is feasible or if an alternative approach should be considered.&lt;/P&gt;</description>
      <pubDate>Fri, 27 Feb 2026 10:31:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-Quadrature-Encoder-Example-using-LCU-eMIOS-RTD/m-p/2324364#M57032</guid>
      <dc:creator>gayancho</dc:creator>
      <dc:date>2026-02-27T10:31:25Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 – Quadrature Encoder Example using LCU + eMIOS (RTD)</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-Quadrature-Encoder-Example-using-LCU-eMIOS-RTD/m-p/2324555#M57040</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/258551"&gt;@gayancho&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes, the number of supported encoders will be limited by the LCU. Each LCU contains only three Logic Cells (LCs), and every LC provides four inputs and four outputs. Since each encoder requires its own dedicated LC, the maximum number of encoders you can connect is six. However, this number may be lower if other parts of your application also require LC resources.&lt;/P&gt;</description>
      <pubDate>Fri, 27 Feb 2026 22:46:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-Quadrature-Encoder-Example-using-LCU-eMIOS-RTD/m-p/2324555#M57040</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2026-02-27T22:46:13Z</dc:date>
    </item>
  </channel>
</rss>