<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K3 Clock Switching Flowchart in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K3-Clock-Switching-Flowchart/m-p/2322135#M56976</link>
    <description>&lt;P&gt;Yeah, I see this now. I was confused because I assumed that "software-controlled" meant that the software that I was writing controlled it, but both types of clock muxes have software initiate the control.&lt;/P&gt;</description>
    <pubDate>Tue, 24 Feb 2026 23:05:14 GMT</pubDate>
    <dc:creator>kscz</dc:creator>
    <dc:date>2026-02-24T23:05:14Z</dc:date>
    <item>
      <title>S32K3 Clock Switching Flowchart</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-Clock-Switching-Flowchart/m-p/2321542#M56956</link>
      <description>&lt;P&gt;The S32K3 reference manual section&amp;nbsp;25.4.1.2 has the following flowchart:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot From 2026-02-23 16-25-05.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/377598iF84A4AACB8AF2850/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Screenshot From 2026-02-23 16-25-05.png" alt="Screenshot From 2026-02-23 16-25-05.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; And the MUX_0_CSC register description has this diagram in section 25.5.6:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot From 2026-02-23 16-25-32.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/377599iEBC53F943BF790FE/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Screenshot From 2026-02-23 16-25-32.png" alt="Screenshot From 2026-02-23 16-25-32.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; What is "MUX_n_CSC[CG]" referring to in the register??&lt;/P&gt;</description>
      <pubDate>Tue, 24 Feb 2026 00:31:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-Clock-Switching-Flowchart/m-p/2321542#M56956</guid>
      <dc:creator>kscz</dc:creator>
      <dc:date>2026-02-24T00:31:24Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 Clock Switching Flowchart</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-Clock-Switching-Flowchart/m-p/2321853#M56969</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;DIV&gt;
&lt;P&gt;The MC_CGM provides two types of clock multiplexers:&lt;BR /&gt;- Hardware‑controlled clock multiplexers, and&lt;BR /&gt;&lt;SPAN&gt;- Software‑controlled clock multiplexers&lt;/SPAN&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Figure 124 illustrates the clock‑switching flow for software‑controlled multiplexers only, using either the synchronous/graceful clock gate bit (MUX_n_CSC[CG]) or the forced clock gate bit (MUX_n_CSC[FCG]).&lt;/P&gt;
&lt;P&gt;The CG/FCG bits are available only on software‑controlled multiplexers, such as MUX_5_CSC, MUX_6_CSC, etc.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="image.png" style="width: 536px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/377660iA3C2942A03B820F1/image-size/large?v=v2&amp;amp;px=999" role="button" title="image.png" alt="image.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;To determine whether a specific multiplexer is hardware‑ or software‑controlled, refer to the MUX_n_CSC register description in the reference manual.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;
&lt;/DIV&gt;</description>
      <pubDate>Tue, 24 Feb 2026 09:58:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-Clock-Switching-Flowchart/m-p/2321853#M56969</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2026-02-24T09:58:21Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 Clock Switching Flowchart</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-Clock-Switching-Flowchart/m-p/2322135#M56976</link>
      <description>&lt;P&gt;Yeah, I see this now. I was confused because I assumed that "software-controlled" meant that the software that I was writing controlled it, but both types of clock muxes have software initiate the control.&lt;/P&gt;</description>
      <pubDate>Tue, 24 Feb 2026 23:05:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-Clock-Switching-Flowchart/m-p/2322135#M56976</guid>
      <dc:creator>kscz</dc:creator>
      <dc:date>2026-02-24T23:05:14Z</dc:date>
    </item>
  </channel>
</rss>