<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MCAL/RTD support for ANAMUX input selection (DCMRWF1 register) in S32K</title>
    <link>https://community.nxp.com/t5/S32K/MCAL-RTD-support-for-ANAMUX-input-selection-DCMRWF1-register/m-p/2320201#M56908</link>
    <description>I was hoping that the ADC RTD would have an API to select and enable the ANAMUX functionality. But I create my own control.</description>
    <pubDate>Thu, 19 Feb 2026 11:19:40 GMT</pubDate>
    <dc:creator>DirkEtzler</dc:creator>
    <dc:date>2026-02-19T11:19:40Z</dc:date>
    <item>
      <title>MCAL/RTD support for ANAMUX input selection (DCMRWF1 register)</title>
      <link>https://community.nxp.com/t5/S32K/MCAL-RTD-support-for-ANAMUX-input-selection-DCMRWF1-register/m-p/2319465#M56885</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52961"&gt;@PetrS&lt;/a&gt;&amp;nbsp;&lt;LI-MESSAGE title="Example S32K344 PIT SWtrig ADC ANAMUX S32DS 3.6.0 RTD 6.0.0" uid="2319179" url="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-PIT-SWtrig-ADC-ANAMUX-S32DS-3-6-0-RTD-6-0-0/m-p/2319179#U2319179" discussion_style_icon_css="lia-mention-container-editor-message lia-img-icon-tkb-thread lia-fa-icon lia-fa-tkb lia-fa-thread lia-fa"&gt;&lt;/LI-MESSAGE&gt;&amp;nbsp;&amp;nbsp;Looking through the example "S32K344_PIT_SW_ADC_ANAMUX_RTD600" the input selection for the ANAMUX is done via "direct" access of the DCMRWF1 register.&lt;/P&gt;&lt;P&gt;Is/are there already an MCAL or RTD function(s) available to enable the voltage dividers for the individual internal voltages and to select the input for the analog multiplexer?&amp;nbsp; Or do I need to write my own functions to do that?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="DirkEtzler_1-1771419003698.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/377154i6287B68EC7651533/image-size/medium?v=v2&amp;amp;px=400" role="button" title="DirkEtzler_1-1771419003698.png" alt="DirkEtzler_1-1771419003698.png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 18 Feb 2026 13:05:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MCAL-RTD-support-for-ANAMUX-input-selection-DCMRWF1-register/m-p/2319465#M56885</guid>
      <dc:creator>DirkEtzler</dc:creator>
      <dc:date>2026-02-18T13:05:18Z</dc:date>
    </item>
    <item>
      <title>Re: MCAL/RTD support for ANAMUX input selection (DCMRWF1 register)</title>
      <link>https://community.nxp.com/t5/S32K/MCAL-RTD-support-for-ANAMUX-input-selection-DCMRWF1-register/m-p/2320107#M56904</link>
      <description>&lt;P&gt;Hi Dirk,&lt;/P&gt;
&lt;DIV&gt;some RTD drivers probably use DCM_GPR registers internally when needed, but there is no dedicated RTD driver&amp;nbsp;or a&amp;nbsp;&lt;SPAN&gt;public API for arbitrary DCM_GPR access.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/DIV&gt;
&lt;DIV&gt;&lt;SPAN&gt;BR, Petr&lt;/SPAN&gt;&lt;/DIV&gt;</description>
      <pubDate>Thu, 19 Feb 2026 08:41:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MCAL-RTD-support-for-ANAMUX-input-selection-DCMRWF1-register/m-p/2320107#M56904</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2026-02-19T08:41:32Z</dc:date>
    </item>
    <item>
      <title>Re: MCAL/RTD support for ANAMUX input selection (DCMRWF1 register)</title>
      <link>https://community.nxp.com/t5/S32K/MCAL-RTD-support-for-ANAMUX-input-selection-DCMRWF1-register/m-p/2320201#M56908</link>
      <description>I was hoping that the ADC RTD would have an API to select and enable the ANAMUX functionality. But I create my own control.</description>
      <pubDate>Thu, 19 Feb 2026 11:19:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/MCAL-RTD-support-for-ANAMUX-input-selection-DCMRWF1-register/m-p/2320201#M56908</guid>
      <dc:creator>DirkEtzler</dc:creator>
      <dc:date>2026-02-19T11:19:40Z</dc:date>
    </item>
  </channel>
</rss>