<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K328 – Missing Information: Switching Frequency at PMOS_CTRL (SMPS V15 Regulator)</title>
    <link>https://community.nxp.com/t5/S32K/S32K328-Missing-Information-Switching-Frequency-at-PMOS-CTRL/m-p/2316536#M56752</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/233505"&gt;@PavelL&lt;/a&gt;&amp;nbsp;,&lt;BR /&gt;&lt;BR /&gt;Thank You, this is the same Information I could find as well.&lt;BR /&gt;&lt;BR /&gt;I was still wondering if it is a Problem for the IC if the inductor is in DCM which would be the case with the recommended values and a 3V3 supply voltage.&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Markus&lt;/P&gt;</description>
    <pubDate>Wed, 11 Feb 2026 15:06:53 GMT</pubDate>
    <dc:creator>MarkusÖsterle</dc:creator>
    <dc:date>2026-02-11T15:06:53Z</dc:date>
    <item>
      <title>S32K328 – Missing Information: Switching Frequency at PMOS_CTRL (SMPS V15 Regulator)</title>
      <link>https://community.nxp.com/t5/S32K/S32K328-Missing-Information-Switching-Frequency-at-PMOS-CTRL/m-p/2316426#M56746</link>
      <description>&lt;DIV&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using the S32K328 with the SMPS option for the V15 regulator.&amp;nbsp; However, I cannot find any information in the publicly available documentation regarding the switching frequency used at the PMOS_CTRL pin.&lt;/P&gt;&lt;P&gt;Could you provide the switching frequency used by the S32K328 when driving the external PMOS in SMPS mode? This information is required for correct inductor/diode selection.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/DIV&gt;</description>
      <pubDate>Wed, 11 Feb 2026 11:44:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K328-Missing-Information-Switching-Frequency-at-PMOS-CTRL/m-p/2316426#M56746</guid>
      <dc:creator>MarkusÖsterle</dc:creator>
      <dc:date>2026-02-11T11:44:23Z</dc:date>
    </item>
    <item>
      <title>Re: S32K328 – Missing Information: Switching Frequency at PMOS_CTRL (SMPS V15 Regulator)</title>
      <link>https://community.nxp.com/t5/S32K/S32K328-Missing-Information-Switching-Frequency-at-PMOS-CTRL/m-p/2316525#M56751</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/259819"&gt;@MarkusÖsterle&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;The information about switching frequency is not available.&lt;/P&gt;
&lt;P&gt;The&amp;nbsp;S32K3xx - Hardware Design Guidelines, Rev. E2, recommends Schottky diode and&amp;nbsp;4.7uH - 5.6uH .&lt;/P&gt;
&lt;P&gt;The S32K3xx Data Sheet, Rev. 13, specifies 2A Schottky diode and typ. 4.7uH.&lt;/P&gt;
&lt;P&gt;Board S32K3x8-Q289 uses PMEG4050EP and 5.6uH, as well as S32K388EVB-Q289. Detailed part number and manufacturer can be found in the BOM file for the board.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Wed, 11 Feb 2026 14:53:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K328-Missing-Information-Switching-Frequency-at-PMOS-CTRL/m-p/2316525#M56751</guid>
      <dc:creator>PavelL</dc:creator>
      <dc:date>2026-02-11T14:53:30Z</dc:date>
    </item>
    <item>
      <title>Re: S32K328 – Missing Information: Switching Frequency at PMOS_CTRL (SMPS V15 Regulator)</title>
      <link>https://community.nxp.com/t5/S32K/S32K328-Missing-Information-Switching-Frequency-at-PMOS-CTRL/m-p/2316536#M56752</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/233505"&gt;@PavelL&lt;/a&gt;&amp;nbsp;,&lt;BR /&gt;&lt;BR /&gt;Thank You, this is the same Information I could find as well.&lt;BR /&gt;&lt;BR /&gt;I was still wondering if it is a Problem for the IC if the inductor is in DCM which would be the case with the recommended values and a 3V3 supply voltage.&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Markus&lt;/P&gt;</description>
      <pubDate>Wed, 11 Feb 2026 15:06:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K328-Missing-Information-Switching-Frequency-at-PMOS-CTRL/m-p/2316536#M56752</guid>
      <dc:creator>MarkusÖsterle</dc:creator>
      <dc:date>2026-02-11T15:06:53Z</dc:date>
    </item>
    <item>
      <title>Re: S32K328 – Missing Information: Switching Frequency at PMOS_CTRL (SMPS V15 Regulator)</title>
      <link>https://community.nxp.com/t5/S32K/S32K328-Missing-Information-Switching-Frequency-at-PMOS-CTRL/m-p/2316885#M56768</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/259819"&gt;@MarkusÖsterle&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;I’ve summarized the information here so others can follow along.&lt;/P&gt;
&lt;P&gt;Operating in DCM with the recommended component values at a 3.3 V supply is not an issue for the device.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Thu, 12 Feb 2026 07:26:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K328-Missing-Information-Switching-Frequency-at-PMOS-CTRL/m-p/2316885#M56768</guid>
      <dc:creator>PavelL</dc:creator>
      <dc:date>2026-02-12T07:26:35Z</dc:date>
    </item>
  </channel>
</rss>