<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Is S32K144 compliant to ISO 11898-1:2015 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Is-S32K144-compliant-to-ISO-11898-1-2015/m-p/2313169#M56634</link>
    <description>Hi lukaszadrapa,&lt;BR /&gt;&lt;BR /&gt;Please provide the conformance report for the S32K148 or a link to where these reports are available on the NXP site.&lt;BR /&gt;&lt;BR /&gt;Thank you.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Doug</description>
    <pubDate>Thu, 05 Feb 2026 19:15:07 GMT</pubDate>
    <dc:creator>dougwoody</dc:creator>
    <dc:date>2026-02-05T19:15:07Z</dc:date>
    <item>
      <title>Is S32K144 compliant to ISO 11898-1:2015</title>
      <link>https://community.nxp.com/t5/S32K/Is-S32K144-compliant-to-ISO-11898-1-2015/m-p/1651024#M22959</link>
      <description>&lt;P&gt;Hi&amp;nbsp; we are going to use S32K144 MCU for our product and our customer wants to have&amp;nbsp;ISO 11898-1:2015. May I know does s32k144 support&amp;nbsp;ISO 11898-1:2015? In reference manual its mentioned&amp;nbsp;ISO 11898-1:2003 but not&amp;nbsp;ISO 11898-1:2015.&lt;/P&gt;</description>
      <pubDate>Tue, 16 May 2023 09:31:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Is-S32K144-compliant-to-ISO-11898-1-2015/m-p/1651024#M22959</guid>
      <dc:creator>Dhwani</dc:creator>
      <dc:date>2023-05-16T09:31:41Z</dc:date>
    </item>
    <item>
      <title>Re: Is S32K144 compliant to ISO 11898-1:2015</title>
      <link>https://community.nxp.com/t5/S32K/Is-S32K144-compliant-to-ISO-11898-1-2015/m-p/1651344#M22970</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/199092"&gt;@Dhwani&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;yes, the CAN module supports ISO 11898-1:2015.&lt;/P&gt;
&lt;P&gt;Attached is conformance test report per ISO 16845-1:2016. This ISO defines conformance testing of ISO 11898-1:2015.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Tue, 16 May 2023 16:13:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Is-S32K144-compliant-to-ISO-11898-1-2015/m-p/1651344#M22970</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2023-05-16T16:13:09Z</dc:date>
    </item>
    <item>
      <title>Re: Is S32K144 compliant to ISO 11898-1:2015</title>
      <link>https://community.nxp.com/t5/S32K/Is-S32K144-compliant-to-ISO-11898-1-2015/m-p/2313169#M56634</link>
      <description>Hi lukaszadrapa,&lt;BR /&gt;&lt;BR /&gt;Please provide the conformance report for the S32K148 or a link to where these reports are available on the NXP site.&lt;BR /&gt;&lt;BR /&gt;Thank you.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Doug</description>
      <pubDate>Thu, 05 Feb 2026 19:15:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Is-S32K144-compliant-to-ISO-11898-1-2015/m-p/2313169#M56634</guid>
      <dc:creator>dougwoody</dc:creator>
      <dc:date>2026-02-05T19:15:07Z</dc:date>
    </item>
  </channel>
</rss>