<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックInquiry Regarding DMA Transmission Interference Between LPUART0 and LPUART1 (LIN Channel)</title>
    <link>https://community.nxp.com/t5/S32K/Inquiry-Regarding-DMA-Transmission-Interference-Between-LPUART0/m-p/2312653#M56612</link>
    <description>&lt;P&gt;Dear NXP Team,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Hello! I am currently working on a project utilizing the LPUART0​ instance for asynchronous UART data transmission with DMA. Additionally, LPUART1​ is configured as a LIN channel​ for communication with a slave device. I have encountered an issue where activating the DMA-based data transmission on LPUART0​ appears to interfere with the transmission process of LPUART1 (LIN channel). Specifically, I have traced the problem to the function Lpuart_Uart_Ip_StartSendDataUsingDma(), which suggests that the DMA Tx interrupt​ may be a contributing factor.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;Could you please help clarify why two separate LPUART instances might experience this type of interference, leading to LIN transmission errors (note: LIN reception remains unaffected)? Any insight into the potential root cause or recommendations for resolving this conflict would be greatly appreciated. Thank you for your time and assistance.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;DongXun&lt;/P&gt;</description>
    <pubDate>Thu, 05 Feb 2026 07:59:05 GMT</pubDate>
    <dc:creator>dongxun</dc:creator>
    <dc:date>2026-02-05T07:59:05Z</dc:date>
    <item>
      <title>Inquiry Regarding DMA Transmission Interference Between LPUART0 and LPUART1 (LIN Channel)</title>
      <link>https://community.nxp.com/t5/S32K/Inquiry-Regarding-DMA-Transmission-Interference-Between-LPUART0/m-p/2312653#M56612</link>
      <description>&lt;P&gt;Dear NXP Team,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Hello! I am currently working on a project utilizing the LPUART0​ instance for asynchronous UART data transmission with DMA. Additionally, LPUART1​ is configured as a LIN channel​ for communication with a slave device. I have encountered an issue where activating the DMA-based data transmission on LPUART0​ appears to interfere with the transmission process of LPUART1 (LIN channel). Specifically, I have traced the problem to the function Lpuart_Uart_Ip_StartSendDataUsingDma(), which suggests that the DMA Tx interrupt​ may be a contributing factor.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;Could you please help clarify why two separate LPUART instances might experience this type of interference, leading to LIN transmission errors (note: LIN reception remains unaffected)? Any insight into the potential root cause or recommendations for resolving this conflict would be greatly appreciated. Thank you for your time and assistance.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;DongXun&lt;/P&gt;</description>
      <pubDate>Thu, 05 Feb 2026 07:59:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Inquiry-Regarding-DMA-Transmission-Interference-Between-LPUART0/m-p/2312653#M56612</guid>
      <dc:creator>dongxun</dc:creator>
      <dc:date>2026-02-05T07:59:05Z</dc:date>
    </item>
    <item>
      <title>Re: Inquiry Regarding DMA Transmission Interference Between LPUART0 and LPUART1 (LIN Channel)</title>
      <link>https://community.nxp.com/t5/S32K/Inquiry-Regarding-DMA-Transmission-Interference-Between-LPUART0/m-p/2313743#M56644</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/247897"&gt;@dongxun&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Hard to say from the limited description, but since the LIN transmission is&amp;nbsp;timing‑sensitive, have you tried using a higher interrupt priority for the LIN channel?&lt;/P&gt;
&lt;P&gt;You did not mention what MCU part you use. But the DMA has also configurable priorities (fixed mode or round-robin) and bandwidth.&lt;/P&gt;
&lt;P&gt;There could be also a bug in the RTD. Please specify the RTD version.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 06 Feb 2026 12:05:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Inquiry-Regarding-DMA-Transmission-Interference-Between-LPUART0/m-p/2313743#M56644</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2026-02-06T12:05:55Z</dc:date>
    </item>
  </channel>
</rss>