<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FLXIO SENT IP driver in S32K</title>
    <link>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2303848#M56501</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;We have configured 4 SENT channels and assigned the channels as shown in the attachments. We are expecting Timer0, 1, 2, 3 to be configured for SENT RX and DMA transfer. Timer 5, 6, 7, 8 are configured for SPCO. We are seeing SENT frames with SPCO. We would expect Timer compare flags bit0 and 1 set and DMA transfer initiated which would clear the flag. We are using the S32K388 controller.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;FYI - The Software is currently using only 2 SENTs - meaning SPCO is sent out only for channel 0 and 1.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;One observation is that the TIMERSDEN register is showing a value of 0x0C. When all 4 SENTs are configured, shouldn't it be showing a value of 0x0F? Also, if only 2 SENTs are being used, should it only show 2 bits sets in this register? If only 2 bits, shouldn't it be Timer 0 and Timer1 bits at bits0 and 1? We think there is some mismatch in the timer mapping to the TIMERSDEN register.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Please find the attached screen shots for the configuration details also software version as below.&lt;/P&gt;&lt;P&gt;Build Version : S32K3_RTD_6_0_0_D2506_ASR_REL_4_7_REV_0000_20250610&lt;/P&gt;&lt;P&gt;* Project : RTD AUTOSAR 4.7&lt;BR /&gt;* Platform : CORTEXM&lt;BR /&gt;* Peripheral : FLEXIO_SENT_IP&lt;/P&gt;</description>
    <pubDate>Fri, 30 Jan 2026 14:25:18 GMT</pubDate>
    <dc:creator>annappa</dc:creator>
    <dc:date>2026-01-30T14:25:18Z</dc:date>
    <item>
      <title>FLXIO SENT IP driver</title>
      <link>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2303848#M56501</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;We have configured 4 SENT channels and assigned the channels as shown in the attachments. We are expecting Timer0, 1, 2, 3 to be configured for SENT RX and DMA transfer. Timer 5, 6, 7, 8 are configured for SPCO. We are seeing SENT frames with SPCO. We would expect Timer compare flags bit0 and 1 set and DMA transfer initiated which would clear the flag. We are using the S32K388 controller.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;FYI - The Software is currently using only 2 SENTs - meaning SPCO is sent out only for channel 0 and 1.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;One observation is that the TIMERSDEN register is showing a value of 0x0C. When all 4 SENTs are configured, shouldn't it be showing a value of 0x0F? Also, if only 2 SENTs are being used, should it only show 2 bits sets in this register? If only 2 bits, shouldn't it be Timer 0 and Timer1 bits at bits0 and 1? We think there is some mismatch in the timer mapping to the TIMERSDEN register.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Please find the attached screen shots for the configuration details also software version as below.&lt;/P&gt;&lt;P&gt;Build Version : S32K3_RTD_6_0_0_D2506_ASR_REL_4_7_REV_0000_20250610&lt;/P&gt;&lt;P&gt;* Project : RTD AUTOSAR 4.7&lt;BR /&gt;* Platform : CORTEXM&lt;BR /&gt;* Peripheral : FLEXIO_SENT_IP&lt;/P&gt;</description>
      <pubDate>Fri, 30 Jan 2026 14:25:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2303848#M56501</guid>
      <dc:creator>annappa</dc:creator>
      <dc:date>2026-01-30T14:25:18Z</dc:date>
    </item>
    <item>
      <title>Re: FLXIO SENT IP driver</title>
      <link>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2306956#M56585</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I tried to mimic your configuration using Sent_Receiver_S32K344 RTD demo example within S32DS.&lt;BR /&gt;&lt;SPAN&gt;I selected FlexIO channels 0,1,2,3 to be configured for SENT RX and DMA transfer and channels&amp;nbsp; 5, 6, 7, 8 configured for SPC.&lt;BR /&gt;&lt;/SPAN&gt;After Sent_init is called I see&amp;nbsp;&lt;SPAN&gt;TIMERSDEN=0xF, this seems to be consistent with channel mapping.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Are you able to share full configuration and simplified project so we can check it directly?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR, Petr&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 04 Feb 2026 11:54:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2306956#M56585</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2026-02-04T11:54:29Z</dc:date>
    </item>
    <item>
      <title>Re: FLXIO SENT IP driver</title>
      <link>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2312918#M56624</link>
      <description>&lt;P&gt;&lt;SPAN&gt;We are using the S32K388 controller, please find the attached configuration files for our project and pls let me know your feedback.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 05 Feb 2026 11:38:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2312918#M56624</guid>
      <dc:creator>annappa</dc:creator>
      <dc:date>2026-02-05T11:38:54Z</dc:date>
    </item>
    <item>
      <title>Re: FLXIO SENT IP driver</title>
      <link>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2318998#M56858</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I do not work with EB Tresos a lot, so I asked SW team to check your config files.&lt;BR /&gt;I forwarded SW engineer reply (indicating callback usage) directly to you, forgot to place it here. If that does not help, let me know so I can ask them again.&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;Petr&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 17 Feb 2026 11:49:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2318998#M56858</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2026-02-17T11:49:31Z</dc:date>
    </item>
    <item>
      <title>Re: FLXIO SENT IP driver</title>
      <link>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2320049#M56897</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/256605"&gt;@annappa&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;As we discussed on the call, can you upload latest configuration and code modifications you made?&lt;/P&gt;
&lt;P&gt;Thanks in advance!&lt;/P&gt;</description>
      <pubDate>Thu, 19 Feb 2026 05:26:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2320049#M56897</guid>
      <dc:creator>AxelR</dc:creator>
      <dc:date>2026-02-19T05:26:23Z</dc:date>
    </item>
    <item>
      <title>Re: FLXIO SENT IP driver</title>
      <link>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2320077#M56898</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;DMA buffer allocated for the Channel 0 &lt;STRONG&gt;Flexio_Sent_Ip_DmaTimerValue_0_0&lt;/STRONG&gt; array has value &lt;STRONG&gt;12&lt;/STRONG&gt;. During data processing we are calculating the Number of data including SPC (Func: &lt;STRONG&gt;Flexio_Sent_Ip_DmaHandler&lt;/STRONG&gt; line:&lt;STRONG&gt;NumberOfData = Receiver-&amp;gt;ChnlCfg[ChannelId].DmaBufferDepth * (Receiver-&amp;gt;ChnlCfg[ChannelId].NibbleCnt + 3U + (uint8)((Receiver-&amp;gt;ChnlCfg[ChannelId].SpcMode == FALSE) ? 0U : 1U)); )&lt;/STRONG&gt; the generated buffer array should be &lt;STRONG&gt;14&lt;/STRONG&gt; not &lt;STRONG&gt;12&lt;/STRONG&gt;. and We are seeing the DMA buffer value for Ch0 is overflowing to Ch1 buffer.&lt;/P&gt;&lt;P&gt;Below are the screenshot attached with Description.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;DMA_BufferSize12_WithOverFlow&lt;/STRONG&gt;: With DMA buffer size 12 the data is overflow to the Ch1 Buffer.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;DMA_BufferSize14_WithOutOverFlow&lt;/STRONG&gt;:&amp;nbsp;With DMA buffer size 14 there is no overflow of the data to Ch1.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Buffer_comparison_Srouce_Code&lt;/STRONG&gt;: Code comparison after manually editing buffer size to 14 in the&amp;nbsp;&lt;STRONG&gt;Flexio_Sent_Ip_Cfg.c&lt;/STRONG&gt; file.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 19 Feb 2026 07:36:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2320077#M56898</guid>
      <dc:creator>annappa</dc:creator>
      <dc:date>2026-02-19T07:36:55Z</dc:date>
    </item>
    <item>
      <title>Re: FLXIO SENT IP driver</title>
      <link>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2320091#M56899</link>
      <description>&lt;P&gt;Thanks&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/256605"&gt;@annappa&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Also can you share your latest configuration?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Thu, 19 Feb 2026 08:03:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2320091#M56899</guid>
      <dc:creator>AxelR</dc:creator>
      <dc:date>2026-02-19T08:03:13Z</dc:date>
    </item>
    <item>
      <title>Re: FLXIO SENT IP driver</title>
      <link>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2322056#M56973</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Please find the latest configuration attached.&lt;/P&gt;</description>
      <pubDate>Tue, 24 Feb 2026 17:18:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2322056#M56973</guid>
      <dc:creator>annappa</dc:creator>
      <dc:date>2026-02-24T17:18:26Z</dc:date>
    </item>
    <item>
      <title>Re: FLXIO SENT IP driver</title>
      <link>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2325268#M57068</link>
      <description>Hi Annappa&lt;BR /&gt;Thanks for the configuration update, I'm already reported the DMA issue with RTD team, they are investigating more on this, however, I see that you are enabling FlexIO ISR but not DMA ISR.&lt;BR /&gt;&lt;BR /&gt;The recommendation on Driver is to use the DMA interrupt in DMA to handle it.&lt;BR /&gt;&lt;BR /&gt;For the DMA buffer I'll update you as soon as we get feedback from RTD team, thanks!</description>
      <pubDate>Tue, 03 Mar 2026 01:50:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2325268#M57068</guid>
      <dc:creator>AxelR</dc:creator>
      <dc:date>2026-03-03T01:50:44Z</dc:date>
    </item>
    <item>
      <title>Re: FLXIO SENT IP driver</title>
      <link>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2325302#M57069</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/256605"&gt;@annappa&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Can you try to change the SENT Pause pulse to enabled?&lt;/P&gt;
&lt;DIV id="tinyMceEditorAxelR_0" class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="2026-03-03_11-26-19.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/378150iBF30C131CD1C119A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="2026-03-03_11-26-19.png" alt="2026-03-03_11-26-19.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;2026-03-03_11-26-19.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt; Thanks &amp;amp; best regards.&lt;/P&gt;
&lt;P&gt;Axel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Mar 2026 02:27:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2325302#M57069</guid>
      <dc:creator>AxelR</dc:creator>
      <dc:date>2026-03-03T02:27:18Z</dc:date>
    </item>
    <item>
      <title>Re: FLXIO SENT IP driver</title>
      <link>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2331113#M57273</link>
      <description>&lt;P&gt;Hi Axel,&lt;/P&gt;&lt;P&gt;We have configure the DMA logical channel and Flexio callback function in the Mcl, please find the attached Screenshot(DMA_Channel_config), Also SENT procesing type is set to DMA please find the attached screenshot(SENT_DMA_Process).&lt;/P&gt;&lt;P&gt;Please let me know how&amp;nbsp;&lt;SPAN&gt;Driver to use the DMA interrupt in DMA to handle it.?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Annappa&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 12 Mar 2026 07:35:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2331113#M57273</guid>
      <dc:creator>annappa</dc:creator>
      <dc:date>2026-03-12T07:35:25Z</dc:date>
    </item>
    <item>
      <title>Re: FLXIO SENT IP driver</title>
      <link>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2331397#M57290</link>
      <description>Also we need update on the DMA buffer.</description>
      <pubDate>Thu, 12 Mar 2026 11:10:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2331397#M57290</guid>
      <dc:creator>annappa</dc:creator>
      <dc:date>2026-03-12T11:10:47Z</dc:date>
    </item>
    <item>
      <title>Re: FLXIO SENT IP driver</title>
      <link>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2334338#M57367</link>
      <description>&lt;P&gt;Hi Annapa, have you tried the PAUSE checkbox I posted few weeks ago?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Also, the processing from SENT is done through notifications&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot 2026-03-18 095735.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/379562i1E1FDDC3617BA3EE/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Screenshot 2026-03-18 095735.png" alt="Screenshot 2026-03-18 095735.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Screenshot 2026-03-18 095735.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Please confirm that enabling the Pause pulse fixes the issue of DMA buffer (It increases from 12 to 14 elements the buffer).&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;
&lt;P&gt;Axel&lt;/P&gt;</description>
      <pubDate>Wed, 18 Mar 2026 00:59:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2334338#M57367</guid>
      <dc:creator>AxelR</dc:creator>
      <dc:date>2026-03-18T00:59:07Z</dc:date>
    </item>
    <item>
      <title>Re: FLXIO SENT IP driver</title>
      <link>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2334478#M57370</link>
      <description>&lt;P&gt;Hi Axel,&lt;/P&gt;&lt;P&gt;If we enable pause Pulse Buffer size may increase but this configuration doesn't match with our sensor configuration, our sensor configuration is without Pause pulse. Without Pause pulse array should generate with buffer size of 14.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Annappa&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 18 Mar 2026 07:08:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2334478#M57370</guid>
      <dc:creator>annappa</dc:creator>
      <dc:date>2026-03-18T07:08:41Z</dc:date>
    </item>
    <item>
      <title>Re: FLXIO SENT IP driver</title>
      <link>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2376811#M59029</link>
      <description>&lt;P&gt;Hello Axel,&lt;BR /&gt;Do you have any update on this topic ?&amp;nbsp;&lt;BR /&gt;Is this a defect in the Driver ?&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;Rahul&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 04 Jun 2026 11:18:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2376811#M59029</guid>
      <dc:creator>Rahul_Chakravarty</dc:creator>
      <dc:date>2026-06-04T11:18:14Z</dc:date>
    </item>
    <item>
      <title>Re: FLXIO SENT IP driver</title>
      <link>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2405801#M60513</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;It has confirmed that a change to the driver is needed.&amp;nbsp; Here is the Jira ticket:&amp;nbsp;&lt;A href="https://jira.sw.nxp.com/browse/SRTDCCOM-3401" target="_blank"&gt;[SRTDCCOM-3401] [SENT]Dma buffer is overflow when using SPC mode - NXP JIRA&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;John&lt;/P&gt;</description>
      <pubDate>Mon, 17 Aug 2026 14:22:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FLXIO-SENT-IP-driver/m-p/2405801#M60513</guid>
      <dc:creator>john_floros</dc:creator>
      <dc:date>2026-08-17T14:22:02Z</dc:date>
    </item>
  </channel>
</rss>